EmberCommandState Struct Reference
For use when declaring a separate command streams. The fields are not accessed directly by the application. More...
#include <
command-interpreter2.h
>
Data Fields | |
uint8_t | state |
uint8_t | buffer [EMBER_COMMAND_BUFFER_LENGTH] |
uint8_t | tokenIndices [MAX_TOKEN_COUNT+1] |
uint8_t | tokenCount |
uint16_t | index |
uint8_t | error |
uint8_t | hexHighNibble |
uint8_t | argOffset |
uint8_t | previousCharacter |
uint8_t | defaultBase |
EmberCommandEntry * | currentCommand |
For use when declaring a separate command streams. The fields are not accessed directly by the application.
Definition at line 399
of file command-interpreter2.h
.
Field Documentation
uint8_t EmberCommandState::argOffset |
Definition at line 425
of file command-interpreter2.h
.
uint8_t EmberCommandState::buffer[EMBER_COMMAND_BUFFER_LENGTH] |
Definition at line 406
of file command-interpreter2.h
.
EmberCommandEntry* EmberCommandState::currentCommand |
Definition at line 435
of file command-interpreter2.h
.
uint8_t EmberCommandState::defaultBase |
Definition at line 432
of file command-interpreter2.h
.
uint8_t EmberCommandState::error |
Definition at line 419
of file command-interpreter2.h
.
uint8_t EmberCommandState::hexHighNibble |
Definition at line 422
of file command-interpreter2.h
.
uint16_t EmberCommandState::index |
Definition at line 416
of file command-interpreter2.h
.
uint8_t EmberCommandState::previousCharacter |
Definition at line 429
of file command-interpreter2.h
.
uint8_t EmberCommandState::state |
Definition at line 401
of file command-interpreter2.h
.
uint8_t EmberCommandState::tokenCount |
Definition at line 413
of file command-interpreter2.h
.
uint8_t EmberCommandState::tokenIndices[MAX_TOKEN_COUNT+1] |
Definition at line 410
of file command-interpreter2.h
.
The documentation for this struct was generated from the following file:
command-interpreter2.h