Macros

#define EMBER_TASK_COUNT
The number of event tasks that can be tracked for the purpose of processor idling. More...
#define EMBER_HEAP_SIZE
The size in bytes of the Ember heap. More...
#define EMBER_CHILD_TABLE_SIZE
The maximum number of children that a node may have set by default to 0. If the application includes the optional parent support stack feature, this should be adjusted accordingly. More...
#define EMBER_CHILD_TABLE_TOKEN_SIZE
#define EMBER_CHILD_TIMEOUT_SEC
Every child should exchange regularly some sort of traffic with the parent. Eventually, if traffic is not exchanged for a prolonged period of time, the parent will remove the child from the child table. Range extenders periodically exchange network-level commands with the coordinator. End devices and sleepy end devices can use emberPollForData() as keep alive mechanism. More...
#define EMBER_INDIRECT_QUEUE_SIZE
The maximum number of pending indirect packets set by default to 0. If the application includes the optional parent support stack feature, this should be adjusted accordingly. More...
#define EMBER_MAC_OUTGOING_QUEUE_SIZE
The maximum number of packets in the outgoing MAC queue set by default to 0. If the application includes the optional MAC queue stack feature, this should be adjusted accordingly. More...
#define EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS
The maximum amount of time (in milliseconds) that the MAC will hold a message for indirect transmission to a child. More...
#define EMBER_MAX_INDIRECT_TRANSMISSION_TIMEOUT_MS
#define EMBER_NWK_RANGE_EXTENDER_UPDATE_PERIOD_SEC
The period in seconds a range extender sends an update command to the coordinator containing the list of its children. More...
#define EMBER_MAC_ACK_TIMEOUT_MS
The ACK timeout in milliseconds. This parameter should be fine-tuned to reduce energy consumption for sleepy devices and depends on the data rate of the PHY configuration used. More...
#define EMBER_RADIO_CCA_THRESHOLD
The CCA threshold used at the MAC layer. More...
#define EMBER_FREQUENCY_HOPPING_SEED
The frequency hopping channel sequence generation seed. More...
#define EMBER_FREQUENCY_HOPPING_START_CHANNEL
The lowest channel on the frequency hopping list. More...
#define EMBER_FREQUENCY_HOPPING_END_CHANNEL
The highest channel on the frequency hopping list. More...
#define EMBER_FREQUENCY_HOPPING_CHANNEL_DURATION_MS
The time in milliseconds to stay on each channel for frequency hopping. More...
#define EMBER_FREQUENCY_HOPPING_CHANNEL_GUARD_DURATION_MS
The time in milliseconds to guard each channel while frequency hopping. No MAC activity is allowed when entering or exiting the slot. More...
#define EMBER_FREQUENCY_HOPPING_SERVER_FREQ_INFO_BROADCAST_PERIOD_S
The duration in seconds after which the server should broadcast its frequency hopping information to allow clients to realign. More...
#define EMBER_FREQUENCY_HOPPING_CLIENT_RESYNC_PERIOD_S
The duration in seconds after which the client should resync with the server if the last resync happened more than this duration ago. More...

Detailed Description

All configurations have defaults. Therefore, many applications may not need to do anything special. However, you can override these defaults by creating a CONFIGURATION_HEADER and, within this header, defining the appropriate macro to a different size.

See ember-configuration-defaults.h for source code.

Macro Definition Documentation

#define EMBER_CHILD_TABLE_SIZE

The maximum number of children that a node may have set by default to 0. If the application includes the optional parent support stack feature, this should be adjusted accordingly.

Definition at line 51 of file ember-configuration-defaults.h .

#define EMBER_CHILD_TABLE_TOKEN_SIZE

Definition at line 54 of file ember-configuration-defaults.h .

#define EMBER_CHILD_TIMEOUT_SEC

Every child should exchange regularly some sort of traffic with the parent. Eventually, if traffic is not exchanged for a prolonged period of time, the parent will remove the child from the child table. Range extenders periodically exchange network-level commands with the coordinator. End devices and sleepy end devices can use emberPollForData() as keep alive mechanism.

Definition at line 64 of file ember-configuration-defaults.h .

#define EMBER_FREQUENCY_HOPPING_CHANNEL_DURATION_MS

The time in milliseconds to stay on each channel for frequency hopping.

Definition at line 142 of file ember-configuration-defaults.h .

#define EMBER_FREQUENCY_HOPPING_CHANNEL_GUARD_DURATION_MS

The time in milliseconds to guard each channel while frequency hopping. No MAC activity is allowed when entering or exiting the slot.

Definition at line 149 of file ember-configuration-defaults.h .

#define EMBER_FREQUENCY_HOPPING_CLIENT_RESYNC_PERIOD_S

The duration in seconds after which the client should resync with the server if the last resync happened more than this duration ago.

Definition at line 163 of file ember-configuration-defaults.h .

#define EMBER_FREQUENCY_HOPPING_END_CHANNEL

The highest channel on the frequency hopping list.

Definition at line 135 of file ember-configuration-defaults.h .

#define EMBER_FREQUENCY_HOPPING_SEED

The frequency hopping channel sequence generation seed.

Definition at line 123 of file ember-configuration-defaults.h .

#define EMBER_FREQUENCY_HOPPING_SERVER_FREQ_INFO_BROADCAST_PERIOD_S

The duration in seconds after which the server should broadcast its frequency hopping information to allow clients to realign.

Definition at line 156 of file ember-configuration-defaults.h .

#define EMBER_FREQUENCY_HOPPING_START_CHANNEL

The lowest channel on the frequency hopping list.

Definition at line 129 of file ember-configuration-defaults.h .

#define EMBER_HEAP_SIZE

The size in bytes of the Ember heap.

Definition at line 43 of file ember-configuration-defaults.h .

#define EMBER_INDIRECT_QUEUE_SIZE

The maximum number of pending indirect packets set by default to 0. If the application includes the optional parent support stack feature, this should be adjusted accordingly.

Definition at line 72 of file ember-configuration-defaults.h .

#define EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS

The maximum amount of time (in milliseconds) that the MAC will hold a message for indirect transmission to a child.

The default is 8000 milliseconds (8 sec). The maximum value is 30 seconds (30000 milliseconds). Larger values will cause rollover confusion.

Definition at line 91 of file ember-configuration-defaults.h .

#define EMBER_MAC_ACK_TIMEOUT_MS

The ACK timeout in milliseconds. This parameter should be fine-tuned to reduce energy consumption for sleepy devices and depends on the data rate of the PHY configuration used.

Definition at line 111 of file ember-configuration-defaults.h .

#define EMBER_MAC_OUTGOING_QUEUE_SIZE

The maximum number of packets in the outgoing MAC queue set by default to 0. If the application includes the optional MAC queue stack feature, this should be adjusted accordingly.

Definition at line 80 of file ember-configuration-defaults.h .

#define EMBER_MAX_INDIRECT_TRANSMISSION_TIMEOUT_MS

Definition at line 93 of file ember-configuration-defaults.h .

#define EMBER_NWK_RANGE_EXTENDER_UPDATE_PERIOD_SEC

The period in seconds a range extender sends an update command to the coordinator containing the list of its children.

Definition at line 103 of file ember-configuration-defaults.h .

#define EMBER_RADIO_CCA_THRESHOLD

The CCA threshold used at the MAC layer.

Definition at line 117 of file ember-configuration-defaults.h .

#define EMBER_TASK_COUNT

The number of event tasks that can be tracked for the purpose of processor idling.

Definition at line 37 of file ember-configuration-defaults.h .