Ota Broadcast Bootloader Server Plugin
Macros |
|
| #define | EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_STACK_ERRORS |
|
The number of consecutive stack message submission errors or stack-related errors, such as CCA failures, after which the plugin gives up.
More...
|
|
| #define | EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_UNICAST_ERRORS |
|
The number of consecutive unicast attempts after which a target is declared unreachable. Legal values for this are in the [0,7] range.
More...
|
|
| #define | EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_RESPONSE_TIMEOUT_MS |
|
The time in milliseconds after which the server gives up waiting for a response from a client.
More...
|
|
| #define | EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_BROADCAST_ROUNDS |
|
The maximum number of image broadcast rounds the server performs before declaring an image distribution process failed.
More...
|
|
Functions |
|
| EmberAfOtaBootloaderStatus | emberAfPluginOtaBootloaderServerInitiateImageDistribution (uint32_t imageSize, uint8_t imageTag, EmberNodeId *targetList, uint16_t targetListLength) |
|
Initiates the image distribution process. The application can use the
emberAfPluginBootloaderServerGetTargetStatus()
API at any time during the image distribution process to check the status of each target.
More...
|
|
| EmberAfOtaBootloaderStatus | emberAfPluginBootloaderServerInitiateRequestTargetsStatus ( EmberNodeId *targetList, uint16_t targetListLength, uint8_t applicationServerStatus) |
|
Initiates the process to request the status of a set of target devices. The application can use the
emberAfPluginBootloaderServerGetTargetStatus()
API at any time during the target status request process to check the status of each target.
More...
|
|
| EmberAfOtaBootloaderStatus | emberAfPluginBootloaderServerInitiateRequestTargetsBootload (uint32_t bootloadDelayMs, uint8_t imageTag, EmberNodeId *targetList, uint16_t targetListLength) |
|
Starts the process where a server requests a set of target devices to initiate the bootload of a received image at some point in the future. The application can use the
emberAfPluginBootloaderServerGetTargetStatus()
API at any time during the bootload request process to check the status of each target.
More...
|
|
| EmberAfOtaBootloaderTargetStatus | emberAfPluginBootloaderServerGetTargetStatus ( EmberNodeId targetId, uint8_t *applicationTargetStatus) |
|
Retrieves the status of an individual target in the distribution list.
More...
|
|
| EmberAfOtaBootloaderStatus | emberAfPluginOtaBootloaderServerAbortCurrentProcess (void) |
|
Aborts the ongoing process (image distribution, status request or bootload request). Note that aborting a bootload request process likely results in some targets performing the bootload while some others do not.
More...
|
|
| bool | emberAfPluginOtaBootloaderServerGetImageSegmentCallback (uint32_t startIndex, uint32_t endIndex, uint8_t imageTag, uint8_t *imageSegment) |
|
A callback invoked by the OTA Bootloader Server plugin during an image distribution process to retrieve a contiguous segment of the image being distributed.
More...
|
|
| void | emberAfPluginOtaBootloaderServerImageDistributionCompleteCallback ( EmberAfOtaBootloaderStatus status) |
|
A callback invoked by the OTA Bootloader Server plugin when the image distribution process is terminated. The application can use the
emberAfPluginBootloaderServerGetTargetStatus()
API to retrieve the status reported by each target device.
More...
|
|
| void | emberAfPluginBootloaderServerRequestTargetsStatusCompleteCallback ( EmberAfOtaBootloaderStatus status) |
|
A callback invoked by the OTA Bootloader Server plugin when bootload request process has completed. Within this callback, the application should use the ::emberAfPluginBoootloaderServerGetTargetStatus() API to retrieve the status and application status reported by each target.
More...
|
|
| void | emberAfPluginBootloaderServerRequestTargetsBootloadCompleteCallback ( EmberAfOtaBootloaderStatus status) |
|
A callback invoked by the OTA Bootloader Server plugin when a bootload request process has completed. Within this callback, the application should use the ::emberAfPluginBoootloaderServerGetTargetStatus() API to retrieve the status and the application status reported by each target.
More...
|
|
Detailed Description
See
ota-broadcast-bootloader-server.h
for source code.
Macro Definition Documentation
| #define EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_BROADCAST_ROUNDS |
The maximum number of image broadcast rounds the server performs before declaring an image distribution process failed.
Definition at line
36
of file
ota-broadcast-bootloader-server.h
.
| #define EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_STACK_ERRORS |
The number of consecutive stack message submission errors or stack-related errors, such as CCA failures, after which the plugin gives up.
Definition at line
18
of file
ota-broadcast-bootloader-server.h
.
| #define EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_UNICAST_ERRORS |
The number of consecutive unicast attempts after which a target is declared unreachable. Legal values for this are in the [0,7] range.
Definition at line
24
of file
ota-broadcast-bootloader-server.h
.
| #define EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_RESPONSE_TIMEOUT_MS |
The time in milliseconds after which the server gives up waiting for a response from a client.
Definition at line
30
of file
ota-broadcast-bootloader-server.h
.
Function Documentation
| EmberAfOtaBootloaderTargetStatus emberAfPluginBootloaderServerGetTargetStatus | ( | EmberNodeId |
targetId,
|
| uint8_t * |
applicationTargetStatus
|
||
| ) |
Retrieves the status of an individual target in the distribution list.
- Parameters
-
targetIdThe node ID of the target device whose status is being requested. applicationTargetStatusThe application status reported by the client side application. This parameter is valid only for certain return status codes (see return status documentation).
- Returns
-
An
EmberAfOtaBootloaderTargetStatus
value of:
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_INVALID if the passed node ID does not appear in the current server target list of the current ongoing process or if there is no current ongoing process.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_UNREACHABLE if the target has not responded to any of the server's unicast messages.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_COMPLETED if the server is currently performing an image distribution process and the target confirmed that it received the full image.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_ONGOING if the server is currently performing an image distribution process and the target has partially received the image and distribution is continuing.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_REFUSED if the target has refused the current image.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_FAILED if the server is currently performing an image distribution process and the target reported that an error was encountered.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_DISTRIBUTION_ABORTED if the server is currently performing an image distribution process and the target decided to abort the image download process. In this case, the client also reports an application status. Therefore, the applicationTargetStatus parameter is valid.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_STATUS_REQUEST_COMPLETED if the server is currently performing a target status request process and the target has responded to the server's inquiry. In this case, the client also reports an application status. Therefore, the applicationTargetStatus parameter is valid.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_STATUS_REQUEST_ONGOING if the server is currently performing a target status request process and the target is not yet queried by the server.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_BOOTLOAD_REQUEST_ACCEPTED is the server is currently performing a bootload request process and the target has accepted to perform the requested image bootload.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_BOOTLOAD_REQUEST_REFUSED is the server is currently performing a bootload request process and the target has refused to perform the requested image bootload.
- EMBER_OTA_BROADCAST_BOOTLOADER_TARGET_STATUS_BOOTLOAD_REQUEST_ONGOING is the server is currently performing a bootload request process and the target is not yet reached by the server.
| EmberAfOtaBootloaderStatus emberAfPluginBootloaderServerInitiateRequestTargetsBootload | ( | uint32_t |
bootloadDelayMs,
|
| uint8_t |
imageTag,
|
||
| EmberNodeId * |
targetList,
|
||
| uint16_t |
targetListLength
|
||
| ) |
Starts the process where a server requests a set of target devices to initiate the bootload of a received image at some point in the future. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API at any time during the bootload request process to check the status of each target.
- Parameters
-
bootloadDelayMsThe delay in milliseconds after which all the targets should perform an image bootload. imageTagA 1-byte tag that identifies the image to be bootloaded at the target devices. targetListAn array of EmberNodeId indicating the node IDs of the target devices that is requested to bootload an image. targetListLengthThe length of the passed target list.
- Returns
-
An
EmberAfOtaBootloaderStatus
value of:
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if the plugin successfully initiated the process of requesting a set of targets to initiate a bootload. If this is the case, the corresponding callback emberAfPluginBootloaderServerRequestTargetsBootloadCompleteCallback() shall be invoked when the request process to all targets has completed.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_INVALID_CALL if some of the passed parameters are invalid.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_BUSY if the server is currently involved in another over-the-air process.
| EmberAfOtaBootloaderStatus emberAfPluginBootloaderServerInitiateRequestTargetsStatus | ( | EmberNodeId * |
targetList,
|
| uint16_t |
targetListLength,
|
||
| uint8_t |
applicationServerStatus
|
||
| ) |
Initiates the process to request the status of a set of target devices. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API at any time during the target status request process to check the status of each target.
- Parameters
-
targetListAn array of EmberNodeId indicating the node IDs of the target devices that are queried for their status. targetListLengthThe length of the passed target list.
- Returns
-
An
EmberAfOtaBootloaderStatus
value of:
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if the plugin successfully initiated the process of requesting the status of a set of targets. If this is the case, the corresponding callback emberAfPluginBootloaderServerRequestTargetsStatusCompleteCallback() is invoked when the request process to all targets completes.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_INVALID_CALL if some of the passed parameters are invalid.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_BUSY if the server is currently involved in another over-the-air process.
| void emberAfPluginBootloaderServerRequestTargetsBootloadCompleteCallback | ( | EmberAfOtaBootloaderStatus |
status
|
) |
A callback invoked by the OTA Bootloader Server plugin when a bootload request process has completed. Within this callback, the application should use the ::emberAfPluginBoootloaderServerGetTargetStatus() API to retrieve the status and the application status reported by each target.
- Parameters
-
statusAn EmberAfOtaBootloaderStatus value of: - EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if all targets have been requested to perform a bootload. Notice that some targets might have been declared unreachable.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_STACK_ERROR if the server encountered multiple consecutive transmission errors. The Server gives up the bootload request process if EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_STACK_ERRORS consecutive transmission errors are encountered.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_ABORTED if the application aborted the current bootload request process.
| void emberAfPluginBootloaderServerRequestTargetsStatusCompleteCallback | ( | EmberAfOtaBootloaderStatus |
status
|
) |
A callback invoked by the OTA Bootloader Server plugin when bootload request process has completed. Within this callback, the application should use the ::emberAfPluginBoootloaderServerGetTargetStatus() API to retrieve the status and application status reported by each target.
- Parameters
-
statusAn EmberAfOtaBootloaderStatus value of: - EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if all the targets have been queried for their status. Notice that some targets might have been declared unreachable.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_STACK_ERROR if the server encountered multiple consecutive transmission errors. The Server gives up the targets status request process if EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_STACK_ERRORS consecutive transmission errors are encountered.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_ABORTED if the application aborted the current targets status request process.
| EmberAfOtaBootloaderStatus emberAfPluginOtaBootloaderServerAbortCurrentProcess | ( | void |
|
) |
Aborts the ongoing process (image distribution, status request or bootload request). Note that aborting a bootload request process likely results in some targets performing the bootload while some others do not.
- Returns
-
An
EmberAfOtaBootloaderStatus
value of:
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if the current ongoing process was successfully aborted.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_INVALID_CALL if the server is not currently involved in any process.
| bool emberAfPluginOtaBootloaderServerGetImageSegmentCallback | ( | uint32_t |
startIndex,
|
| uint32_t |
endIndex,
|
||
| uint8_t |
imageTag,
|
||
| uint8_t * |
imageSegment
|
||
| ) |
A callback invoked by the OTA Bootloader Server plugin during an image distribution process to retrieve a contiguous segment of the image being distributed.
- Parameters
-
startIndexThe index of the first byte the application should copy into the passed array. endIndexThe index of the last byte the application should copy into the passed array. imageTagA 1-byte tag of the image for which a segment is being requested. imageSegmentAn array of (endIndex - startIndex + 1) length to which the application should copy the requested image segment.
- Returns
- A boolean indicating whether the application successfully copied the requested bytes into the passed array. If the application returns FALSE, the OTA Server plugin aborts the ongoing distribution process.
| void emberAfPluginOtaBootloaderServerImageDistributionCompleteCallback | ( | EmberAfOtaBootloaderStatus |
status
|
) |
A callback invoked by the OTA Bootloader Server plugin when the image distribution process is terminated. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API to retrieve the status reported by each target device.
- Parameters
-
statusAn EmberAfOtaBootloaderStatus value of: - EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if all targets have confirmed that the full image was received except for those that have been declared "unreachable".
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_DATA_UNDERFLOW if the application failed to supply the requested image segments.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_STACK_ERROR if the server encountered multiple consecutive transmission errors. The Server gives up the image distribution process if EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_STACK_ERRORS consecutive transmission errors are encountered.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_FAILED if the distribution process terminated prematurely because all targets have been declared unreachable.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_TIMEOUT if the server performed all the allowable broadcast rounds and there are still missing segments at one or more targets. The maximum allowable rounds are defined by EMBER_AF_PLUGIN_OTA_BROADCAST_BOOTLOADER_SERVER_MAX_BROADCAST_ROUNDS .
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_ABORTED if the application aborted the current image distribution process.
| EmberAfOtaBootloaderStatus emberAfPluginOtaBootloaderServerInitiateImageDistribution | ( | uint32_t |
imageSize,
|
| uint8_t |
imageTag,
|
||
| EmberNodeId * |
targetList,
|
||
| uint16_t |
targetListLength
|
||
| ) |
Initiates the image distribution process. The application can use the emberAfPluginBootloaderServerGetTargetStatus() API at any time during the image distribution process to check the status of each target.
- Parameters
-
imageSizeThe image size in bytes to be distributed. imageTagA 1-byte tag that will be embedded in the server-to-client over-the-air messages. The application can use the image tag for versioning purposes and/or for distinguishing between different image types. targetListAn array of EmberNodeId indicating the node IDs of the target devices. targetListLengthThe length of the passed target list.
- Returns
-
An
EmberAfOtaBootloaderStatus
value of:
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_SUCCESS if the image distribution is successfully initiated. If this is the case, the ::emberAfPluginOtaBootloaderServerDistributionCompletedCallback() callback is invoked when the distribution process terminates.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_INVALID_CALL if some of the passed parameters are invalid.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_BUSY if the server is already performing another image distribution or some other over-the-air process.
- EMBER_OTA_BROADCAST_BOOTLOADER_STATUS_NO_BUFFERS if the server currently doesn't have enough RAM to store the passed target list.