EmberIncomingMessage Struct Reference

An instance of this structure is passed to emberIncomingMessageHandler(). It describes the incoming message. More...

#include <ember-types.h>

Data Fields

EmberMessageOptions options
 
EmberNodeId source
 
uint8_t endpoint
 
int8_t rssi
 
EmberMessageLength length
 
uint8_t * payload
 

An instance of this structure is passed to emberIncomingMessageHandler(). It describes the incoming message.

Definition at line 180 of file ember-types.h.

Field Documentation

uint8_t EmberIncomingMessage::endpoint

The endpoint the message is destined to.

Definition at line 193 of file ember-types.h.

EmberMessageLength EmberIncomingMessage::length

An EmberMessageLength value indicating the length in bytes of the incoming message.

Definition at line 202 of file ember-types.h.

EmberMessageOptions EmberIncomingMessage::options

An EmberMessageOptions value indicating the options used for the incoming packet.

Definition at line 185 of file ember-types.h.

uint8_t* EmberIncomingMessage::payload

A pointer to the message payload.

Definition at line 206 of file ember-types.h.

int8_t EmberIncomingMessage::rssi

The RSSI the packet was received with.

Definition at line 197 of file ember-types.h.

EmberNodeId EmberIncomingMessage::source

An EmberNodeId value indicating source node ID.

Definition at line 189 of file ember-types.h.


The documentation for this struct was generated from the following file:
  • ember-types.h