You are viewing documentation for version:
2.5
|
Version History
-
Global
EMBER_MAX_SECURED_APPLICATION_PAYLOAD_LENGTH
-
The maximum length in bytes of the application payload for a secured message. This define has been deprecated, you should use the
emberGetMaximumPayloadLength
API instead.
-
Global
EMBER_MAX_UNSECURED_APPLICATION_PAYLOAD_LENGTH
-
The maximum length in bytes of the application payload for an unsecured message. This define has been deprecated, you should use the
emberGetMaximumPayloadLength
API instead.
-
Global
emberIncomingBeaconHandler
(EmberPanId panId, EmberNodeId nodeId, int8_t rssi, bool permitJoining, uint8_t payloadLength, uint8_t *payload)
-
This stack handler has been deprecated and will be removed in a future release. The application should implement
emberIncomingBeaconExtendedHandler
instead.
-
Global
emberMacSetAllocateAddressFlag
(bool allocateAddress)
-
Configures the "allocate address" flag in the association request command for nodes joining as
EMBER_MAC_MODE_DEVICE
or
EMBER_MAC_MODE_SLEEPY_DEVICE
. This flag should be set if the device wishes to obtain a random 16-bit address from the coordinator. If cleared, the coordinator will not assign a 16-bit address to the device.