An instance of this structure is passed to emberIncomingMessageHandler() . It describes the incoming message. More...

#include < ember-types.h >

Data Fields

EmberMessageOptions options
EmberNodeId source
uint8_t endpoint
int8_t rssi
EmberMessageLength length
uint8_t * payload

An instance of this structure is passed to emberIncomingMessageHandler() . It describes the incoming message.

Definition at line 215 of file ember-types.h .

Field Documentation

uint8_t EmberIncomingMessage::endpoint

The endpoint the message is destined to.

Definition at line 228 of file ember-types.h .

EmberMessageLength EmberIncomingMessage::length

An EmberMessageLength value indicating the length in bytes of the incoming message.

Definition at line 237 of file ember-types.h .

EmberMessageOptions EmberIncomingMessage::options

An EmberMessageOptions value indicating the options used for the incoming packet.

Definition at line 220 of file ember-types.h .

uint8_t* EmberIncomingMessage::payload

A pointer to the message payload.

Definition at line 241 of file ember-types.h .

int8_t EmberIncomingMessage::rssi

The RSSI in dBm the packet was received with.

Definition at line 232 of file ember-types.h .

EmberNodeId EmberIncomingMessage::source

An EmberNodeId value indicating source node ID.

Definition at line 224 of file ember-types.h .


The documentation for this struct was generated from the following file:
  • ember-types.h