Common Microcontroller Functions
Data Structures |
|
| struct | RTCCRamData |
Macros |
|
| #define | halGetEm2xxResetInfo () |
|
Calls
halGetExtendedResetInfo()
and translates the EM35x reset code to the corresponding value used by the EM2XX HAL. Any reset codes not present in the EM2XX are returned after being OR'ed with 0x80.
More...
|
|
| #define | MICRO_DISABLE_WATCH_DOG_KEY |
|
The value that must be passed as the single parameter to
halInternalDisableWatchDog()
in order to successfully disable the watchdog timer.
More...
|
|
| #define | GPIO_MASK_SIZE |
| #define | GPIO_MASK |
| #define | WAKE_GPIO_MASK |
| #define | WAKE_GPIO_SIZE |
| #define | WAKE_MASK_INVALID |
| #define | WAKE_EVENT_SIZE |
| #define | DEBUG_TOGGLE (n) |
Typedefs |
|
| typedef uint32_t | WakeEvents |
| typedef uint32_t | WakeMask |
Enumerations |
|
| enum |
SleepModes
{
SLEEPMODE_RUNNING , SLEEPMODE_IDLE , SLEEPMODE_WAKETIMER , SLEEPMODE_MAINTAINTIMER , SLEEPMODE_NOTIMER , SLEEPMODE_HIBERNATE , SLEEPMODE_RESERVED , SLEEPMODE_POWERDOWN , SLEEPMODE_POWERSAVE } |
|
Enumerations for the possible microcontroller sleep modes.
More...
|
|
Functions |
|
| void | halStackProcessBootCount (void) |
|
Called from emberInit and provides a means for the HAL to increment a boot counter, most commonly in non-volatile memory.
More...
|
|
| uint8_t | halGetResetInfo (void) |
|
Gets information about what caused the microcontroller to reset.
More...
|
|
| PGM_P | halGetResetString (void) |
|
Calls
halGetResetInfo()
and supplies a string describing it.
More...
|
|
| void | halInit (void) |
|
Initializes microcontroller-specific peripherals.
More...
|
|
| void | halReboot (void) |
|
Restarts the microcontroller and therefore everything else.
More...
|
|
| void | halPowerUp (void) |
|
Powers up microcontroller peripherals and board peripherals.
More...
|
|
| void | halPowerDown (void) |
|
Powers down microcontroller peripherals and board peripherals.
More...
|
|
| void | halResume (void) |
|
Resumes microcontroller peripherals and board peripherals.
More...
|
|
| void | halSuspend (void) |
|
Suspends microcontroller peripherals and board peripherals.
More...
|
|
| void | halInternalEnableWatchDog (void) |
|
Enables the watchdog timer.
More...
|
|
| void | halInternalDisableWatchDog (uint8_t magicKey) |
|
Disables the watchdog timer.
More...
|
|
| bool | halInternalWatchDogEnabled (void) |
|
Determines whether the watchdog has been enabled or disabled.
More...
|
|
| void | halSleep ( SleepModes sleepMode) |
|
Puts the microcontroller to sleep in a specified mode.
More...
|
|
| void | halSleepPreserveInts ( SleepModes sleepMode) |
|
Same as
halSleep()
except it preserves the current interrupt state rather than always enabling interrupts prior to returning.
More...
|
|
| void | halCommonDelayMicroseconds (uint16_t us) |
|
Blocks the current thread of execution for the specified amount of time, in microseconds.
More...
|
|
| void | halCommonDisableVreg1v8 (void) |
|
Disable the 1.8V regulator. This function is to be used when the 1.8V supply is provided externally. Disabling the regulator saves current consumption. Disabling the regulator will cause ADC readings of external signals to be wrong. These exteranl signals include analog sources ADC0 thru ADC5 and VDD_PADS/4.
More...
|
|
| void | halCommonEnableVreg1v8 (void) |
|
Enable the 1.8V regulator. Normally the 1.8V regulator is enabled out of reset. This function is only needed if the 1.8V regulator has been disabled and ADC conversions on external signals are needed. These exteranl signals include analog sources ADC0 thru ADC5 and VDD_PADS/4. The state of 1v8 survives deep sleep.
More...
|
|
| void | halBeforeEM4 (uint32_t duration, RTCCRamData input) |
| RTCCRamData | halAfterEM4 (void) |
| void | halInternalSysReset (uint16_t extendedCause) |
|
Records the specified reset cause then forces a reboot.
More...
|
|
| uint16_t | halGetExtendedResetInfo (void) |
|
Returns the Extended Reset Cause information.
More...
|
|
| PGM_P | halGetExtendedResetString (void) |
|
Calls
halGetExtendedResetInfo()
and supplies a string describing the extended cause of the reset.
halGetResetString()
should also be called to get the string for the base reset cause.
More...
|
|
| EmberStatus | halSetRadioHoldOff (bool enable) |
|
Enables or disables Radio HoldOff support.
More...
|
|
| bool | halGetRadioHoldOff (void) |
|
Returns whether Radio HoldOff has been enabled or not.
More...
|
|
| void | halStackRadioPowerDownBoard (void) |
|
To assist with saving power when the radio automatically powers down, this function allows the stack to tell the HAL to put pins specific to radio functionality in their powerdown state. The pin state used is the state used by halInternalPowerDownBoard, but applied only to the pins identified in the global variable gpioRadioPowerBoardMask. The stack will automatically call this function as needed, but it will only change GPIO state based on gpioRadioPowerBoardMask. Most commonly, the bits set in gpioRadioPowerBoardMask petain to using a Front End Module. This function is often called from interrupt context.
More...
|
|
| void | halStackRadio2PowerDownBoard (void) |
|
To assist with saving power when radio2 automatically powers down, this function allows the stack to tell the HAL to put pins specific to radio functionality in their powerdown state. The pin state used is the state used by halInternalPowerDownBoard, but applied only to the pins identified in the global variable gpioRadioPowerBoardMask. The stack will automatically call this function as needed, but it will only change GPIO state based on gpioRadioPowerBoardMask. Most commonly, the bits set in gpioRadioPowerBoardMask petain to using a Front End Module. This function is often called from interrupt context.
More...
|
|
| void | halStackRadioPowerUpBoard (void) |
|
To assist with saving power when the radio automatically powers up, this function allows the stack to tell the HAL to put pins specific to radio functionality in their powerup state. The pin state used is the state used by halInternalPowerUpBoard, but applied only to the pins identified in the global variable gpioRadioPowerBoardMask. The stack will automatically call this function as needed, but it will only change GPIO state based on gpioRadioPowerBoardMask. Most commonly, the bits set in gpioRadioPowerBoardMask petain to using a Front End Module. This function can be called from interrupt context.
More...
|
|
| void | halStackRadio2PowerUpBoard (void) |
|
To assist with saving power when radio2 automatically powers up, this function allows the stack to tell the HAL to put pins specific to radio functionality in their powerup state. The pin state used is the state used by halInternalPowerUpBoard, but applied only to the pins identified in the global variable gpioRadioPowerBoardMask. The stack will automatically call this function as needed, but it will only change GPIO state based on gpioRadioPowerBoardMask. Most commonly, the bits set in gpioRadioPowerBoardMask petain to using a Front End Module. This function can be called from interrupt context.
More...
|
|
| void | halStackRadioPowerMainControl (bool powerUp) |
|
This function is called automatically by the stack prior to Radio power-up and after Radio power-down. It can be used to prepare for the radio being powered on and to clean up after it's been powered off. Unlike
halStackRadioPowerUpBoard()
and
halStackRadioPowerDownBoard()
, which can be called from interrupt context, this function is only called from main-line context.
More...
|
|
| void | halRadioPowerUpHandler (void) |
|
Handler called in main context prior to radio being powered on.
More...
|
|
| void | halRadioPowerDownHandler (void) |
|
Handler called in main context after radio has been powered off.
More...
|
|
Variables |
|
| volatile int8_t | halCommonVreg1v8EnableCount |
|
Helper variable to track the state of 1.8V regulator.
More...
|
|
Vector Table Index Definitions |
|
|
These are numerical definitions for vector table. Indices 0 through 15 are Cortex-M3 standard exception vectors and indices 16 through 35 are EM3XX specific interrupt vectors. |
|
| #define | STACK_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | RESET_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | NMI_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | HARD_FAULT_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | MEMORY_FAULT_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | BUS_FAULT_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | USAGE_FAULT_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | RESERVED07_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | RESERVED08_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | RESERVED09_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | RESERVED10_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | SVCALL_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | DEBUG_MONITOR_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | RESERVED13_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | PENDSV_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | SYSTICK_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | TIMER1_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | TIMER2_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | MANAGEMENT_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | BASEBAND_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | SLEEP_TIMER_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | SC1_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | SC2_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | SECURITY_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | MAC_TIMER_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | MAC_TX_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | MAC_RX_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | ADC_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | IRQA_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | IRQB_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | IRQC_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | IRQD_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | DEBUG_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | SC3_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | SC4_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | USB_VECTOR_INDEX |
|
A numerical definition for a vector.
More...
|
|
| #define | VECTOR_TABLE_LENGTH |
|
Number of vectors.
More...
|
|
Detailed Description
Many of the supplied example applications use these microcontroller functions. See
hal/micro/micro.h
for source code.
- Note
- The term SFD refers to the Start Frame Delimiter.
Many of the supplied example applications use these microcontroller functions. See
hal/micro/micro-common.h
for source code.
See also
hal/micro/cortexm3/micro.h
for source code.
Macro Definition Documentation
| #define ADC_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
162
of file
cortexm3/micro.h
.
| #define BASEBAND_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
154
of file
cortexm3/micro.h
.
| #define BUS_FAULT_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
140
of file
cortexm3/micro.h
.
| #define DEBUG_MONITOR_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
147
of file
cortexm3/micro.h
.
| #define DEBUG_TOGGLE | ( |
n
|
) |
Definition at line
278
of file
micro-common.h
.
| #define DEBUG_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
167
of file
cortexm3/micro.h
.
| #define GPIO_MASK |
Definition at line
228
of file
micro-common.h
.
| #define GPIO_MASK_SIZE |
Definition at line
227
of file
micro-common.h
.
| #define halGetEm2xxResetInfo | ( |
|
) |
Calls halGetExtendedResetInfo() and translates the EM35x reset code to the corresponding value used by the EM2XX HAL. Any reset codes not present in the EM2XX are returned after being OR'ed with 0x80.
- Application Usage:
- Used by the EZSP host as a platform-independent NCP reset code.
- Returns
- The EM2XX-compatible reset code. If not supported by the EM2XX, return the platform-specific code with B7 set.
Definition at line
98
of file
micro.h
.
| #define HARD_FAULT_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
138
of file
cortexm3/micro.h
.
| #define IRQA_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
163
of file
cortexm3/micro.h
.
| #define IRQB_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
164
of file
cortexm3/micro.h
.
| #define IRQC_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
165
of file
cortexm3/micro.h
.
| #define IRQD_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
166
of file
cortexm3/micro.h
.
| #define MAC_RX_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
161
of file
cortexm3/micro.h
.
| #define MAC_TIMER_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
159
of file
cortexm3/micro.h
.
| #define MAC_TX_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
160
of file
cortexm3/micro.h
.
| #define MANAGEMENT_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
153
of file
cortexm3/micro.h
.
| #define MEMORY_FAULT_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
139
of file
cortexm3/micro.h
.
| #define MICRO_DISABLE_WATCH_DOG_KEY |
The value that must be passed as the single parameter to halInternalDisableWatchDog() in order to successfully disable the watchdog timer.
Definition at line
56
of file
micro-common.h
.
| #define NMI_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
137
of file
cortexm3/micro.h
.
| #define PENDSV_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
149
of file
cortexm3/micro.h
.
| #define RESERVED07_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
142
of file
cortexm3/micro.h
.
| #define RESERVED08_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
143
of file
cortexm3/micro.h
.
| #define RESERVED09_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
144
of file
cortexm3/micro.h
.
| #define RESERVED10_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
145
of file
cortexm3/micro.h
.
| #define RESERVED13_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
148
of file
cortexm3/micro.h
.
| #define RESET_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
136
of file
cortexm3/micro.h
.
| #define SC1_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
156
of file
cortexm3/micro.h
.
| #define SC2_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
157
of file
cortexm3/micro.h
.
| #define SC3_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
168
of file
cortexm3/micro.h
.
| #define SC4_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
169
of file
cortexm3/micro.h
.
| #define SECURITY_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
158
of file
cortexm3/micro.h
.
| #define SLEEP_TIMER_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
155
of file
cortexm3/micro.h
.
| #define STACK_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
135
of file
cortexm3/micro.h
.
| #define SVCALL_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
146
of file
cortexm3/micro.h
.
| #define SYSTICK_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
150
of file
cortexm3/micro.h
.
| #define TIMER1_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
151
of file
cortexm3/micro.h
.
| #define TIMER2_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
152
of file
cortexm3/micro.h
.
| #define USAGE_FAULT_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
141
of file
cortexm3/micro.h
.
| #define USB_VECTOR_INDEX |
A numerical definition for a vector.
Definition at line
170
of file
cortexm3/micro.h
.
| #define VECTOR_TABLE_LENGTH |
Number of vectors.
Definition at line
175
of file
cortexm3/micro.h
.
| #define WAKE_EVENT_SIZE |
- Note
- The preprocessor symbol WAKE_EVENT_SIZE has been deprecated. Please use WakeMask instead.
Definition at line
240
of file
micro-common.h
.
| #define WAKE_GPIO_MASK |
Definition at line
229
of file
micro-common.h
.
| #define WAKE_GPIO_SIZE |
Definition at line
230
of file
micro-common.h
.
| #define WAKE_MASK_INVALID |
Definition at line
235
of file
micro-common.h
.
Typedef Documentation
| typedef uint32_t WakeEvents |
Definition at line
231
of file
micro-common.h
.
| typedef uint32_t WakeMask |
Definition at line
232
of file
micro-common.h
.
Enumeration Type Documentation
| enum SleepModes |
Enumerations for the possible microcontroller sleep modes.
- SLEEPMODE_RUNNING Everything is active and running. In practice this mode is not used, but it is defined for completeness of information.
- SLEEPMODE_IDLE Only the CPU is idled. The rest of the chip continues running normally. The chip will wake from any interrupt.
- SLEEPMODE_WAKETIMER The sleep timer clock sources remain running. The RC is always running and the 32kHz XTAL depends on the board header. Wakeup is possible from both GPIO and the sleep timer. System time is maintained. The sleep timer is assumed to be configured properly for wake events.
- SLEEPMODE_MAINTAINTIMER The sleep timer clock sources remain running. The RC is always running and the 32kHz XTAL depends on the board header. Wakeup is possible from only GPIO. System time is maintained. NOTE: This mode is not available on EM2XX chips.
- SLEEPMODE_NOTIMER The sleep timer clock sources (both RC and XTAL) are turned off. Wakeup is possible from only GPIO. System time is lost.
- SLEEPMODE_HIBERNATE This maps to EM4 Hibernate on the EFM32/EFR32 devices. RAM is not retained in SLEEPMODE_HIBERNATE so waking up from this sleepmode will behave like a reset. NOTE: This mode is only available on EFM32/EFR32
| Enumerator | |
|---|---|
| SLEEPMODE_RUNNING | |
| SLEEPMODE_IDLE | |
| SLEEPMODE_WAKETIMER | |
| SLEEPMODE_MAINTAINTIMER | |
| SLEEPMODE_NOTIMER | |
| SLEEPMODE_HIBERNATE | |
| SLEEPMODE_RESERVED | |
| SLEEPMODE_POWERDOWN | |
| SLEEPMODE_POWERSAVE | |
Definition at line
106
of file
micro-common.h
.
Function Documentation
| RTCCRamData halAfterEM4 | ( | void |
|
) |
| void halBeforeEM4 | ( | uint32_t |
duration,
|
| RTCCRamData |
input
|
||
| ) |
| void halCommonDelayMicroseconds | ( | uint16_t |
us
|
) |
Blocks the current thread of execution for the specified amount of time, in microseconds.
The function is implemented with cycle-counted busy loops and is intended to create the short delays required when interfacing with hardware peripherals.
The accuracy of the timing provided by this function is not specified, but a general rule is that when running off of a crystal oscillator it will be within 10us. If the micro is running off of another type of oscillator (e.g. RC) the timing accuracy will potentially be much worse.
- Parameters
-
usThe specified time, in microseconds. Values should be between 1 and 65535 microseconds.
| void halCommonDisableVreg1v8 | ( | void |
|
) |
Disable the 1.8V regulator. This function is to be used when the 1.8V supply is provided externally. Disabling the regulator saves current consumption. Disabling the regulator will cause ADC readings of external signals to be wrong. These exteranl signals include analog sources ADC0 thru ADC5 and VDD_PADS/4.
- Note
- : Only used when DISABLE_INTERNAL_1V8_REGULATOR is defined.
| void halCommonEnableVreg1v8 | ( | void |
|
) |
Enable the 1.8V regulator. Normally the 1.8V regulator is enabled out of reset. This function is only needed if the 1.8V regulator has been disabled and ADC conversions on external signals are needed. These exteranl signals include analog sources ADC0 thru ADC5 and VDD_PADS/4. The state of 1v8 survives deep sleep.
- Note
- : Only used when DISABLE_INTERNAL_1V8_REGULATOR is defined.
| uint16_t halGetExtendedResetInfo | ( | void |
|
) |
Returns the Extended Reset Cause information.
- Returns
- A 16-bit code identifying the base and extended cause of the reset
| PGM_P halGetExtendedResetString | ( | void |
|
) |
Calls halGetExtendedResetInfo() and supplies a string describing the extended cause of the reset. halGetResetString() should also be called to get the string for the base reset cause.
- Application Usage:
- Useful for diagnostic printing of text just after program initialization.
- Returns
- A pointer to a program space string.
| bool halGetRadioHoldOff | ( | void |
|
) |
Returns whether Radio HoldOff has been enabled or not.
- Returns
- true if Radio HoldOff has been enabled, false otherwise.
| uint8_t halGetResetInfo | ( | void |
|
) |
Gets information about what caused the microcontroller to reset.
- Returns
- A code identifying the cause of the reset.
| PGM_P halGetResetString | ( | void |
|
) |
Calls halGetResetInfo() and supplies a string describing it.
- Application Usage:
- Useful for diagnostic printing of text just after program initialization.
- Returns
- A pointer to a program space string.
| void halInit | ( | void |
|
) |
Initializes microcontroller-specific peripherals.
| void halInternalDisableWatchDog | ( | uint8_t |
magicKey
|
) |
Disables the watchdog timer.
- Note
- To prevent the watchdog from being disabled accidentally, a magic key must be provided.
- Parameters
-
magicKeyA value ( MICRO_DISABLE_WATCH_DOG_KEY ) that enables the function.
| void halInternalEnableWatchDog | ( | void |
|
) |
Enables the watchdog timer.
| void halInternalSysReset | ( | uint16_t |
extendedCause
|
) |
Records the specified reset cause then forces a reboot.
| bool halInternalWatchDogEnabled | ( | void |
|
) |
Determines whether the watchdog has been enabled or disabled.
- Returns
- A bool value indicating if the watchdog is current enabled.
| void halPowerDown | ( | void |
|
) |
Powers down microcontroller peripherals and board peripherals.
| void halPowerUp | ( | void |
|
) |
Powers up microcontroller peripherals and board peripherals.
| void halRadioPowerDownHandler | ( | void |
|
) |
Handler called in main context after radio has been powered off.
| void halRadioPowerUpHandler | ( | void |
|
) |
Handler called in main context prior to radio being powered on.
| void halReboot | ( | void |
|
) |
Restarts the microcontroller and therefore everything else.
| void halResume | ( | void |
|
) |
Resumes microcontroller peripherals and board peripherals.
| EmberStatus halSetRadioHoldOff | ( | bool |
enable
|
) |
Enables or disables Radio HoldOff support.
- Parameters
-
enableWhen true, configures ::RHO_GPIO in BOARD_HEADER as an input which, when asserted, will prevent the radio from transmitting. When false, configures ::RHO_GPIO for its original default purpose.
- Returns
- EMBER_SUCCESS if Radio HoldOff was configured as desired or EMBER_BAD_ARGUMENT if requesting it be enabled but RHO has not been configured by the BOARD_HEADER.
| void halSleep | ( | SleepModes |
sleepMode
|
) |
Puts the microcontroller to sleep in a specified mode.
- Note
- This routine always enables interrupts.
- Parameters
-
sleepModeA microcontroller sleep mode
- See also
- SleepModes
| void halSleepPreserveInts | ( | SleepModes |
sleepMode
|
) |
Same as halSleep() except it preserves the current interrupt state rather than always enabling interrupts prior to returning.
- Parameters
-
sleepModeA microcontroller sleep mode
- See also
- SleepModes
| void halStackProcessBootCount | ( | void |
|
) |
Called from emberInit and provides a means for the HAL to increment a boot counter, most commonly in non-volatile memory.
This is useful while debugging to determine the number of resets that might be seen over a period of time. Exposing this functionality allows the application to disable or alter processing of the boot counter if, for example, the application is expecting a lot of resets that could wear out non-volatile storage or some
- EmberStack Usage:
- Called from emberInit only as helpful debugging information. This should be left enabled by default, but this function can also be reduced to a simple return statement if boot counting is not desired.
| void halStackRadio2PowerDownBoard | ( | void |
|
) |
To assist with saving power when radio2 automatically powers down, this function allows the stack to tell the HAL to put pins specific to radio functionality in their powerdown state. The pin state used is the state used by halInternalPowerDownBoard, but applied only to the pins identified in the global variable gpioRadioPowerBoardMask. The stack will automatically call this function as needed, but it will only change GPIO state based on gpioRadioPowerBoardMask. Most commonly, the bits set in gpioRadioPowerBoardMask petain to using a Front End Module. This function is often called from interrupt context.
| void halStackRadio2PowerUpBoard | ( | void |
|
) |
To assist with saving power when radio2 automatically powers up, this function allows the stack to tell the HAL to put pins specific to radio functionality in their powerup state. The pin state used is the state used by halInternalPowerUpBoard, but applied only to the pins identified in the global variable gpioRadioPowerBoardMask. The stack will automatically call this function as needed, but it will only change GPIO state based on gpioRadioPowerBoardMask. Most commonly, the bits set in gpioRadioPowerBoardMask petain to using a Front End Module. This function can be called from interrupt context.
| void halStackRadioPowerDownBoard | ( | void |
|
) |
To assist with saving power when the radio automatically powers down, this function allows the stack to tell the HAL to put pins specific to radio functionality in their powerdown state. The pin state used is the state used by halInternalPowerDownBoard, but applied only to the pins identified in the global variable gpioRadioPowerBoardMask. The stack will automatically call this function as needed, but it will only change GPIO state based on gpioRadioPowerBoardMask. Most commonly, the bits set in gpioRadioPowerBoardMask petain to using a Front End Module. This function is often called from interrupt context.
| void halStackRadioPowerMainControl | ( | bool |
powerUp
|
) |
This function is called automatically by the stack prior to Radio power-up and after Radio power-down. It can be used to prepare for the radio being powered on and to clean up after it's been powered off. Unlike halStackRadioPowerUpBoard() and halStackRadioPowerDownBoard() , which can be called from interrupt context, this function is only called from main-line context.
| void halStackRadioPowerUpBoard | ( | void |
|
) |
To assist with saving power when the radio automatically powers up, this function allows the stack to tell the HAL to put pins specific to radio functionality in their powerup state. The pin state used is the state used by halInternalPowerUpBoard, but applied only to the pins identified in the global variable gpioRadioPowerBoardMask. The stack will automatically call this function as needed, but it will only change GPIO state based on gpioRadioPowerBoardMask. Most commonly, the bits set in gpioRadioPowerBoardMask petain to using a Front End Module. This function can be called from interrupt context.
| void halSuspend | ( | void |
|
) |
Suspends microcontroller peripherals and board peripherals.
Variable Documentation
| volatile int8_t halCommonVreg1v8EnableCount |
Helper variable to track the state of 1.8V regulator.
- Note
- : Only used when DISABLE_INTERNAL_1V8_REGULATOR is defined.