• Reads a sample of the temperature and relative humidity values from the WSTK Si7013 sensors.
More...

Functions

EmberStatus emberAfPluginWstkSensorsGetSample (uint32_t *rhData, int32_t *tData)
  • Reads a sample of the temperature and relative humidity values from the WSTK Si7013 sensors.
Parameters
rhData A pointer to a 32-bit unsigned integer where the relative humidity sample is written.
tData A pointer to a 32-bit signed integer where the temperature is written. Temperature is sampled in "millicelsius".
Returns
An EmberStatus value of EMBER_SUCCESS if the relative humidity and temperature sample were successfully read from the Si7013 sensors. Otherwise, an EmberStatus value of EMBER_ERR_FATAL .

License

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.

See wstk-sensors.h for source code.

Function Documentation

EmberStatus emberAfPluginWstkSensorsGetSample ( uint32_t * rhData,
int32_t * tData
)