GPD Address for sending and receiving a GPDF.
Public Attribute Documentation#
gpdIeeeAddress#
sl_802154_long_addr_t sl_zigbee_gp_address_t::gpdIeeeAddress
The IEEE address is used when the application identifier is SL_ZIGBEE_GP_APPLICATION_IEEE_ADDRESS.
Definition at line
308
of file stack/include/gp-types.h
sourceId#
sl_zigbee_gp_source_id_t sl_zigbee_gp_address_t::sourceId
The 32-bit source identifier is used when the application identifier is SL_ZIGBEE_GP_APPLICATION_SOURCE_ID.
Definition at line
312
of file stack/include/gp-types.h
id#
union sl_zigbee_gp_address_t::@6 sl_zigbee_gp_address_t::id
Definition at line
313
of file stack/include/gp-types.h
applicationId#
sl_zigbee_gp_application_id_t sl_zigbee_gp_address_t::applicationId
Application identifier of the GPD.
Definition at line
315
of file stack/include/gp-types.h
endpoint#
uint8_t sl_zigbee_gp_address_t::endpoint
Application endpoint , only used when application identifier is SL_ZIGBEE_GP_APPLICATION_IEEE_ADDRESS
Definition at line
319
of file stack/include/gp-types.h