Switch Information.

Public Attributes#

Public Attribute Documentation#

currentStatus#

uint8_t sl_zigbee_gp_generic_switch_data_t::currentStatus

provides button information of the Generic switch for the current contacts status


Definition at line 704 of file stack/include/gp-types.h

contactBitmask#

uint8_t sl_zigbee_gp_generic_switch_data_t::contactBitmask

Provides the bitmask to evaluate the received contact. As a result, the bitmask only depends on the number of contacts of the current GPD.


Definition at line 708 of file stack/include/gp-types.h