Additional Information Block Option Record Fields. Provides information regarding the record fields from the linked translation table. Typically, a translation table, which contains the generic switch, multi sensor or the compact attribute reporting GPD, needs to populate the information during commissioning and use it to translate the shorter GPDF to the longer ZCL payload.
Public Attributes#
uint8_t
uint8_t
uint8_t
uint8_t
uint16_t
uint16_t
uint8_t
uint8_t
uint16_t
struct sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9::@10
uint8_t
uint8_t
struct sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9::@11
union sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9
Public Attribute Documentation#
totalLengthOfAddInfoBlock#
uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::totalLengthOfAddInfoBlock
Total Length of the additional information block
Definition at line
719
of file stack/include/gp-types.h
optionSelector#
uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::optionSelector
Option selector
Definition at line
721
of file stack/include/gp-types.h
reportIdentifier#
uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::reportIdentifier
Definition at line
725
of file stack/include/gp-types.h
attrOffsetWithinReport#
uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::attrOffsetWithinReport
Definition at line
726
of file stack/include/gp-types.h
clusterID#
uint16_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::clusterID
Definition at line
727
of file stack/include/gp-types.h
attributeID#
uint16_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::attributeID
Definition at line
728
of file stack/include/gp-types.h
attributeDataType#
uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::attributeDataType
Definition at line
729
of file stack/include/gp-types.h
attributeOptions#
uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::attributeOptions
Definition at line
730
of file stack/include/gp-types.h
manufacturerID#
uint16_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::manufacturerID
Definition at line
731
of file stack/include/gp-types.h
compactAttr#
struct sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9::@10 sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::compactAttr
Compact Attribute Reporting or Multi sensor
Definition at line
732
of file stack/include/gp-types.h
contactStatus#
uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::contactStatus
Provides button information of the Generic switch for contacts status
Definition at line
736
of file stack/include/gp-types.h
contactBitmask#
uint8_t sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::contactBitmask
Provides the bitmask to evaluate the received contact. As a result, the bitmask only depends on the number of contacts of the current GPD.
Definition at line
740
of file stack/include/gp-types.h
genericSwitch#
struct sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9::@11 sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::genericSwitch
Generic switch information
Definition at line
741
of file stack/include/gp-types.h
optionData#
union sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::@9 sl_zigbee_gp_translation_table_additional_info_block_option_record_field_t::optionData
Definition at line
742
of file stack/include/gp-types.h