GP Tx queue entry.
Public Attribute Documentation#
inUse#
bool sl_zigbee_gp_tx_queue_entry_t::inUse
The entry in use
Definition at line
565
of file stack/include/gp-types.h
useCca#
bool sl_zigbee_gp_tx_queue_entry_t::useCca
Use CCA during transmit
Definition at line
567
of file stack/include/gp-types.h
addr#
sl_zigbee_gp_address_t sl_zigbee_gp_tx_queue_entry_t::addr
GP address
Definition at line
569
of file stack/include/gp-types.h
gpdCommandId#
uint8_t sl_zigbee_gp_tx_queue_entry_t::gpdCommandId
GPD Command ID
Definition at line
571
of file stack/include/gp-types.h
gpepHandle#
uint8_t sl_zigbee_gp_tx_queue_entry_t::gpepHandle
Handle for the outgoing message
Definition at line
573
of file stack/include/gp-types.h
queueEntryLifetimeMs#
uint16_t sl_zigbee_gp_tx_queue_entry_t::queueEntryLifetimeMs
Life time in milliseconds for the entry to expire, 0 indicates no expiry
Definition at line
575
of file stack/include/gp-types.h