Application information. During the commissioning of GPD that supports generic switch, multi sensor extension and compact report attribute the application information is exchanged as part of the GPD commissioning command 0xE0 and 0xE4. This structure holds the information for the commissioned GPD.
Public Attributes#
Public Attribute Documentation#
deviceId#
uint8_t sl_zigbee_gp_application_info_t::deviceId
Device ID of the GPD
586
of file stack/include/gp-types.h
applInfoBitmap#
uint8_t sl_zigbee_gp_application_info_t::applInfoBitmap
Application Information bitmap
588
of file stack/include/gp-types.h
manufacturerId#
uint16_t sl_zigbee_gp_application_info_t::manufacturerId
Manufacturer ID of the GPD
590
of file stack/include/gp-types.h
modelId#
uint16_t sl_zigbee_gp_application_info_t::modelId
Model ID of the GPD
592
of file stack/include/gp-types.h
numberOfGpdCommands#
uint8_t sl_zigbee_gp_application_info_t::numberOfGpdCommands
Number of GPD commands supported by the GPD
594
of file stack/include/gp-types.h
gpdCommands#
uint8_t sl_zigbee_gp_application_info_t::gpdCommands[GP_COMMISSIONING_MAX_BYTES - 1]
Supported GPD Commands
596
of file stack/include/gp-types.h
numberOfPairedEndpoints#
uint8_t sl_zigbee_gp_application_info_t::numberOfPairedEndpoints
Number of paired endpoints for the GPD
598
of file stack/include/gp-types.h
pairedEndpoints#
uint8_t sl_zigbee_gp_application_info_t::pairedEndpoints[GP_COMMISSIONING_MAX_BYTES - 1]
Paired endpoints
600
of file stack/include/gp-types.h
numberOfGpdClientCluster#
uint8_t sl_zigbee_gp_application_info_t::numberOfGpdClientCluster
Number of operational client clusters present on the GPD, maximum is 15.
602
of file stack/include/gp-types.h
numberOfGpdServerCluster#
uint8_t sl_zigbee_gp_application_info_t::numberOfGpdServerCluster
Number of operational server clusters present on the GPD, maximum is 15.
604
of file stack/include/gp-types.h
serverClusters#
uint16_t sl_zigbee_gp_application_info_t::serverClusters[15]
Operational server clusters present on the GPD
606
of file stack/include/gp-types.h
clientClusters#
uint16_t sl_zigbee_gp_application_info_t::clientClusters[15]
Operational client clusters present on the GPD
608
of file stack/include/gp-types.h