Data point descriptor. Compact attribute, Multi sensor or Generic switch feature uses this as descriptor to interpret the incoming data from the GPD. This descriptor is set up at the sink during the commissioning.
Public Attribute Documentation#
nbAttrRecord#
uint8_t sl_zigbee_gp_data_point_descriptor_t::nbAttrRecord
Number of attribute records
Definition at line
649
of file stack/include/gp-types.h
clientServer#
uint8_t sl_zigbee_gp_data_point_descriptor_t::clientServer
Client or Server flag
Definition at line
651
of file stack/include/gp-types.h
ManIdPresent#
uint8_t sl_zigbee_gp_data_point_descriptor_t::ManIdPresent
Manufacture ID present
Definition at line
653
of file stack/include/gp-types.h
datapointOptions#
uint8_t sl_zigbee_gp_data_point_descriptor_t::datapointOptions
Data point options
Definition at line
655
of file stack/include/gp-types.h
clusterID#
uint16_t sl_zigbee_gp_data_point_descriptor_t::clusterID
Cluster ID
Definition at line
657
of file stack/include/gp-types.h
manufacturerID#
uint16_t sl_zigbee_gp_data_point_descriptor_t::manufacturerID
Manufacture ID
Definition at line
659
of file stack/include/gp-types.h
attrRecord#
sl_zigbee_gp_attribute_record_t sl_zigbee_gp_data_point_descriptor_t::attrRecord
Attribute Record
Definition at line
661
of file stack/include/gp-types.h