BURTC_Init_TypeDef Struct Reference
BURTC initialization structure for Series 0 devices.
#include <em_burtc.h>
Data Fields | |
bool | enable |
Enable BURTC after initialization (starts counter). | |
BURTC_Mode_TypeDef | mode |
Configure energy mode operation. | |
bool | debugRun |
If true, counter will keep running under debug halt. | |
BURTC_ClkSel_TypeDef | clkSel |
Select clock source. | |
uint32_t | clkDiv |
Clock divider; for ULFRCO 1Khz or 2kHz operation. | |
uint32_t | lowPowerComp |
Number of least significantt clock bits to ignore in low power mode. | |
bool | timeStamp |
Enable time stamp on entering backup power domain. | |
bool | compare0Top |
Set if Compare Value 0 is also top value (counter restart). | |
BURTC_LP_TypeDef | lowPowerMode |
Low power operation mode, requires LFXO or LFRCO. | |
BURTC initialization structure for Series 0 devices.
Field Documentation
◆ enable
bool BURTC_Init_TypeDef::enable |
Enable BURTC after initialization (starts counter).
◆ mode
BURTC_Mode_TypeDef BURTC_Init_TypeDef::mode |
Configure energy mode operation.
◆ debugRun
bool BURTC_Init_TypeDef::debugRun |
If true, counter will keep running under debug halt.
◆ clkSel
BURTC_ClkSel_TypeDef BURTC_Init_TypeDef::clkSel |
Select clock source.
◆ clkDiv
uint32_t BURTC_Init_TypeDef::clkDiv |
Clock divider; for ULFRCO 1Khz or 2kHz operation.
◆ lowPowerComp
uint32_t BURTC_Init_TypeDef::lowPowerComp |
Number of least significantt clock bits to ignore in low power mode.
◆ timeStamp
bool BURTC_Init_TypeDef::timeStamp |
Enable time stamp on entering backup power domain.
◆ compare0Top
bool BURTC_Init_TypeDef::compare0Top |
Set if Compare Value 0 is also top value (counter restart).
◆ lowPowerMode
BURTC_LP_TypeDef BURTC_Init_TypeDef::lowPowerMode |
Low power operation mode, requires LFXO or LFRCO.