LESENSE_CoreCtrlDesc_TypeDef Struct Reference
Core control (LESENSE_CTRL) descriptor structure.
#include <em_lesense.h>
Data Fields |
|
| LESENSE_ScanMode_TypeDef | scanStart |
|
Select scan start mode to control how the scan start is being triggered.
|
|
| LESENSE_PRSSel_TypeDef | prsSel |
|
Select PRS source for scan start if scanMode is set to lesensePrsPulse.
|
|
| LESENSE_ScanConfSel_TypeDef | scanConfSel |
|
Select scan configuration register usage strategy.
|
|
| bool | invACMP0 |
|
Set to true to invert ACMP0 output.
|
|
| bool | invACMP1 |
|
Set to true to invert ACMP1 output.
|
|
| bool | dualSample |
|
Set to true to sample both ACMPs simultaneously.
|
|
| bool | storeScanRes |
|
Set to true in order to store SCANRES in the RAM (accessible via RESDATA) after each scan.
|
|
| bool | bufOverWr |
|
Set to true in order to always make LESENSE write to the result buffer, even if it is full.
|
|
| LESENSE_BufTrigLevel_TypeDef | bufTrigLevel |
|
Select trigger conditions for the interrupt and DMA.
|
|
| LESENSE_DMAWakeUp_TypeDef | wakeupOnDMA |
|
Configure trigger condition for the DMA wakeup from EM2.
|
|
| LESENSE_BiasMode_TypeDef | biasMode |
|
Select bias mode.
|
|
| bool | debugRun |
|
Set to true to keep LESENSE running in the debug mode.
|
|
Core control (LESENSE_CTRL) descriptor structure.
Field Documentation
◆ scanStart
| LESENSE_ScanMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanStart |
Select scan start mode to control how the scan start is being triggered.
◆ prsSel
| LESENSE_PRSSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::prsSel |
Select PRS source for scan start if scanMode is set to lesensePrsPulse.
◆ scanConfSel
| LESENSE_ScanConfSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanConfSel |
Select scan configuration register usage strategy.
◆ invACMP0
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP0 |
Set to true to invert ACMP0 output.
◆ invACMP1
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP1 |
Set to true to invert ACMP1 output.
◆ dualSample
| bool LESENSE_CoreCtrlDesc_TypeDef::dualSample |
Set to true to sample both ACMPs simultaneously.
◆ storeScanRes
| bool LESENSE_CoreCtrlDesc_TypeDef::storeScanRes |
Set to true in order to store SCANRES in the RAM (accessible via RESDATA) after each scan.
◆ bufOverWr
| bool LESENSE_CoreCtrlDesc_TypeDef::bufOverWr |
Set to true in order to always make LESENSE write to the result buffer, even if it is full.
◆ bufTrigLevel
| LESENSE_BufTrigLevel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::bufTrigLevel |
Select trigger conditions for the interrupt and DMA.
◆ wakeupOnDMA
| LESENSE_DMAWakeUp_TypeDef LESENSE_CoreCtrlDesc_TypeDef::wakeupOnDMA |
Configure trigger condition for the DMA wakeup from EM2.
◆ biasMode
| LESENSE_BiasMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::biasMode |
Select bias mode.
◆ debugRun
| bool LESENSE_CoreCtrlDesc_TypeDef::debugRun |
Set to true to keep LESENSE running in the debug mode.