WDOG_Init_TypeDef Struct Reference
Watchdog initialization structure.
#include <em_wdog.h>
Data Fields | |
| bool | enable |
| Enable watchdog when initialization completed. | |
| bool | debugRun |
| Counter keeps running during debug halt. | |
| bool | em2Run |
| Counter keeps running when in EM2. | |
| bool | em3Run |
| Counter keeps running when in EM3. | |
| bool | em4Block |
| Block EMU from entering EM4. | |
| bool | swoscBlock |
| Block SW from disabling LFRCO/LFXO oscillators. | |
| bool | lock |
| Block SW from modifying the configuration (a reset is needed to reconfigure). | |
| WDOG_ClkSel_TypeDef | clkSel |
| Clock source to use for watchdog. | |
| WDOG_PeriodSel_TypeDef | perSel |
| Watchdog timeout period. | |
| WDOG_WarnSel_TypeDef | warnSel |
| Select warning time as % of the watchdog timeout. | |
| WDOG_WinSel_TypeDef | winSel |
| Select illegal window time as % of the watchdog timeout. | |
| bool | resetDisable |
| Disable watchdog reset output if true. | |
Watchdog initialization structure.
Field Documentation
◆ enable
| bool WDOG_Init_TypeDef::enable |
Enable watchdog when initialization completed.
◆ debugRun
| bool WDOG_Init_TypeDef::debugRun |
Counter keeps running during debug halt.
◆ em2Run
| bool WDOG_Init_TypeDef::em2Run |
Counter keeps running when in EM2.
◆ em3Run
| bool WDOG_Init_TypeDef::em3Run |
Counter keeps running when in EM3.
◆ em4Block
| bool WDOG_Init_TypeDef::em4Block |
Block EMU from entering EM4.
◆ swoscBlock
| bool WDOG_Init_TypeDef::swoscBlock |
Block SW from disabling LFRCO/LFXO oscillators.
◆ lock
| bool WDOG_Init_TypeDef::lock |
Block SW from modifying the configuration (a reset is needed to reconfigure).
◆ clkSel
| WDOG_ClkSel_TypeDef WDOG_Init_TypeDef::clkSel |
Clock source to use for watchdog.
◆ perSel
| WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel |
Watchdog timeout period.
◆ warnSel
| WDOG_WarnSel_TypeDef WDOG_Init_TypeDef::warnSel |
Select warning time as % of the watchdog timeout.
◆ winSel
| WDOG_WinSel_TypeDef WDOG_Init_TypeDef::winSel |
Select illegal window time as % of the watchdog timeout.
◆ resetDisable
| bool WDOG_Init_TypeDef::resetDisable |
Disable watchdog reset output if true.