ACMP_VBConfig_TypeDef Struct Reference
VB Configuration structure.
#include <em_acmp.h>
Data Fields |
|
ACMP_VBInput_TypeDef | input |
VB Voltage input source.
|
|
uint32_t | div0 |
A divider for VB voltage input source when ACMP output is 0.
|
|
uint32_t | div1 |
A divider for VB voltage input source when ACMP output is 1.
|
|
VB Configuration structure.
This structure is used to configure the VB voltage input source and its dividers.
Field Documentation
◆ input
ACMP_VBInput_TypeDef ACMP_VBConfig_TypeDef::input |
VB Voltage input source.
◆ div0
uint32_t ACMP_VBConfig_TypeDef::div0 |
A divider for VB voltage input source when ACMP output is 0.
This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.
VB divided = VB input * (div0 + 1) / 64
◆ div1
uint32_t ACMP_VBConfig_TypeDef::div1 |
A divider for VB voltage input source when ACMP output is 1.
This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.
VB divided = VB input * (div1 + 1) / 64