OPAMP_Init_TypeDef Struct Reference
OPAMP init structure.
#include <em_opamp.h>
Data Fields |
|
OPAMP_NegSel_TypeDef | negSel |
Select input source for negative terminal.
|
|
OPAMP_PosSel_TypeDef | posSel |
Select input source for positive terminal.
|
|
OPAMP_OutMode_TypeDef | outMode |
Output terminal connection.
|
|
OPAMP_ResSel_TypeDef | resSel |
Select R2/R1 resistor ratio.
|
|
OPAMP_ResInMux_TypeDef | resInMux |
Select input source for resistor ladder.
|
|
uint32_t | outPen |
Alternate output enable bit mask.
|
|
OPAMP_DrvStr_Typedef | drvStr |
OPAx operation mode.
|
|
bool | gain3xEn |
Enable 3x gain resistor ladder.
|
|
bool | halfDrvStr |
Half or full output drive strength.
|
|
bool | ugBwScale |
Unity gain bandwidth scaled by factor of 2.5.
|
|
bool | prsEn |
Enable PRS as OPAMP trigger.
|
|
OPAMP_PrsMode_TypeDef | prsMode |
Selects PRS trigger mode.
|
|
OPAMP_PrsSel_TypeDef | prsSel |
PRS channel trigger select.
|
|
OPAMP_PrsOut_TypeDef | prsOutSel |
PRS output select.
|
|
bool | aportYMasterDisable |
Disable bus master request on APORT Y.
|
|
bool | aportXMasterDisable |
Disable bus master request on APORT X.
|
|
uint32_t | settleTime |
Number of clock cycles to drive the output.
|
|
uint32_t | startupDly |
OPAx startup delay in microseconds.
|
|
bool | hcmDisable |
Disable input rail-to-rail capability.
|
|
bool | defaultOffsetN |
Use factory calibrated opamp inverting input offset value.
|
|
uint32_t | offsetN |
Opamp inverting input offset value when
defaultOffsetN
is false.
|
|
bool | defaultOffsetP |
Use factory calibrated opamp non-inverting input offset value.
|
|
uint32_t | offsetP |
Opamp non-inverting input offset value when
defaultOffsetP
is false.
|
|
OPAMP init structure.
Field Documentation
◆ negSel
OPAMP_NegSel_TypeDef OPAMP_Init_TypeDef::negSel |
Select input source for negative terminal.
◆ posSel
OPAMP_PosSel_TypeDef OPAMP_Init_TypeDef::posSel |
Select input source for positive terminal.
◆ outMode
OPAMP_OutMode_TypeDef OPAMP_Init_TypeDef::outMode |
Output terminal connection.
◆ resSel
OPAMP_ResSel_TypeDef OPAMP_Init_TypeDef::resSel |
Select R2/R1 resistor ratio.
◆ resInMux
OPAMP_ResInMux_TypeDef OPAMP_Init_TypeDef::resInMux |
Select input source for resistor ladder.
◆ outPen
uint32_t OPAMP_Init_TypeDef::outPen |
Alternate output enable bit mask.
This value should consist one or more of the VDAC_OPA_OUT_ALTOUTPADEN_OUT[output#] flags (defined in <part_name>_vdac.h) OR'ed together.
- VDAC_OPA_OUT_ALTOUTPADEN_OUT0
- VDAC_OPA_OUT_ALTOUTPADEN_OUT1
- VDAC_OPA_OUT_ALTOUTPADEN_OUT2
- VDAC_OPA_OUT_ALTOUTPADEN_OUT3
- VDAC_OPA_OUT_ALTOUTPADEN_OUT4
E.g:
init.outPen = VDAC_OPA_OUT_ALTOUTPADEN_OUT0 | VDAC_OPA_OUT_ALTOUTPADEN_OUT2 | VDAC_OPA_OUT_ALTOUTPADEN_OUT4;
◆ drvStr
OPAMP_DrvStr_Typedef OPAMP_Init_TypeDef::drvStr |
OPAx operation mode.
◆ gain3xEn
bool OPAMP_Init_TypeDef::gain3xEn |
Enable 3x gain resistor ladder.
◆ halfDrvStr
bool OPAMP_Init_TypeDef::halfDrvStr |
Half or full output drive strength.
◆ ugBwScale
bool OPAMP_Init_TypeDef::ugBwScale |
Unity gain bandwidth scaled by factor of 2.5.
◆ prsEn
bool OPAMP_Init_TypeDef::prsEn |
Enable PRS as OPAMP trigger.
◆ prsMode
OPAMP_PrsMode_TypeDef OPAMP_Init_TypeDef::prsMode |
Selects PRS trigger mode.
◆ prsSel
OPAMP_PrsSel_TypeDef OPAMP_Init_TypeDef::prsSel |
PRS channel trigger select.
◆ prsOutSel
OPAMP_PrsOut_TypeDef OPAMP_Init_TypeDef::prsOutSel |
PRS output select.
◆ aportYMasterDisable
bool OPAMP_Init_TypeDef::aportYMasterDisable |
Disable bus master request on APORT Y.
◆ aportXMasterDisable
bool OPAMP_Init_TypeDef::aportXMasterDisable |
Disable bus master request on APORT X.
◆ settleTime
uint32_t OPAMP_Init_TypeDef::settleTime |
Number of clock cycles to drive the output.
◆ startupDly
uint32_t OPAMP_Init_TypeDef::startupDly |
OPAx startup delay in microseconds.
◆ hcmDisable
bool OPAMP_Init_TypeDef::hcmDisable |
Disable input rail-to-rail capability.
◆ defaultOffsetN
bool OPAMP_Init_TypeDef::defaultOffsetN |
Use factory calibrated opamp inverting input offset value.
◆ offsetN
uint32_t OPAMP_Init_TypeDef::offsetN |
Opamp inverting input offset value when defaultOffsetN is false.
◆ defaultOffsetP
bool OPAMP_Init_TypeDef::defaultOffsetP |
Use factory calibrated opamp non-inverting input offset value.
◆ offsetP
uint32_t OPAMP_Init_TypeDef::offsetP |
Opamp non-inverting input offset value when defaultOffsetP is false.