DMA_CB_TypeDef Struct Reference
Callback structure that can be used to define DMA complete actions.
#include <em_dma.h>
Data Fields | |
DMA_FuncPtr_TypeDef | cbFunc |
Pointer to callback function to invoke when DMA transfer cycle is done. | |
void * | userPtr |
User defined pointer to provide with callback function. | |
uint8_t | primary |
For internal use only: Indicates if next callback applies to primary or alternate descriptor completion. | |
Callback structure that can be used to define DMA complete actions.
A reference to this structure is only stored in the primary descriptor for a channel (if using callback feature). If callback is required for both primary and alternate descriptor completion, this must be handled by one common callback, using the provided 'primary' parameter with the callback function.
Field Documentation
◆ cbFunc
DMA_FuncPtr_TypeDef DMA_CB_TypeDef::cbFunc |
Pointer to callback function to invoke when DMA transfer cycle is done.
Notice that this function is invoked in interrupt context, and therefore should be short and non-blocking.
◆ userPtr
void* DMA_CB_TypeDef::userPtr |
User defined pointer to provide with callback function.
◆ primary
uint8_t DMA_CB_TypeDef::primary |
For internal use only: Indicates if next callback applies to primary or alternate descriptor completion.
Mainly useful for ping-pong DMA cycles. Set this value to 0 prior to configuring callback handling.