ADC_InitScan_TypeDef Struct Reference
Scan sequence initialization structure.
#include <em_adc.h>
Data Fields |
|
ADC_PRSSEL_TypeDef | prsSel |
Peripheral reflex system trigger selection.
|
|
ADC_AcqTime_TypeDef | acqTime |
Acquisition time (in ADC clock cycles).
|
|
ADC_Ref_TypeDef | reference |
Sample reference selection.
|
|
ADC_Res_TypeDef | resolution |
Sample resolution.
|
|
uint32_t | input |
Scan input selection.
|
|
bool | diff |
Select if single-ended or differential input.
|
|
bool | prsEnable |
Peripheral reflex system trigger enable.
|
|
bool | leftAdjust |
Select if left adjustment should be done.
|
|
bool | rep |
Select if continuous conversion until explicit stop.
|
|
Scan sequence initialization structure.
Field Documentation
◆ prsSel
ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel |
Peripheral reflex system trigger selection.
Only applicable if
prsEnable
is enabled.
◆ acqTime
ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
◆ reference
ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference |
Sample reference selection.
Note that, for external references, the ADC calibration register must be set explicitly.
◆ resolution
ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution |
Sample resolution.
◆ input
uint32_t ADC_InitScan_TypeDef::input |
Scan input selection.
If single ended (
diff
is false), use logical combination of ADC_SCANCTRL_INPUTMASK_CHx defines. If differential input (
diff
is true), use logical combination of ADC_SCANCTRL_INPUTMASK_CHxCHy defines. (Notice underscore prefix for defines used.)
◆ diff
bool ADC_InitScan_TypeDef::diff |
Select if single-ended or differential input.
◆ prsEnable
bool ADC_InitScan_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
◆ leftAdjust
bool ADC_InitScan_TypeDef::leftAdjust |
Select if left adjustment should be done.
◆ rep
bool ADC_InitScan_TypeDef::rep |
Select if continuous conversion until explicit stop.