DMA_CB_TypeDef Struct Reference

Callback structure that can be used to define DMA complete actions.

#include <em_dma.h>

Data Fields

DMA_FuncPtr_TypeDef cbFunc
Pointer to callback function to invoke when DMA transfer cycle is done.
void * userPtr
User defined pointer to provide with callback function.
uint8_t primary
For internal use only: Indicates if next callback applies to primary or alternate descriptor completion.

Callback structure that can be used to define DMA complete actions.

A reference to this structure is only stored in the primary descriptor for a channel (if using callback feature). If callback is required for both primary and alternate descriptor completion, this must be handled by one common callback, using the provided 'primary' parameter with the callback function.

Field Documentation

◆ cbFunc

DMA_FuncPtr_TypeDef DMA_CB_TypeDef::cbFunc

Pointer to callback function to invoke when DMA transfer cycle is done.

Notice that this function is invoked in interrupt context, and therefore should be short and non-blocking.

◆ userPtr

void* DMA_CB_TypeDef::userPtr

User defined pointer to provide with callback function.

◆ primary

uint8_t DMA_CB_TypeDef::primary

For internal use only: Indicates if next callback applies to primary or alternate descriptor completion.

Mainly useful for ping-pong DMA cycles. Set this value to 0 prior to configuring callback handling.