RTCC_Init_TypeDef Struct Reference
RTCC initialization structure.
      
       #include <em_rtcc.h>
      
     
         Data Fields | 
       |
| bool | enable | 
| 
         Enable/disable counting when initialization is completed.
          | 
       |
| bool | debugRun | 
| 
         Enable/disable timer counting during debug halt.
          | 
       |
| bool | precntWrapOnCCV0 | 
| 
         Enable/disable pre-counter wrap on ch.
          | 
       |
| bool | cntWrapOnCCV1 | 
| 
         Enable/disable counter wrap on ch.
          | 
       |
| RTCC_CntPresc_TypeDef | presc | 
| 
         Counter prescaler.
          | 
       |
| RTCC_PrescMode_TypeDef | prescMode | 
| 
         Prescaler mode.
          | 
       |
| bool | enaOSCFailDetect | 
| 
         Enable/disable the check that sets OSCFFAIL interrupt flag if no LFCLK-RTCC ticks are detected within one ULFRCO cycles.
          | 
       |
| RTCC_CntMode_TypeDef | cntMode | 
| 
         Select operational mode of the counter.
          | 
       |
| bool | disLeapYearCorr | 
| 
         Disable leap year correction for calendar mode.
          | 
       |
RTCC initialization structure.
Field Documentation
◆ enable
| bool RTCC_Init_TypeDef::enable | 
Enable/disable counting when initialization is completed.
◆ debugRun
| bool RTCC_Init_TypeDef::debugRun | 
Enable/disable timer counting during debug halt.
◆ precntWrapOnCCV0
| bool RTCC_Init_TypeDef::precntWrapOnCCV0 | 
Enable/disable pre-counter wrap on ch.
0 CCV value.
◆ cntWrapOnCCV1
| bool RTCC_Init_TypeDef::cntWrapOnCCV1 | 
Enable/disable counter wrap on ch.
1 CCV value.
◆ presc
| RTCC_CntPresc_TypeDef RTCC_Init_TypeDef::presc | 
Counter prescaler.
◆ prescMode
| RTCC_PrescMode_TypeDef RTCC_Init_TypeDef::prescMode | 
Prescaler mode.
◆ enaOSCFailDetect
| bool RTCC_Init_TypeDef::enaOSCFailDetect | 
Enable/disable the check that sets OSCFFAIL interrupt flag if no LFCLK-RTCC ticks are detected within one ULFRCO cycles.
◆ cntMode
| RTCC_CntMode_TypeDef RTCC_Init_TypeDef::cntMode | 
Select operational mode of the counter.
◆ disLeapYearCorr
| bool RTCC_Init_TypeDef::disLeapYearCorr | 
Disable leap year correction for calendar mode.
When this parameter is set to false, February has 29 days if (year % 4 == 0). If set to true, February always has 28 days.