TIMER_InitDTI_TypeDef Struct Reference
TIMER Dead Time Insertion (DTI) initialization structure.
#include <em_timer.h>
Data Fields | |
bool | enable |
Enable DTI or leave it disabled until TIMER_EnableDTI() is called. | |
bool | activeLowOut |
DTI Output Polarity. | |
bool | invertComplementaryOut |
DTI Complementary Output Invert. | |
bool | autoRestart |
Enable Automatic Start-up functionality (when debugger exits). | |
bool | enablePrsSource |
Enable/disable PRS as DTI input. | |
TIMER_PRSSEL_TypeDef | prsSel |
Select which PRS channel as DTI input. | |
TIMER_Prescale_TypeDef | prescale |
DTI prescaling factor, if HFPER / HFPERB clock used. | |
unsigned int | riseTime |
DTI Rise Time. | |
unsigned int | fallTime |
DTI Fall Time. | |
uint32_t | outputsEnableMask |
DTI outputs enable bit mask, consisting of one bit per DTI output signal, i.e., CC0, CC1, CC2, CDTI0, CDTI1, and CDTI2. | |
bool | enableFaultSourceCoreLockup |
Enable core lockup as a fault source. | |
bool | enableFaultSourceDebugger |
Enable debugger as a fault source. | |
bool | enableFaultSourcePrsSel0 |
Enable PRS fault source 0 (faultSourcePrsSel0 ). | |
TIMER_PRSSEL_TypeDef | faultSourcePrsSel0 |
Select which PRS signal to be PRS fault source 0. | |
bool | enableFaultSourcePrsSel1 |
Enable PRS fault source 1 (faultSourcePrsSel1 ). | |
TIMER_PRSSEL_TypeDef | faultSourcePrsSel1 |
Select which PRS signal to be PRS fault source 1. | |
TIMER_DtiFaultAction_TypeDef | faultAction |
Fault Action. | |
TIMER Dead Time Insertion (DTI) initialization structure.
Field Documentation
◆ enable
bool TIMER_InitDTI_TypeDef::enable |
Enable DTI or leave it disabled until TIMER_EnableDTI() is called.
◆ activeLowOut
bool TIMER_InitDTI_TypeDef::activeLowOut |
DTI Output Polarity.
◆ invertComplementaryOut
bool TIMER_InitDTI_TypeDef::invertComplementaryOut |
DTI Complementary Output Invert.
◆ autoRestart
bool TIMER_InitDTI_TypeDef::autoRestart |
Enable Automatic Start-up functionality (when debugger exits).
◆ enablePrsSource
bool TIMER_InitDTI_TypeDef::enablePrsSource |
Enable/disable PRS as DTI input.
◆ prsSel
TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::prsSel |
Select which PRS channel as DTI input.
Only valid if enablePrsSource
is enabled.
◆ prescale
TIMER_Prescale_TypeDef TIMER_InitDTI_TypeDef::prescale |
DTI prescaling factor, if HFPER / HFPERB clock used.
◆ riseTime
unsigned int TIMER_InitDTI_TypeDef::riseTime |
DTI Rise Time.
◆ fallTime
unsigned int TIMER_InitDTI_TypeDef::fallTime |
DTI Fall Time.
◆ outputsEnableMask
uint32_t TIMER_InitDTI_TypeDef::outputsEnableMask |
DTI outputs enable bit mask, consisting of one bit per DTI output signal, i.e., CC0, CC1, CC2, CDTI0, CDTI1, and CDTI2.
This value should consist of one or more TIMER_DTOGEN_DTOGnnnEN flags (defined in <part_name>_timer.h) OR'ed together.
◆ enableFaultSourceCoreLockup
bool TIMER_InitDTI_TypeDef::enableFaultSourceCoreLockup |
Enable core lockup as a fault source.
◆ enableFaultSourceDebugger
bool TIMER_InitDTI_TypeDef::enableFaultSourceDebugger |
Enable debugger as a fault source.
◆ enableFaultSourcePrsSel0
bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel0 |
Enable PRS fault source 0 (faultSourcePrsSel0
).
◆ faultSourcePrsSel0
TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel0 |
Select which PRS signal to be PRS fault source 0.
◆ enableFaultSourcePrsSel1
bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel1 |
Enable PRS fault source 1 (faultSourcePrsSel1
).
◆ faultSourcePrsSel1
TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel1 |
Select which PRS signal to be PRS fault source 1.
◆ faultAction
TIMER_DtiFaultAction_TypeDef TIMER_InitDTI_TypeDef::faultAction |
Fault Action.