VDAC_InitChannel_TypeDef Struct Reference
VDAC channel initialization structure.
#include <em_vdac.h>
Data Fields | |
bool | enable |
Enable channel. | |
VDAC_PrsSel_TypeDef | prsSel |
Peripheral reflex system trigger selection. | |
bool | prsAsync |
Treat the PRS signal asynchronously. | |
VDAC_TrigMode_TypeDef | trigMode |
Channel conversion trigger mode. | |
bool | sampleOffMode |
Set channel conversion mode to sample/shut-off mode. | |
VDAC channel initialization structure.
Field Documentation
◆ enable
bool VDAC_InitChannel_TypeDef::enable |
Enable channel.
◆ prsSel
VDAC_PrsSel_TypeDef VDAC_InitChannel_TypeDef::prsSel |
Peripheral reflex system trigger selection.
Only applicable if trigMode
is set to vdacTrigModePrs
or vdacTrigModeSwPrs
.
◆ prsAsync
bool VDAC_InitChannel_TypeDef::prsAsync |
Treat the PRS signal asynchronously.
◆ trigMode
VDAC_TrigMode_TypeDef VDAC_InitChannel_TypeDef::trigMode |
Channel conversion trigger mode.
◆ sampleOffMode
bool VDAC_InitChannel_TypeDef::sampleOffMode |
Set channel conversion mode to sample/shut-off mode.
Default is continuous.