CMU_LFXOInit_TypeDef Struct Reference
LFXO initialization structure.
      
       #include <em_cmu.h>
      
     
| Data Fields | |
| uint8_t | ctune | 
| CTUNE (load capacitance) value. | |
| uint8_t | gain | 
| Gain/max startup margin. | |
| uint8_t | timeout | 
| Startup delay. | |
| CMU_OscMode_TypeDef | mode | 
| Oscillator mode. | |
LFXO initialization structure.
       Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
       
      
Field Documentation
◆ ctune
| uint8_t CMU_LFXOInit_TypeDef::ctune | 
CTUNE (load capacitance) value.
◆ gain
| uint8_t CMU_LFXOInit_TypeDef::gain | 
Gain/max startup margin.
◆ timeout
| uint8_t CMU_LFXOInit_TypeDef::timeout | 
Startup delay.
◆ mode
| CMU_OscMode_TypeDef CMU_LFXOInit_TypeDef::mode | 
Oscillator mode.