IADC_SingleInput_t Struct Reference

IADC single input selection structure.

#include <em_iadc.h>

Data Fields

IADC_NegInput_t negInput
 Port/pin input for the negative side of the ADC.
 
IADC_PosInput_t posInput
 Port/pin input for the positive side of the ADC.
 
uint8_t configId
 Configuration id.
 
bool compare
 Perform digital window comparison on the result from this entry.
 

IADC single input selection structure.

Field Documentation

◆ negInput

IADC_NegInput_t IADC_SingleInput_t::negInput

Port/pin input for the negative side of the ADC.


◆ posInput

IADC_PosInput_t IADC_SingleInput_t::posInput

Port/pin input for the positive side of the ADC.


◆ configId

uint8_t IADC_SingleInput_t::configId

Configuration id.

◆ compare

bool IADC_SingleInput_t::compare

Perform digital window comparison on the result from this entry.