SE_Command_t Struct Reference

SE Command structure to which all commands to the SE must adhere.

#include <em_se.h>

Data Fields

uint32_t command
 SE Command.
 
SE_DataTransfer_tdata_in
 Input data.
 
SE_DataTransfer_tdata_out
 Output data.
 
uint32_t parameters [SE_MAX_PARAMETERS]
 Parameters.
 
size_t num_parameters
 Number of parameters.
 

SE Command structure to which all commands to the SE must adhere.

Field Documentation

◆ command

uint32_t SE_Command_t::command

SE Command.

◆ data_in

SE_DataTransfer_t* SE_Command_t::data_in

Input data.

◆ data_out

SE_DataTransfer_t* SE_Command_t::data_out

Output data.

◆ parameters

uint32_t SE_Command_t::parameters[SE_MAX_PARAMETERS]

Parameters.

◆ num_parameters

size_t SE_Command_t::num_parameters

Number of parameters.