QSPI_DelayConfig_TypeDef Struct Reference
QSPI Device Delay Configuration Structure.
      
       #include <em_qspi.h>
      
     
| Data Fields | |
| uint8_t | deassert | 
| The minimal delay to keep the chip select line de-asserted between two transactions. | |
| uint8_t | deviceSwitch | 
| Delay between one chip select being de-activated and the activation of another. | |
| uint8_t | lastBit | 
| Delay between last bit and chip select de-assert. | |
| uint8_t | firstBit | 
| Delay chip select assert and first bit in a transaction. | |
QSPI Device Delay Configuration Structure.
Field Documentation
◆ deassert
| uint8_t QSPI_DelayConfig_TypeDef::deassert | 
The minimal delay to keep the chip select line de-asserted between two transactions.
◆ deviceSwitch
| uint8_t QSPI_DelayConfig_TypeDef::deviceSwitch | 
Delay between one chip select being de-activated and the activation of another.
◆ lastBit
| uint8_t QSPI_DelayConfig_TypeDef::lastBit | 
Delay between last bit and chip select de-assert.
◆ firstBit
| uint8_t QSPI_DelayConfig_TypeDef::firstBit | 
Delay chip select assert and first bit in a transaction.