VDAC_InitChannel_TypeDef Struct Reference
VDAC channel initialization structure.
      
       #include <em_vdac.h>
      
     
| Data Fields | |
| bool | enable | 
| Enable channel. | |
| VDAC_PrsSel_TypeDef | prsSel | 
| Peripheral reflex system trigger selection. | |
| bool | prsAsync | 
| Treat the PRS signal asynchronously. | |
| VDAC_TrigMode_TypeDef | trigMode | 
| Channel conversion trigger mode. | |
| bool | sampleOffMode | 
| Set channel conversion mode to sample/shut-off mode. | |
VDAC channel initialization structure.
Field Documentation
◆ enable
| bool VDAC_InitChannel_TypeDef::enable | 
Enable channel.
◆ prsSel
| VDAC_PrsSel_TypeDef VDAC_InitChannel_TypeDef::prsSel | 
Peripheral reflex system trigger selection.
        Only applicable if
        
         trigMode
        
        is set to
        
         vdacTrigModePrs
        
        or
        
         vdacTrigModeSwPrs
        
        .
       
◆ prsAsync
| bool VDAC_InitChannel_TypeDef::prsAsync | 
Treat the PRS signal asynchronously.
◆ trigMode
| VDAC_TrigMode_TypeDef VDAC_InitChannel_TypeDef::trigMode | 
Channel conversion trigger mode.
◆ sampleOffMode
| bool VDAC_InitChannel_TypeDef::sampleOffMode | 
Set channel conversion mode to sample/shut-off mode.
Default is continuous.