QSPI_Init_TypeDef Struct Reference
QSPI initialization structure.
      
       #include <em_qspi.h>
      
     
| Data Fields | |
| bool | enable | 
| Enable/disable Quad SPI when initialization is completed. | |
| uint8_t | divisor | 
| Master mode baud rate divisor. | |
QSPI initialization structure.
Field Documentation
◆ enable
| bool QSPI_Init_TypeDef::enable | 
Enable/disable Quad SPI when initialization is completed.
◆ divisor
| uint8_t QSPI_Init_TypeDef::divisor | 
Master mode baud rate divisor.
Values can be even numbers in the range [2-32] inclusive.