ACMP_CapsenseInit_TypeDef Struct Reference
Capsense initialization structure.
      
       #include <em_acmp.h>
      
     
| Data Fields | |
| uint32_t | biasProg | 
| Bias current. | |
| ACMP_HysteresisLevel_TypeDef | hysteresisLevel | 
| Hysteresis level. | |
| ACMP_CapsenseResistor_TypeDef | resistor | 
| A resistor used in the capacitive sensing circuit. | |
| uint32_t | vrefDiv | 
| VDD division factor. | |
| bool | enable | 
| If true, ACMP is enabled after configuration. | |
Capsense initialization structure.
Field Documentation
◆ biasProg
| uint32_t ACMP_CapsenseInit_TypeDef::biasProg | 
Bias current.
See the ACMP chapter about bias and response time in the reference manual for details.
◆ hysteresisLevel
| ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel | 
Hysteresis level.
◆ resistor
| ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor | 
A resistor used in the capacitive sensing circuit.
For values see the device data sheet.
◆ vrefDiv
| uint32_t ACMP_CapsenseInit_TypeDef::vrefDiv | 
VDD division factor.
VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.
◆ enable
| bool ACMP_CapsenseInit_TypeDef::enable | 
If true, ACMP is enabled after configuration.