LESENSE_ConfAltEx_TypeDef Struct Reference
Configuration structure for the alternate excitation.
      
       #include <em_lesense.h>
      
     
| Data Fields | |
| LESENSE_AltExDesc_TypeDef | AltEx [16] | 
| Alternate excitation channel descriptors. | |
Configuration structure for the alternate excitation.
Field Documentation
◆ AltEx
| LESENSE_AltExDesc_TypeDef LESENSE_ConfAltEx_TypeDef::AltEx[16] | 
Alternate excitation channel descriptors.
When altExMap==lesenseAltExMapALTEX, only the 8 first descriptors are used. In this mode they describe the configuration of LES_ALTEX0-7 pins. When altExMap==lesenseAltExMapACMP, all 16 descriptors are used. In this mode they describe the configuration of the 16 possible ACMP0-1 excitation channels. Please refer to the user manual for a complete mapping of routing. NOTE: Some parameters in the descriptors are not valid when altExMap==lesenseAltExMapACMP. Refer to the definition of the LESENSE_AltExDesc_TypeDef structure for details regarding which parameters are valid.