EMU_DCDCInit_TypeDef Struct Reference
DCDC regulator initialization structure.
      
       #include <em_emu.h>
      
     
| Data Fields | |
| EMU_DcdcMode_TypeDef | mode | 
| DCDC mode. | |
| EMU_VreginCmpThreshold_TypeDef | cmpThreshold | 
| VREGIN comparator threshold. | |
| EMU_DcdcTonMaxTimeout_TypeDef | tonMax | 
| Ton max timeout control. | |
| EMU_DcdcDriveSpeed_TypeDef | driveSpeedEM01 | 
| DCDC drive speed in EM0/1. | |
| EMU_DcdcDriveSpeed_TypeDef | driveSpeedEM23 | 
| DCDC drive speed in EM2/3. | |
| EMU_DcdcPeakCurrent_TypeDef | peakCurrentEM01 | 
| EM0/1 peak current setting. | |
| EMU_DcdcPeakCurrent_TypeDef | peakCurrentEM23 | 
| EM2/3 peak current setting. | |
DCDC regulator initialization structure.
Field Documentation
◆ mode
| EMU_DcdcMode_TypeDef EMU_DCDCInit_TypeDef::mode | 
DCDC mode.
◆ cmpThreshold
| EMU_VreginCmpThreshold_TypeDef EMU_DCDCInit_TypeDef::cmpThreshold | 
VREGIN comparator threshold.
◆ tonMax
| EMU_DcdcTonMaxTimeout_TypeDef EMU_DCDCInit_TypeDef::tonMax | 
Ton max timeout control.
◆ driveSpeedEM01
| EMU_DcdcDriveSpeed_TypeDef EMU_DCDCInit_TypeDef::driveSpeedEM01 | 
DCDC drive speed in EM0/1.
◆ driveSpeedEM23
| EMU_DcdcDriveSpeed_TypeDef EMU_DCDCInit_TypeDef::driveSpeedEM23 | 
DCDC drive speed in EM2/3.
◆ peakCurrentEM01
| EMU_DcdcPeakCurrent_TypeDef EMU_DCDCInit_TypeDef::peakCurrentEM01 | 
EM0/1 peak current setting.
◆ peakCurrentEM23
| EMU_DcdcPeakCurrent_TypeDef EMU_DCDCInit_TypeDef::peakCurrentEM23 | 
EM2/3 peak current setting.