VDAC_Init_TypeDef Struct Reference
VDAC initialization structure, common for both channels.
#include <em_vdac.h>
Data Fields | |
uint32_t | warmupTime |
Number of prescaled CLK_DAC + 1 for the vdac to warmup. | |
bool | dbgHalt |
Halt during debug. | |
bool | onDemandClk |
Always allow clk_dac. | |
bool | dmaWakeUp |
DMA Wakeup. | |
bool | biasKeepWarm |
Bias keep warm enable. | |
VDAC_Refresh_TypeDef | refresh |
Channel refresh period. | |
VDAC_TimerOverflow_TypeDef | timerOverflow |
Internal timer overflow period. | |
uint32_t | prescaler |
Prescaler for VDAC clock. | |
VDAC_Ref_TypeDef | reference |
Reference voltage to use. | |
bool | ch0ResetPre |
Enable/disable reset of prescaler on CH 0 start. | |
bool | sineReset |
Sine reset mode. | |
bool | sineEnable |
Enable/disable sine mode. | |
bool | diff |
Select if single ended or differential output mode. | |
VDAC initialization structure, common for both channels.
Field Documentation
◆ warmupTime
uint32_t VDAC_Init_TypeDef::warmupTime |
Number of prescaled CLK_DAC + 1 for the vdac to warmup.
◆ dbgHalt
bool VDAC_Init_TypeDef::dbgHalt |
Halt during debug.
◆ onDemandClk
bool VDAC_Init_TypeDef::onDemandClk |
Always allow clk_dac.
◆ dmaWakeUp
bool VDAC_Init_TypeDef::dmaWakeUp |
DMA Wakeup.
◆ biasKeepWarm
bool VDAC_Init_TypeDef::biasKeepWarm |
Bias keep warm enable.
◆ refresh
VDAC_Refresh_TypeDef VDAC_Init_TypeDef::refresh |
Channel refresh period.
◆ timerOverflow
VDAC_TimerOverflow_TypeDef VDAC_Init_TypeDef::timerOverflow |
Internal timer overflow period.
◆ prescaler
uint32_t VDAC_Init_TypeDef::prescaler |
Prescaler for VDAC clock.
Clock is source clock divided by prescaler+1.
◆ reference
VDAC_Ref_TypeDef VDAC_Init_TypeDef::reference |
Reference voltage to use.
◆ ch0ResetPre
bool VDAC_Init_TypeDef::ch0ResetPre |
Enable/disable reset of prescaler on CH 0 start.
◆ sineReset
bool VDAC_Init_TypeDef::sineReset |
Sine reset mode.
◆ sineEnable
bool VDAC_Init_TypeDef::sineEnable |
Enable/disable sine mode.
◆ diff
bool VDAC_Init_TypeDef::diff |
Select if single ended or differential output mode.