ACMP - Analog Comparator

Description

Analog comparator (ACMP) Peripheral API.

The Analog Comparator is used to compare voltage of two analog inputs with a digital output indicating which input voltage is higher. Inputs can either be one of the selectable internal references or from external pins. Response time and current consumption can be configured by altering the current supply to the comparator.

ACMP is available down to EM3 and is able to wake up the system when input signals pass a certain threshold. Use ACMP_IntEnable() to enable an edge interrupt to use this functionality.

This example shows how to use the em_acmp.h API for comparing an input pin to an internal 2.5 V reference voltage.

/* The ACMP is a high-frequency peripheral so we need to enable
* both the HFPER clock and the ACMP0 clock. */
/* Initialize with default settings. */
init. enable = false ;
ACMP_Init (ACMP0, &init);
/* In this example we want to compare an analog input to the 2.5 V
* internal reference. To achieve this we first have to configure the
* VB source which is used for internal reference voltages. */
ACMP_VBSetup (ACMP0, &vbconfig);
/* Now we select the two inputs to compare. Here we compare the APORT0XCH0
* input to the internal 2.5V reference that we previously configured. When
* APORT0XCH0 is lower than 2.5 V then the ACMP output is 0 and when
* APORT0XCH0 is is higher than 2.5 V then the ACMP output is 1. */
/* To be able to probe the output we can send the ACMP output to a pin.
* The second argument to this function is the pin location which is
* device dependent. */
ACMP_GPIOSetup (ACMP0, 0, true , false );
/* Finally we enable the ACMP. */
ACMP_Enable (ACMP0);
Note
ACMP can also be used to compare two separate input pins.

ACMP also contains specialized hardware for capacitive sensing. This module contains the ACMP_CapsenseInit() function to initialize ACMP for capacitive sensing and the ACMP_CapsenseChannelSet() function to select the current capsense channel.

For applications that require capacitive sensing it is recommended to use a library, such as cslib, which is provided by Silicon Labs.

Data Structures

struct ACMP_CapsenseInit_TypeDef
Capsense initialization structure.
struct ACMP_Init_TypeDef
ACMP initialization structure.
struct ACMP_VAConfig_TypeDef
VA Configuration structure.
struct ACMP_VBConfig_TypeDef
VB Configuration structure.

Functions

void ACMP_CapsenseInit (ACMP_TypeDef *acmp, const ACMP_CapsenseInit_TypeDef *init)
Set up ACMP for use in capacitive sense applications.
void ACMP_CapsenseChannelSet (ACMP_TypeDef *acmp, ACMP_Channel_TypeDef channel)
Set the ACMP channel used for capacitive sensing.
void ACMP_ChannelSet (ACMP_TypeDef *acmp, ACMP_Channel_TypeDef negSel, ACMP_Channel_TypeDef posSel)
Set which channels should be used in ACMP comparisons.
void ACMP_Disable (ACMP_TypeDef *acmp)
Disable ACMP.
void ACMP_Enable (ACMP_TypeDef *acmp)
Enable ACMP.
void ACMP_ExternalInputSelect (ACMP_TypeDef *acmp, ACMP_ExternalInput_Typedef aport)
Select and enable external input.
void ACMP_GPIOSetup (ACMP_TypeDef *acmp, uint32_t location, bool enable, bool invert)
Set up GPIO output from ACMP.
void ACMP_Init (ACMP_TypeDef *acmp, const ACMP_Init_TypeDef *init)
Initialize ACMP.
void ACMP_Reset (ACMP_TypeDef *acmp)
Reset ACMP to the same state that it was in after a hardware reset.
void ACMP_VASetup (ACMP_TypeDef *acmp, const ACMP_VAConfig_TypeDef *vaconfig)
Set up the VA source.
void ACMP_VBSetup (ACMP_TypeDef *acmp, const ACMP_VBConfig_TypeDef *vbconfig)
Set up the VB Source.
void ACMP_IntClear (ACMP_TypeDef *acmp, uint32_t flags)
Clear one or more pending ACMP interrupts.
void ACMP_IntDisable (ACMP_TypeDef *acmp, uint32_t flags)
Disable one or more ACMP interrupts.
void ACMP_IntEnable (ACMP_TypeDef *acmp, uint32_t flags)
Enable one or more ACMP interrupts.
uint32_t ACMP_IntGet (ACMP_TypeDef *acmp)
Get pending ACMP interrupt flags.
uint32_t ACMP_IntGetEnabled (ACMP_TypeDef *acmp)
Get enabled and pending ACMP interrupt flags.
void ACMP_IntSet (ACMP_TypeDef *acmp, uint32_t flags)
Set one or more pending ACMP interrupts from software.

Macros

#define ACMP_CAPSENSE_INIT_DEFAULT
A default configuration for capacitive sense mode initialization.
#define ACMP_INIT_DEFAULT
Default configuration for ACMP regular initialization.
#define ACMP_VACONFIG_DEFAULT
VA default configuration.
#define ACMP_VBCONFIG_DEFAULT
VB default configuration.

Enumerations

enum ACMP_CapsenseResistor_TypeDef {
acmpResistor0 = _ACMP_INPUTSEL_CSRESSEL_RES0,
acmpResistor1 = _ACMP_INPUTSEL_CSRESSEL_RES1,
acmpResistor2 = _ACMP_INPUTSEL_CSRESSEL_RES2,
acmpResistor3 = _ACMP_INPUTSEL_CSRESSEL_RES3,
acmpResistor4 = _ACMP_INPUTSEL_CSRESSEL_RES4,
acmpResistor5 = _ACMP_INPUTSEL_CSRESSEL_RES5,
acmpResistor6 = _ACMP_INPUTSEL_CSRESSEL_RES6,
acmpResistor7 = _ACMP_INPUTSEL_CSRESSEL_RES7
}
Resistor values used for the internal capacitive sense resistor.
enum ACMP_HysteresisLevel_TypeDef {
acmpHysteresisLevel0 = _ACMP_HYSTERESIS0_HYST_HYST0,
acmpHysteresisLevel1 = _ACMP_HYSTERESIS0_HYST_HYST1,
acmpHysteresisLevel2 = _ACMP_HYSTERESIS0_HYST_HYST2,
acmpHysteresisLevel3 = _ACMP_HYSTERESIS0_HYST_HYST3,
acmpHysteresisLevel4 = _ACMP_HYSTERESIS0_HYST_HYST4,
acmpHysteresisLevel5 = _ACMP_HYSTERESIS0_HYST_HYST5,
acmpHysteresisLevel6 = _ACMP_HYSTERESIS0_HYST_HYST6,
acmpHysteresisLevel7 = _ACMP_HYSTERESIS0_HYST_HYST7,
acmpHysteresisLevel8 = _ACMP_HYSTERESIS0_HYST_HYST8,
acmpHysteresisLevel9 = _ACMP_HYSTERESIS0_HYST_HYST9,
acmpHysteresisLevel10 = _ACMP_HYSTERESIS0_HYST_HYST10,
acmpHysteresisLevel11 = _ACMP_HYSTERESIS0_HYST_HYST11,
acmpHysteresisLevel12 = _ACMP_HYSTERESIS0_HYST_HYST12,
acmpHysteresisLevel13 = _ACMP_HYSTERESIS0_HYST_HYST13,
acmpHysteresisLevel14 = _ACMP_HYSTERESIS0_HYST_HYST14,
acmpHysteresisLevel15 = _ACMP_HYSTERESIS0_HYST_HYST15
}
Hysteresis level.
enum ACMP_InputRange_TypeDef {
acmpInputRangeFull = _ACMP_CTRL_INPUTRANGE_FULL,
acmpInputRangeHigh = _ACMP_CTRL_INPUTRANGE_GTVDDDIV2,
acmpInputRangeLow = _ACMP_CTRL_INPUTRANGE_LTVDDDIV2
}
Adjust ACMP performance for a given input voltage range.
enum ACMP_PowerSource_TypeDef {
acmpPowerSourceAvdd = _ACMP_CTRL_PWRSEL_AVDD,
acmpPowerSourceDvdd = _ACMP_CTRL_PWRSEL_DVDD,
acmpPowerSourceIOVdd0 = _ACMP_CTRL_PWRSEL_IOVDD0,
acmpPowerSourceIOVdd1 = _ACMP_CTRL_PWRSEL_IOVDD1
}
ACMP Power source.
enum ACMP_Accuracy_TypeDef {
acmpAccuracyLow = _ACMP_CTRL_ACCURACY_LOW,
acmpAccuracyHigh = _ACMP_CTRL_ACCURACY_HIGH
}
ACMP accuracy mode.
enum ACMP_VAInput_TypeDef {
acmpVAInputVDD = _ACMP_INPUTSEL_VASEL_VDD,
acmpVAInputAPORT2YCH0 = _ACMP_INPUTSEL_VASEL_APORT2YCH0,
acmpVAInputAPORT2YCH2 = _ACMP_INPUTSEL_VASEL_APORT2YCH2,
acmpVAInputAPORT2YCH4 = _ACMP_INPUTSEL_VASEL_APORT2YCH4,
acmpVAInputAPORT2YCH6 = _ACMP_INPUTSEL_VASEL_APORT2YCH6,
acmpVAInputAPORT2YCH8 = _ACMP_INPUTSEL_VASEL_APORT2YCH8,
acmpVAInputAPORT2YCH10 = _ACMP_INPUTSEL_VASEL_APORT2YCH10,
acmpVAInputAPORT2YCH12 = _ACMP_INPUTSEL_VASEL_APORT2YCH12,
acmpVAInputAPORT2YCH14 = _ACMP_INPUTSEL_VASEL_APORT2YCH14,
acmpVAInputAPORT2YCH16 = _ACMP_INPUTSEL_VASEL_APORT2YCH16,
acmpVAInputAPORT2YCH18 = _ACMP_INPUTSEL_VASEL_APORT2YCH18,
acmpVAInputAPORT2YCH20 = _ACMP_INPUTSEL_VASEL_APORT2YCH20,
acmpVAInputAPORT2YCH22 = _ACMP_INPUTSEL_VASEL_APORT2YCH22,
acmpVAInputAPORT2YCH24 = _ACMP_INPUTSEL_VASEL_APORT2YCH24,
acmpVAInputAPORT2YCH26 = _ACMP_INPUTSEL_VASEL_APORT2YCH26,
acmpVAInputAPORT2YCH28 = _ACMP_INPUTSEL_VASEL_APORT2YCH28,
acmpVAInputAPORT2YCH30 = _ACMP_INPUTSEL_VASEL_APORT2YCH30,
acmpVAInputAPORT1XCH0 = _ACMP_INPUTSEL_VASEL_APORT1XCH0,
acmpVAInputAPORT1YCH1 = _ACMP_INPUTSEL_VASEL_APORT1YCH1,
acmpVAInputAPORT1XCH2 = _ACMP_INPUTSEL_VASEL_APORT1XCH2,
acmpVAInputAPORT1YCH3 = _ACMP_INPUTSEL_VASEL_APORT1YCH3,
acmpVAInputAPORT1XCH4 = _ACMP_INPUTSEL_VASEL_APORT1XCH4,
acmpVAInputAPORT1YCH5 = _ACMP_INPUTSEL_VASEL_APORT1YCH5,
acmpVAInputAPORT1XCH6 = _ACMP_INPUTSEL_VASEL_APORT1XCH6,
acmpVAInputAPORT1YCH7 = _ACMP_INPUTSEL_VASEL_APORT1YCH7,
acmpVAInputAPORT1XCH8 = _ACMP_INPUTSEL_VASEL_APORT1XCH8,
acmpVAInputAPORT1YCH9 = _ACMP_INPUTSEL_VASEL_APORT1YCH9,
acmpVAInputAPORT1XCH10 = _ACMP_INPUTSEL_VASEL_APORT1XCH10,
acmpVAInputAPORT1YCH11 = _ACMP_INPUTSEL_VASEL_APORT1YCH11,
acmpVAInputAPORT1XCH12 = _ACMP_INPUTSEL_VASEL_APORT1XCH12,
acmpVAInputAPORT1YCH13 = _ACMP_INPUTSEL_VASEL_APORT1YCH13,
acmpVAInputAPORT1XCH14 = _ACMP_INPUTSEL_VASEL_APORT1XCH14,
acmpVAInputAPORT1YCH15 = _ACMP_INPUTSEL_VASEL_APORT1YCH15,
acmpVAInputAPORT1XCH16 = _ACMP_INPUTSEL_VASEL_APORT1XCH16,
acmpVAInputAPORT1YCH17 = _ACMP_INPUTSEL_VASEL_APORT1YCH17,
acmpVAInputAPORT1XCH18 = _ACMP_INPUTSEL_VASEL_APORT1XCH18,
acmpVAInputAPORT1YCH19 = _ACMP_INPUTSEL_VASEL_APORT1YCH19,
acmpVAInputAPORT1XCH20 = _ACMP_INPUTSEL_VASEL_APORT1XCH20,
acmpVAInputAPORT1YCH21 = _ACMP_INPUTSEL_VASEL_APORT1YCH21,
acmpVAInputAPORT1XCH22 = _ACMP_INPUTSEL_VASEL_APORT1XCH22,
acmpVAInputAPORT1YCH23 = _ACMP_INPUTSEL_VASEL_APORT1YCH23,
acmpVAInputAPORT1XCH24 = _ACMP_INPUTSEL_VASEL_APORT1XCH24,
acmpVAInputAPORT1YCH25 = _ACMP_INPUTSEL_VASEL_APORT1YCH25,
acmpVAInputAPORT1XCH26 = _ACMP_INPUTSEL_VASEL_APORT1XCH26,
acmpVAInputAPORT1YCH27 = _ACMP_INPUTSEL_VASEL_APORT1YCH27,
acmpVAInputAPORT1XCH28 = _ACMP_INPUTSEL_VASEL_APORT1XCH28,
acmpVAInputAPORT1YCH29 = _ACMP_INPUTSEL_VASEL_APORT1YCH29,
acmpVAInputAPORT1XCH30 = _ACMP_INPUTSEL_VASEL_APORT1XCH30,
acmpVAInputAPORT1YCH31 = _ACMP_INPUTSEL_VASEL_APORT1YCH31
}
ACMP input to the VA divider.
enum ACMP_VBInput_TypeDef {
acmpVBInput1V25 = _ACMP_INPUTSEL_VBSEL_1V25,
acmpVBInput2V5 = _ACMP_INPUTSEL_VBSEL_2V5
}
ACMP input to the VB divider.
enum ACMP_VLPInput_Typedef {
acmpVLPInputVADIV = _ACMP_INPUTSEL_VLPSEL_VADIV,
acmpVLPInputVBDIV = _ACMP_INPUTSEL_VLPSEL_VBDIV
}
ACMP Low-Power Input Selection.
enum ACMP_Channel_TypeDef {
acmpInputAPORT0XCH0 = _ACMP_INPUTSEL_POSSEL_APORT0XCH0,
acmpInputAPORT0XCH1 = _ACMP_INPUTSEL_POSSEL_APORT0XCH1,
acmpInputAPORT0XCH2 = _ACMP_INPUTSEL_POSSEL_APORT0XCH2,
acmpInputAPORT0XCH3 = _ACMP_INPUTSEL_POSSEL_APORT0XCH3,
acmpInputAPORT0XCH4 = _ACMP_INPUTSEL_POSSEL_APORT0XCH4,
acmpInputAPORT0XCH5 = _ACMP_INPUTSEL_POSSEL_APORT0XCH5,
acmpInputAPORT0XCH6 = _ACMP_INPUTSEL_POSSEL_APORT0XCH6,
acmpInputAPORT0XCH7 = _ACMP_INPUTSEL_POSSEL_APORT0XCH7,
acmpInputAPORT0XCH8 = _ACMP_INPUTSEL_POSSEL_APORT0XCH8,
acmpInputAPORT0XCH9 = _ACMP_INPUTSEL_POSSEL_APORT0XCH9,
acmpInputAPORT0XCH10 = _ACMP_INPUTSEL_POSSEL_APORT0XCH10,
acmpInputAPORT0XCH11 = _ACMP_INPUTSEL_POSSEL_APORT0XCH11,
acmpInputAPORT0XCH12 = _ACMP_INPUTSEL_POSSEL_APORT0XCH12,
acmpInputAPORT0XCH13 = _ACMP_INPUTSEL_POSSEL_APORT0XCH13,
acmpInputAPORT0XCH14 = _ACMP_INPUTSEL_POSSEL_APORT0XCH14,
acmpInputAPORT0XCH15 = _ACMP_INPUTSEL_POSSEL_APORT0XCH15,
acmpInputAPORT0YCH0 = _ACMP_INPUTSEL_POSSEL_APORT0YCH0,
acmpInputAPORT0YCH1 = _ACMP_INPUTSEL_POSSEL_APORT0YCH1,
acmpInputAPORT0YCH2 = _ACMP_INPUTSEL_POSSEL_APORT0YCH2,
acmpInputAPORT0YCH3 = _ACMP_INPUTSEL_POSSEL_APORT0YCH3,
acmpInputAPORT0YCH4 = _ACMP_INPUTSEL_POSSEL_APORT0YCH4,
acmpInputAPORT0YCH5 = _ACMP_INPUTSEL_POSSEL_APORT0YCH5,
acmpInputAPORT0YCH6 = _ACMP_INPUTSEL_POSSEL_APORT0YCH6,
acmpInputAPORT0YCH7 = _ACMP_INPUTSEL_POSSEL_APORT0YCH7,
acmpInputAPORT0YCH8 = _ACMP_INPUTSEL_POSSEL_APORT0YCH8,
acmpInputAPORT0YCH9 = _ACMP_INPUTSEL_POSSEL_APORT0YCH9,
acmpInputAPORT0YCH10 = _ACMP_INPUTSEL_POSSEL_APORT0YCH10,
acmpInputAPORT0YCH11 = _ACMP_INPUTSEL_POSSEL_APORT0YCH11,
acmpInputAPORT0YCH12 = _ACMP_INPUTSEL_POSSEL_APORT0YCH12,
acmpInputAPORT0YCH13 = _ACMP_INPUTSEL_POSSEL_APORT0YCH13,
acmpInputAPORT0YCH14 = _ACMP_INPUTSEL_POSSEL_APORT0YCH14,
acmpInputAPORT0YCH15 = _ACMP_INPUTSEL_POSSEL_APORT0YCH15,
acmpInputAPORT1XCH0 = _ACMP_INPUTSEL_POSSEL_APORT1XCH0,
acmpInputAPORT1YCH1 = _ACMP_INPUTSEL_POSSEL_APORT1YCH1,
acmpInputAPORT1XCH2 = _ACMP_INPUTSEL_POSSEL_APORT1XCH2,
acmpInputAPORT1YCH3 = _ACMP_INPUTSEL_POSSEL_APORT1YCH3,
acmpInputAPORT1XCH4 = _ACMP_INPUTSEL_POSSEL_APORT1XCH4,
acmpInputAPORT1YCH5 = _ACMP_INPUTSEL_POSSEL_APORT1YCH5,
acmpInputAPORT1XCH6 = _ACMP_INPUTSEL_POSSEL_APORT1XCH6,
acmpInputAPORT1YCH7 = _ACMP_INPUTSEL_POSSEL_APORT1YCH7,
acmpInputAPORT1XCH8 = _ACMP_INPUTSEL_POSSEL_APORT1XCH8,
acmpInputAPORT1YCH9 = _ACMP_INPUTSEL_POSSEL_APORT1YCH9,
acmpInputAPORT1XCH10 = _ACMP_INPUTSEL_POSSEL_APORT1XCH10,
acmpInputAPORT1YCH11 = _ACMP_INPUTSEL_POSSEL_APORT1YCH11,
acmpInputAPORT1XCH12 = _ACMP_INPUTSEL_POSSEL_APORT1XCH12,
acmpInputAPORT1YCH13 = _ACMP_INPUTSEL_POSSEL_APORT1YCH13,
acmpInputAPORT1XCH14 = _ACMP_INPUTSEL_POSSEL_APORT1XCH14,
acmpInputAPORT1YCH15 = _ACMP_INPUTSEL_POSSEL_APORT1YCH15,
acmpInputAPORT1XCH16 = _ACMP_INPUTSEL_POSSEL_APORT1XCH16,
acmpInputAPORT1YCH17 = _ACMP_INPUTSEL_POSSEL_APORT1YCH17,
acmpInputAPORT1XCH18 = _ACMP_INPUTSEL_POSSEL_APORT1XCH18,
acmpInputAPORT1YCH19 = _ACMP_INPUTSEL_POSSEL_APORT1YCH19,
acmpInputAPORT1XCH20 = _ACMP_INPUTSEL_POSSEL_APORT1XCH20,
acmpInputAPORT1YCH21 = _ACMP_INPUTSEL_POSSEL_APORT1YCH21,
acmpInputAPORT1XCH22 = _ACMP_INPUTSEL_POSSEL_APORT1XCH22,
acmpInputAPORT1YCH23 = _ACMP_INPUTSEL_POSSEL_APORT1YCH23,
acmpInputAPORT1XCH24 = _ACMP_INPUTSEL_POSSEL_APORT1XCH24,
acmpInputAPORT1YCH25 = _ACMP_INPUTSEL_POSSEL_APORT1YCH25,
acmpInputAPORT1XCH26 = _ACMP_INPUTSEL_POSSEL_APORT1XCH26,
acmpInputAPORT1YCH27 = _ACMP_INPUTSEL_POSSEL_APORT1YCH27,
acmpInputAPORT1XCH28 = _ACMP_INPUTSEL_POSSEL_APORT1XCH28,
acmpInputAPORT1YCH29 = _ACMP_INPUTSEL_POSSEL_APORT1YCH29,
acmpInputAPORT1XCH30 = _ACMP_INPUTSEL_POSSEL_APORT1XCH30,
acmpInputAPORT1YCH31 = _ACMP_INPUTSEL_POSSEL_APORT1YCH31,
acmpInputAPORT2YCH0 = _ACMP_INPUTSEL_POSSEL_APORT2YCH0,
acmpInputAPORT2XCH1 = _ACMP_INPUTSEL_POSSEL_APORT2XCH1,
acmpInputAPORT2YCH2 = _ACMP_INPUTSEL_POSSEL_APORT2YCH2,
acmpInputAPORT2XCH3 = _ACMP_INPUTSEL_POSSEL_APORT2XCH3,
acmpInputAPORT2YCH4 = _ACMP_INPUTSEL_POSSEL_APORT2YCH4,
acmpInputAPORT2XCH5 = _ACMP_INPUTSEL_POSSEL_APORT2XCH5,
acmpInputAPORT2YCH6 = _ACMP_INPUTSEL_POSSEL_APORT2YCH6,
acmpInputAPORT2XCH7 = _ACMP_INPUTSEL_POSSEL_APORT2XCH7,
acmpInputAPORT2YCH8 = _ACMP_INPUTSEL_POSSEL_APORT2YCH8,
acmpInputAPORT2XCH9 = _ACMP_INPUTSEL_POSSEL_APORT2XCH9,
acmpInputAPORT2YCH10 = _ACMP_INPUTSEL_POSSEL_APORT2YCH10,
acmpInputAPORT2XCH11 = _ACMP_INPUTSEL_POSSEL_APORT2XCH11,
acmpInputAPORT2YCH12 = _ACMP_INPUTSEL_POSSEL_APORT2YCH12,
acmpInputAPORT2XCH13 = _ACMP_INPUTSEL_POSSEL_APORT2XCH13,
acmpInputAPORT2YCH14 = _ACMP_INPUTSEL_POSSEL_APORT2YCH14,
acmpInputAPORT2XCH15 = _ACMP_INPUTSEL_POSSEL_APORT2XCH15,
acmpInputAPORT2YCH16 = _ACMP_INPUTSEL_POSSEL_APORT2YCH16,
acmpInputAPORT2XCH17 = _ACMP_INPUTSEL_POSSEL_APORT2XCH17,
acmpInputAPORT2YCH18 = _ACMP_INPUTSEL_POSSEL_APORT2YCH18,
acmpInputAPORT2XCH19 = _ACMP_INPUTSEL_POSSEL_APORT2XCH19,
acmpInputAPORT2YCH20 = _ACMP_INPUTSEL_POSSEL_APORT2YCH20,
acmpInputAPORT2XCH21 = _ACMP_INPUTSEL_POSSEL_APORT2XCH21,
acmpInputAPORT2YCH22 = _ACMP_INPUTSEL_POSSEL_APORT2YCH22,
acmpInputAPORT2XCH23 = _ACMP_INPUTSEL_POSSEL_APORT2XCH23,
acmpInputAPORT2YCH24 = _ACMP_INPUTSEL_POSSEL_APORT2YCH24,
acmpInputAPORT2XCH25 = _ACMP_INPUTSEL_POSSEL_APORT2XCH25,
acmpInputAPORT2YCH26 = _ACMP_INPUTSEL_POSSEL_APORT2YCH26,
acmpInputAPORT2XCH27 = _ACMP_INPUTSEL_POSSEL_APORT2XCH27,
acmpInputAPORT2YCH28 = _ACMP_INPUTSEL_POSSEL_APORT2YCH28,
acmpInputAPORT2XCH29 = _ACMP_INPUTSEL_POSSEL_APORT2XCH29,
acmpInputAPORT2YCH30 = _ACMP_INPUTSEL_POSSEL_APORT2YCH30,
acmpInputAPORT2XCH31 = _ACMP_INPUTSEL_POSSEL_APORT2XCH31,
acmpInputAPORT3XCH0 = _ACMP_INPUTSEL_POSSEL_APORT3XCH0,
acmpInputAPORT3YCH1 = _ACMP_INPUTSEL_POSSEL_APORT3YCH1,
acmpInputAPORT3XCH2 = _ACMP_INPUTSEL_POSSEL_APORT3XCH2,
acmpInputAPORT3YCH3 = _ACMP_INPUTSEL_POSSEL_APORT3YCH3,
acmpInputAPORT3XCH4 = _ACMP_INPUTSEL_POSSEL_APORT3XCH4,
acmpInputAPORT3YCH5 = _ACMP_INPUTSEL_POSSEL_APORT3YCH5,
acmpInputAPORT3XCH6 = _ACMP_INPUTSEL_POSSEL_APORT3XCH6,
acmpInputAPORT3YCH7 = _ACMP_INPUTSEL_POSSEL_APORT3YCH7,
acmpInputAPORT3XCH8 = _ACMP_INPUTSEL_POSSEL_APORT3XCH8,
acmpInputAPORT3YCH9 = _ACMP_INPUTSEL_POSSEL_APORT3YCH9,
acmpInputAPORT3XCH10 = _ACMP_INPUTSEL_POSSEL_APORT3XCH10,
acmpInputAPORT3YCH11 = _ACMP_INPUTSEL_POSSEL_APORT3YCH11,
acmpInputAPORT3XCH12 = _ACMP_INPUTSEL_POSSEL_APORT3XCH12,
acmpInputAPORT3YCH13 = _ACMP_INPUTSEL_POSSEL_APORT3YCH13,
acmpInputAPORT3XCH14 = _ACMP_INPUTSEL_POSSEL_APORT3XCH14,
acmpInputAPORT3YCH15 = _ACMP_INPUTSEL_POSSEL_APORT3YCH15,
acmpInputAPORT3XCH16 = _ACMP_INPUTSEL_POSSEL_APORT3XCH16,
acmpInputAPORT3YCH17 = _ACMP_INPUTSEL_POSSEL_APORT3YCH17,
acmpInputAPORT3XCH18 = _ACMP_INPUTSEL_POSSEL_APORT3XCH18,
acmpInputAPORT3YCH19 = _ACMP_INPUTSEL_POSSEL_APORT3YCH19,
acmpInputAPORT3XCH20 = _ACMP_INPUTSEL_POSSEL_APORT3XCH20,
acmpInputAPORT3YCH21 = _ACMP_INPUTSEL_POSSEL_APORT3YCH21,
acmpInputAPORT3XCH22 = _ACMP_INPUTSEL_POSSEL_APORT3XCH22,
acmpInputAPORT3YCH23 = _ACMP_INPUTSEL_POSSEL_APORT3YCH23,
acmpInputAPORT3XCH24 = _ACMP_INPUTSEL_POSSEL_APORT3XCH24,
acmpInputAPORT3YCH25 = _ACMP_INPUTSEL_POSSEL_APORT3YCH25,
acmpInputAPORT3XCH26 = _ACMP_INPUTSEL_POSSEL_APORT3XCH26,
acmpInputAPORT3YCH27 = _ACMP_INPUTSEL_POSSEL_APORT3YCH27,
acmpInputAPORT3XCH28 = _ACMP_INPUTSEL_POSSEL_APORT3XCH28,
acmpInputAPORT3YCH29 = _ACMP_INPUTSEL_POSSEL_APORT3YCH29,
acmpInputAPORT3XCH30 = _ACMP_INPUTSEL_POSSEL_APORT3XCH30,
acmpInputAPORT3YCH31 = _ACMP_INPUTSEL_POSSEL_APORT3YCH31,
acmpInputAPORT4YCH0 = _ACMP_INPUTSEL_POSSEL_APORT4YCH0,
acmpInputAPORT4XCH1 = _ACMP_INPUTSEL_POSSEL_APORT4XCH1,
acmpInputAPORT4YCH2 = _ACMP_INPUTSEL_POSSEL_APORT4YCH2,
acmpInputAPORT4XCH3 = _ACMP_INPUTSEL_POSSEL_APORT4XCH3,
acmpInputAPORT4YCH4 = _ACMP_INPUTSEL_POSSEL_APORT4YCH4,
acmpInputAPORT4XCH5 = _ACMP_INPUTSEL_POSSEL_APORT4XCH5,
acmpInputAPORT4YCH6 = _ACMP_INPUTSEL_POSSEL_APORT4YCH6,
acmpInputAPORT4XCH7 = _ACMP_INPUTSEL_POSSEL_APORT4XCH7,
acmpInputAPORT4YCH8 = _ACMP_INPUTSEL_POSSEL_APORT4YCH8,
acmpInputAPORT4XCH9 = _ACMP_INPUTSEL_POSSEL_APORT4XCH9,
acmpInputAPORT4YCH10 = _ACMP_INPUTSEL_POSSEL_APORT4YCH10,
acmpInputAPORT4XCH11 = _ACMP_INPUTSEL_POSSEL_APORT4XCH11,
acmpInputAPORT4YCH12 = _ACMP_INPUTSEL_POSSEL_APORT4YCH12,
acmpInputAPORT4XCH13 = _ACMP_INPUTSEL_POSSEL_APORT4XCH13,
acmpInputAPORT4YCH16 = _ACMP_INPUTSEL_POSSEL_APORT4YCH16,
acmpInputAPORT4XCH17 = _ACMP_INPUTSEL_POSSEL_APORT4XCH17,
acmpInputAPORT4YCH18 = _ACMP_INPUTSEL_POSSEL_APORT4YCH18,
acmpInputAPORT4XCH19 = _ACMP_INPUTSEL_POSSEL_APORT4XCH19,
acmpInputAPORT4YCH20 = _ACMP_INPUTSEL_POSSEL_APORT4YCH20,
acmpInputAPORT4XCH21 = _ACMP_INPUTSEL_POSSEL_APORT4XCH21,
acmpInputAPORT4YCH22 = _ACMP_INPUTSEL_POSSEL_APORT4YCH22,
acmpInputAPORT4XCH23 = _ACMP_INPUTSEL_POSSEL_APORT4XCH23,
acmpInputAPORT4YCH24 = _ACMP_INPUTSEL_POSSEL_APORT4YCH24,
acmpInputAPORT4XCH25 = _ACMP_INPUTSEL_POSSEL_APORT4XCH25,
acmpInputAPORT4YCH26 = _ACMP_INPUTSEL_POSSEL_APORT4YCH26,
acmpInputAPORT4XCH27 = _ACMP_INPUTSEL_POSSEL_APORT4XCH27,
acmpInputAPORT4YCH28 = _ACMP_INPUTSEL_POSSEL_APORT4YCH28,
acmpInputAPORT4XCH29 = _ACMP_INPUTSEL_POSSEL_APORT4XCH29,
acmpInputAPORT4YCH30 = _ACMP_INPUTSEL_POSSEL_APORT4YCH30,
acmpInputAPORT4YCH14 = _ACMP_INPUTSEL_POSSEL_APORT4YCH14,
acmpInputAPORT4XCH15 = _ACMP_INPUTSEL_POSSEL_APORT4XCH15,
acmpInputAPORT4XCH31 = _ACMP_INPUTSEL_POSSEL_APORT4XCH31,
acmpInputDACOUT0 = _ACMP_INPUTSEL_POSSEL_DACOUT0,
acmpInputDACOUT1 = _ACMP_INPUTSEL_POSSEL_DACOUT1,
acmpInputVLP = _ACMP_INPUTSEL_POSSEL_VLP,
acmpInputVBDIV = _ACMP_INPUTSEL_POSSEL_VBDIV,
acmpInputVADIV = _ACMP_INPUTSEL_POSSEL_VADIV,
acmpInputVDD = _ACMP_INPUTSEL_POSSEL_VDD,
acmpInputVSS = _ACMP_INPUTSEL_POSSEL_VSS
}
ACMP Input Selection.
enum ACMP_ExternalInput_Typedef {
acmpExternalInputAPORT0X = _ACMP_EXTIFCTRL_APORTSEL_APORT0X,
acmpExternalInputAPORT0Y = _ACMP_EXTIFCTRL_APORTSEL_APORT0Y,
acmpExternalInputAPORT1X = _ACMP_EXTIFCTRL_APORTSEL_APORT1X,
acmpExternalInputAPORT1Y = _ACMP_EXTIFCTRL_APORTSEL_APORT1Y,
acmpExternalInputAPORT1XY = _ACMP_EXTIFCTRL_APORTSEL_APORT1XY,
acmpExternalInputAPORT2X = _ACMP_EXTIFCTRL_APORTSEL_APORT2X,
acmpExternalInputAPORT2Y = _ACMP_EXTIFCTRL_APORTSEL_APORT2Y,
acmpExternalInputAPORT2YX = _ACMP_EXTIFCTRL_APORTSEL_APORT2YX,
acmpExternalInputAPORT3X = _ACMP_EXTIFCTRL_APORTSEL_APORT3X,
acmpExternalInputAPORT3Y = _ACMP_EXTIFCTRL_APORTSEL_APORT3Y,
acmpExternalInputAPORT3XY = _ACMP_EXTIFCTRL_APORTSEL_APORT3XY,
acmpExternalInputAPORT4X = _ACMP_EXTIFCTRL_APORTSEL_APORT4X,
acmpExternalInputAPORT4Y = _ACMP_EXTIFCTRL_APORTSEL_APORT4Y,
acmpExternalInputAPORT4YX = _ACMP_EXTIFCTRL_APORTSEL_APORT4YX
}
ACMP external input select.

Function Documentation

◆ ACMP_CapsenseInit()

void ACMP_CapsenseInit ( ACMP_TypeDef * acmp,
const ACMP_CapsenseInit_TypeDef * init
)

Set up ACMP for use in capacitive sense applications.

This function sets up ACMP for use in capacitive sense applications. To use the capacitive sense functionality in the ACMP, use the PRS output of the ACMP module to count the number of oscillations in the capacitive sense circuit (possibly using a TIMER).

Note
A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] init A pointer to the initialization structure used to configure ACMP for capacitive sensing operation.

◆ ACMP_CapsenseChannelSet()

void ACMP_CapsenseChannelSet ( ACMP_TypeDef * acmp,
ACMP_Channel_TypeDef channel
)

Set the ACMP channel used for capacitive sensing.

Note
A basic example of capacitive sensing can be found in the STK BSP (capsense demo).
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] channel The ACMP channel to use for capacitive sensing (Possel).

◆ ACMP_ChannelSet()

void ACMP_ChannelSet ( ACMP_TypeDef * acmp,
ACMP_Channel_TypeDef negSel,
ACMP_Channel_TypeDef posSel
)

Set which channels should be used in ACMP comparisons.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
negSel A channel to use on the negative input to the ACMP.
posSel A channel to use on the positive input to the ACMP.

◆ ACMP_Disable()

void ACMP_Disable ( ACMP_TypeDef * acmp )

Disable ACMP.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.

◆ ACMP_Enable()

void ACMP_Enable ( ACMP_TypeDef * acmp )

Enable ACMP.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.

◆ ACMP_ExternalInputSelect()

void ACMP_ExternalInputSelect ( ACMP_TypeDef * acmp,
ACMP_ExternalInput_Typedef aport
)

Select and enable external input.

This is used when an external module needs to take control of the ACMP POSSEL field to configure the APORT input for the ACMP. Modules, such as LESENSE, use this to change the ACMP input during a scan sequence.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] aport This parameter decides which APORT(s) the ACMP will use when it's controlled by an external module.

◆ ACMP_GPIOSetup()

void ACMP_GPIOSetup ( ACMP_TypeDef * acmp,
uint32_t location,
bool enable,
bool invert
)

Set up GPIO output from ACMP.

Note
GPIO must be enabled in the CMU before this function call, i.e.,
CMU_ClockEnable(cmuClock_GPIO, true); 
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
location The pin location to use. See the data sheet for location to pin mappings.
enable Enable or disable pin output.
invert Invert output.

◆ ACMP_Init()

void ACMP_Init ( ACMP_TypeDef * acmp,
const ACMP_Init_TypeDef * init
)

Initialize ACMP.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] init A pointer to the initialization structure used to configure ACMP.

◆ ACMP_Reset()

void ACMP_Reset ( ACMP_TypeDef * acmp )

Reset ACMP to the same state that it was in after a hardware reset.

Note
The GPIO ACMP ROUTE register is NOT reset by this function to allow for centralized setup of this feature.
The peripheral may be enabled and disabled during reset.
Parameters
[in] acmp A pointer to the ACMP peripheral register block.

◆ ACMP_VASetup()

void ACMP_VASetup ( ACMP_TypeDef * acmp,
const ACMP_VAConfig_TypeDef * vaconfig
)

Set up the VA source.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] vaconfig A pointer to the structure used to configure the VA source. This structure contains the input source and the 2 divider values.

◆ ACMP_VBSetup()

void ACMP_VBSetup ( ACMP_TypeDef * acmp,
const ACMP_VBConfig_TypeDef * vbconfig
)

Set up the VB Source.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] vbconfig A pointer to the structure used to configure the VB source. This structure contains the input source and the 2 divider values.

◆ ACMP_IntClear()

void ACMP_IntClear ( ACMP_TypeDef * acmp,
uint32_t flags
)
inline

Clear one or more pending ACMP interrupts.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] flags Pending ACMP interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFC_EDGE or ACMP_IFC_WARMUP.

◆ ACMP_IntDisable()

void ACMP_IntDisable ( ACMP_TypeDef * acmp,
uint32_t flags
)
inline

Disable one or more ACMP interrupts.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] flags ACMP interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP.

◆ ACMP_IntEnable()

void ACMP_IntEnable ( ACMP_TypeDef * acmp,
uint32_t flags
)
inline

Enable one or more ACMP interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using ACMP_IntClear() prior to enabling if a pending interrupt should be ignored.
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] flags ACMP interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IEN_EDGE or ACMP_IEN_WARMUP.

◆ ACMP_IntGet()

uint32_t ACMP_IntGet ( ACMP_TypeDef * acmp )
inline

Get pending ACMP interrupt flags.

Note
This function does not clear event bits.
Parameters
[in] acmp A pointer to the ACMP peripheral register block.
Returns
Pending ACMP interrupt sources. A bitwise logic OR combination of valid interrupt flags for the ACMP module. The pending interrupt sources can be, for instance, ACMP_IF_EDGE or ACMP_IF_WARMUP.

◆ ACMP_IntGetEnabled()

uint32_t ACMP_IntGetEnabled ( ACMP_TypeDef * acmp )
inline

Get enabled and pending ACMP interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
Note
This function does not clear interrupt flags.
Returns
Pending and enabled ACMP interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in ACMPx_IEN_nnn register (ACMPx_IEN_nnn) and
  • the OR combination of valid interrupt flags of the ACMP module (ACMPx_IF_nnn).

◆ ACMP_IntSet()

void ACMP_IntSet ( ACMP_TypeDef * acmp,
uint32_t flags
)
inline

Set one or more pending ACMP interrupts from software.

Parameters
[in] acmp A pointer to the ACMP peripheral register block.
[in] flags ACMP interrupt sources to set as pending. Use a bitwise logic OR combination of valid interrupt flags for the ACMP module. The flags can be, for instance, ACMP_IFS_EDGE or ACMP_IFS_WARMUP.

Macro Definition Documentation

◆ ACMP_CAPSENSE_INIT_DEFAULT

#define ACMP_CAPSENSE_INIT_DEFAULT
Value:
{ \
false, /* Don't use fullBias to lower power consumption. */ \
0x20, /* Using biasProg value of 0x20 (32). */ \
acmpHysteresisLevel8, /* Use hysteresis level 8 when ACMP output is 0. */ \
acmpHysteresisLevel8, /* Use hysteresis level 8 when ACMP output is 1. */ \
acmpResistor5, /* Use internal resistor value 5. */ \
0x30, /* VDD level high. */ \
0x10, /* VDD level low. */ \
true /* Enable after initialization. */ \
}

A default configuration for capacitive sense mode initialization.

◆ ACMP_INIT_DEFAULT

#define ACMP_INIT_DEFAULT
Value:
{ \
false, /* fullBias */ \
0x7, /* biasProg */ \
false, /* No interrupt on falling edge. */ \
false, /* No interrupt on rising edge. */ \
acmpInputRangeFull, /* Input range from 0 to VDD. */ \
acmpAccuracyLow, /* Low accuracy, less current usage. */ \
acmpPowerSourceAvdd, /* Use the AVDD supply. */ \
acmpHysteresisLevel5, /* Use hysteresis level 5 when output is 0 */ \
acmpHysteresisLevel5, /* Use hysteresis level 5 when output is 1 */ \
acmpVLPInputVADIV, /* Use VADIV as the VLP input source. */ \
false, /* Output 0 when ACMP is inactive. */ \
true /* Enable after init. */ \
}

Default configuration for ACMP regular initialization.

◆ ACMP_VACONFIG_DEFAULT

#define ACMP_VACONFIG_DEFAULT
Value:
{ \
acmpVAInputVDD, /* Use VDD as VA voltage input source. */ \
63, /* No division of the VA source when ACMP output is 0. */ \
63, /* No division of the VA source when ACMP output is 1. */ \
}

VA default configuration.

◆ ACMP_VBCONFIG_DEFAULT

#define ACMP_VBCONFIG_DEFAULT
Value:
{ \
acmpVBInput1V25, /* Use 1.25 V as VB voltage input source. */ \
63, /* No division of the VB source when ACMP output is 0. */ \
63, /* No division of the VB source when ACMP output is 1. */ \
}

VB default configuration.

Enumeration Type Documentation

◆ ACMP_CapsenseResistor_TypeDef

Resistor values used for the internal capacitive sense resistor.

See data sheet for your device for details on each resistor value.

Enumerator
acmpResistor0

Resistor value 0.

acmpResistor1

Resistor value 1.

acmpResistor2

Resistor value 2.

acmpResistor3

Resistor value 3.

acmpResistor4

Resistor value 4.

acmpResistor5

Resistor value 5.

acmpResistor6

Resistor value 6.

acmpResistor7

Resistor value 7.

◆ ACMP_HysteresisLevel_TypeDef

Hysteresis level.

See data sheet for your device for details on each level.

Enumerator
acmpHysteresisLevel0

Hysteresis level 0.

acmpHysteresisLevel1

Hysteresis level 1.

acmpHysteresisLevel2

Hysteresis level 2.

acmpHysteresisLevel3

Hysteresis level 3.

acmpHysteresisLevel4

Hysteresis level 4.

acmpHysteresisLevel5

Hysteresis level 5.

acmpHysteresisLevel6

Hysteresis level 6.

acmpHysteresisLevel7

Hysteresis level 7.

acmpHysteresisLevel8

Hysteresis level 8.

acmpHysteresisLevel9

Hysteresis level 9.

acmpHysteresisLevel10

Hysteresis level 10.

acmpHysteresisLevel11

Hysteresis level 11.

acmpHysteresisLevel12

Hysteresis level 12.

acmpHysteresisLevel13

Hysteresis level 13.

acmpHysteresisLevel14

Hysteresis level 14.

acmpHysteresisLevel15

Hysteresis level 15.

◆ ACMP_InputRange_TypeDef

Adjust ACMP performance for a given input voltage range.

Enumerator
acmpInputRangeFull

Input can be from 0 to VDD.

acmpInputRangeHigh

Input will always be greater than VDD/2.

acmpInputRangeLow

Input will always be less than VDD/2.

◆ ACMP_PowerSource_TypeDef

ACMP Power source.

Enumerator
acmpPowerSourceAvdd

Power ACMP using the AVDD supply.

acmpPowerSourceDvdd

Power ACMP using the DVDD supply.

acmpPowerSourceIOVdd0

Power ACMP using the IOVDD/IOVDD0 supply.

acmpPowerSourceIOVdd1

Power ACMP using the IOVDD1 supply (if the part has two I/O voltages).

◆ ACMP_Accuracy_TypeDef

ACMP accuracy mode.

Enumerator
acmpAccuracyLow

Low-accuracy mode which consumes less current.

acmpAccuracyHigh

High-accuracy mode which consumes more current.

◆ ACMP_VAInput_TypeDef

ACMP input to the VA divider.

This enumeration is used to select the input for the VA Divider.

Enumerator
acmpVAInputVDD

Select VDD for the VA divider.

acmpVAInputAPORT2YCH0

Select APORT2Y CHannel 0 for the VA divider.

acmpVAInputAPORT2YCH2

Select APORT2Y CHannel 2 for the VA divider.

acmpVAInputAPORT2YCH4

Select APORT2Y CHannel 4 for the VA divider.

acmpVAInputAPORT2YCH6

Select APORT2Y CHannel 6 for the VA divider.

acmpVAInputAPORT2YCH8

Select APORT2Y CHannel 8 for the VA divider.

acmpVAInputAPORT2YCH10

Select APORT2Y CHannel 10 for the VA divider.

acmpVAInputAPORT2YCH12

Select APORT2Y CHannel 12 for the VA divider.

acmpVAInputAPORT2YCH14

Select APORT2Y CHannel 14 for the VA divider.

acmpVAInputAPORT2YCH16

Select APORT2Y CHannel 16 for the VA divider.

acmpVAInputAPORT2YCH18

Select APORT2Y CHannel 18 for the VA divider.

acmpVAInputAPORT2YCH20

Select APORT2Y CHannel 20 for the VA divider.

acmpVAInputAPORT2YCH22

Select APORT2Y CHannel 22 for the VA divider.

acmpVAInputAPORT2YCH24

Select APORT2Y CHannel 24 for the VA divider.

acmpVAInputAPORT2YCH26

Select APORT2Y CHannel 26 for the VA divider.

acmpVAInputAPORT2YCH28

Select APORT2Y CHannel 28 for the VA divider.

acmpVAInputAPORT2YCH30

Select APORT2Y CHannel 30 for the VA divider.

acmpVAInputAPORT1XCH0

Select APORT1X CHannel 0 for the VA divider.

acmpVAInputAPORT1YCH1

Select APORT1Y CHannel 1 for the VA divider.

acmpVAInputAPORT1XCH2

Select APORT1X CHannel 2 for the VA divider.

acmpVAInputAPORT1YCH3

Select APORT1Y CHannel 3 for the VA divider.

acmpVAInputAPORT1XCH4

Select APORT1X CHannel 4 for the VA divider.

acmpVAInputAPORT1YCH5

Select APORT1Y CHannel 5 for the VA divider.

acmpVAInputAPORT1XCH6

Select APORT1X CHannel 6 for the VA divider.

acmpVAInputAPORT1YCH7

Select APORT1Y CHannel 7 for the VA divider.

acmpVAInputAPORT1XCH8

Select APORT1X CHannel 8 for the VA divider.

acmpVAInputAPORT1YCH9

Select APORT1Y CHannel 9 for the VA divider.

acmpVAInputAPORT1XCH10

Select APORT1X CHannel 10 for the VA divider.

acmpVAInputAPORT1YCH11

Select APORT1Y CHannel 11 for the VA divider.

acmpVAInputAPORT1XCH12

Select APORT1X CHannel 12 for the VA divider.

acmpVAInputAPORT1YCH13

Select APORT1Y CHannel 13 for the VA divider.

acmpVAInputAPORT1XCH14

Select APORT1X CHannel 14 for the VA divider.

acmpVAInputAPORT1YCH15

Select APORT1Y CHannel 15 for the VA divider.

acmpVAInputAPORT1XCH16

Select APORT1X CHannel 16 for the VA divider.

acmpVAInputAPORT1YCH17

Select APORT1Y CHannel 17 for the VA divider.

acmpVAInputAPORT1XCH18

Select APORT1X CHannel 18 for the VA divider.

acmpVAInputAPORT1YCH19

Select APORT1Y CHannel 19 for the VA divider.

acmpVAInputAPORT1XCH20

Select APORT1X CHannel 20 for the VA divider.

acmpVAInputAPORT1YCH21

Select APORT1Y CHannel 21 for the VA divider.

acmpVAInputAPORT1XCH22

Select APORT1X CHannel 22 for the VA divider.

acmpVAInputAPORT1YCH23

Select APORT1Y CHannel 23 for the VA divider.

acmpVAInputAPORT1XCH24

Select APORT1X CHannel 24 for the VA divider.

acmpVAInputAPORT1YCH25

Select APORT1Y CHannel 25 for the VA divider.

acmpVAInputAPORT1XCH26

Select APORT1X CHannel 26 for the VA divider.

acmpVAInputAPORT1YCH27

Select APORT1Y CHannel 27 for the VA divider.

acmpVAInputAPORT1XCH28

Select APORT1X CHannel 28 for the VA divider.

acmpVAInputAPORT1YCH29

Select APORT1Y CHannel 29 for the VA divider.

acmpVAInputAPORT1XCH30

Select APORT1X CHannel 30 for the VA divider.

acmpVAInputAPORT1YCH31

Select APORT1Y CHannel 31 for the VA divider.

◆ ACMP_VBInput_TypeDef

ACMP input to the VB divider.

This enumeration is used to select the input for the VB divider.

Enumerator
acmpVBInput1V25

Mode 1V25 for ACMP_INPUTSEL.

acmpVBInput2V5

Mode 2V5 for ACMP_INPUTSEL.

◆ ACMP_VLPInput_Typedef

ACMP Low-Power Input Selection.

Enumerator
acmpVLPInputVADIV

Mode VADIV for ACMP_INPUTSEL.

acmpVLPInputVBDIV

Mode VBDIV for ACMP_INPUTSEL.

◆ ACMP_Channel_TypeDef

ACMP Input Selection.

Enumerator
acmpInputAPORT0XCH0

Select Dedicated APORT0X CHannel 0.

acmpInputAPORT0XCH1

Select Dedicated APORT0X CHannel 1.

acmpInputAPORT0XCH2

Select Dedicated APORT0X CHannel 2.

acmpInputAPORT0XCH3

Select Dedicated APORT0X CHannel 3.

acmpInputAPORT0XCH4

Select Dedicated APORT0X CHannel 4.

acmpInputAPORT0XCH5

Select Dedicated APORT0X CHannel 5.

acmpInputAPORT0XCH6

Select Dedicated APORT0X CHannel 6.

acmpInputAPORT0XCH7

Select Dedicated APORT0X CHannel 7.

acmpInputAPORT0XCH8

Select Dedicated APORT0X CHannel 8.

acmpInputAPORT0XCH9

Select Dedicated APORT0X CHannel 9.

acmpInputAPORT0XCH10

Select Dedicated APORT0X CHannel 10.

acmpInputAPORT0XCH11

Select Dedicated APORT0X CHannel 11.

acmpInputAPORT0XCH12

Select Dedicated APORT0X CHannel 12.

acmpInputAPORT0XCH13

Select Dedicated APORT0X CHannel 13.

acmpInputAPORT0XCH14

Select Dedicated APORT0X CHannel 14.

acmpInputAPORT0XCH15

Select Dedicated APORT0X CHannel 15.

acmpInputAPORT0YCH0

Select Dedicated APORT0Y CHannel 0.

acmpInputAPORT0YCH1

Select Dedicated APORT0Y CHannel 1.

acmpInputAPORT0YCH2

Select Dedicated APORT0Y CHannel 2.

acmpInputAPORT0YCH3

Select Dedicated APORT0Y CHannel 3.

acmpInputAPORT0YCH4

Select Dedicated APORT0Y CHannel 4.

acmpInputAPORT0YCH5

Select Dedicated APORT0Y CHannel 5.

acmpInputAPORT0YCH6

Select Dedicated APORT0Y CHannel 6.

acmpInputAPORT0YCH7

Select Dedicated APORT0Y CHannel 7.

acmpInputAPORT0YCH8

Select Dedicated APORT0Y CHannel 8.

acmpInputAPORT0YCH9

Select Dedicated APORT0Y CHannel 9.

acmpInputAPORT0YCH10

Select Dedicated APORT0Y CHannel 10.

acmpInputAPORT0YCH11

Select Dedicated APORT0Y CHannel 11.

acmpInputAPORT0YCH12

Select Dedicated APORT0Y CHannel 12.

acmpInputAPORT0YCH13

Select Dedicated APORT0Y CHannel 13.

acmpInputAPORT0YCH14

Select Dedicated APORT0Y CHannel 14.

acmpInputAPORT0YCH15

Select Dedicated APORT0Y CHannel 15.

acmpInputAPORT1XCH0

Select Dedicated APORT1X CHannel 0.

acmpInputAPORT1YCH1

Select Dedicated APORT1Y CHannel 1.

acmpInputAPORT1XCH2

Select Dedicated APORT1X CHannel 2.

acmpInputAPORT1YCH3

Select Dedicated APORT1Y CHannel 3.

acmpInputAPORT1XCH4

Select Dedicated APORT1X CHannel 4.

acmpInputAPORT1YCH5

Select Dedicated APORT1Y CHannel 5.

acmpInputAPORT1XCH6

Select Dedicated APORT1X CHannel 6.

acmpInputAPORT1YCH7

Select Dedicated APORT1Y CHannel 7.

acmpInputAPORT1XCH8

Select Dedicated APORT1X CHannel 8.

acmpInputAPORT1YCH9

Select Dedicated APORT1Y CHannel 9.

acmpInputAPORT1XCH10

Select Dedicated APORT1X CHannel 10.

acmpInputAPORT1YCH11

Select Dedicated APORT1Y CHannel 11.

acmpInputAPORT1XCH12

Select Dedicated APORT1X CHannel 12.

acmpInputAPORT1YCH13

Select Dedicated APORT1Y CHannel 13.

acmpInputAPORT1XCH14

Select Dedicated APORT1X CHannel 14.

acmpInputAPORT1YCH15

Select Dedicated APORT1Y CHannel 15.

acmpInputAPORT1XCH16

Select Dedicated APORT1X CHannel 16.

acmpInputAPORT1YCH17

Select Dedicated APORT1Y CHannel 17.

acmpInputAPORT1XCH18

Select Dedicated APORT1X CHannel 18.

acmpInputAPORT1YCH19

Select Dedicated APORT1Y CHannel 19.

acmpInputAPORT1XCH20

Select Dedicated APORT1X CHannel 20.

acmpInputAPORT1YCH21

Select Dedicated APORT1Y CHannel 21.

acmpInputAPORT1XCH22

Select Dedicated APORT1X CHannel 22.

acmpInputAPORT1YCH23

Select Dedicated APORT1Y CHannel 23.

acmpInputAPORT1XCH24

Select Dedicated APORT1X CHannel 24.

acmpInputAPORT1YCH25

Select Dedicated APORT1Y CHannel 25.

acmpInputAPORT1XCH26

Select Dedicated APORT1X CHannel 26.

acmpInputAPORT1YCH27

Select Dedicated APORT1Y CHannel 27.

acmpInputAPORT1XCH28

Select Dedicated APORT1X CHannel 28.

acmpInputAPORT1YCH29

Select Dedicated APORT1Y CHannel 29.

acmpInputAPORT1XCH30

Select Dedicated APORT1X CHannel 30.

acmpInputAPORT1YCH31

Select Dedicated APORT1Y CHannel 31.

acmpInputAPORT2YCH0

Select Dedicated APORT2Y CHannel 0.

acmpInputAPORT2XCH1

Select Dedicated APORT2X CHannel 1.

acmpInputAPORT2YCH2

Select Dedicated APORT2Y CHannel 2.

acmpInputAPORT2XCH3

Select Dedicated APORT2X CHannel 3.

acmpInputAPORT2YCH4

Select Dedicated APORT2Y CHannel 4.

acmpInputAPORT2XCH5

Select Dedicated APORT2X CHannel 5.

acmpInputAPORT2YCH6

Select Dedicated APORT2Y CHannel 6.

acmpInputAPORT2XCH7

Select Dedicated APORT2X CHannel 7.

acmpInputAPORT2YCH8

Select Dedicated APORT2Y CHannel 8.

acmpInputAPORT2XCH9

Select Dedicated APORT2X CHannel 9.

acmpInputAPORT2YCH10

Select Dedicated APORT2Y CHannel 10.

acmpInputAPORT2XCH11

Select Dedicated APORT2X CHannel 11.

acmpInputAPORT2YCH12

Select Dedicated APORT2Y CHannel 12.

acmpInputAPORT2XCH13

Select Dedicated APORT2X CHannel 13.

acmpInputAPORT2YCH14

Select Dedicated APORT2Y CHannel 14.

acmpInputAPORT2XCH15

Select Dedicated APORT2X CHannel 15.

acmpInputAPORT2YCH16

Select Dedicated APORT2Y CHannel 16.

acmpInputAPORT2XCH17

Select Dedicated APORT2X CHannel 17.

acmpInputAPORT2YCH18

Select Dedicated APORT2Y CHannel 18.

acmpInputAPORT2XCH19

Select Dedicated APORT2X CHannel 19.

acmpInputAPORT2YCH20

Select Dedicated APORT2Y CHannel 20.

acmpInputAPORT2XCH21

Select Dedicated APORT2X CHannel 21.

acmpInputAPORT2YCH22

Select Dedicated APORT2Y CHannel 22.

acmpInputAPORT2XCH23

Select Dedicated APORT2X CHannel 23.

acmpInputAPORT2YCH24

Select Dedicated APORT2Y CHannel 24.

acmpInputAPORT2XCH25

Select Dedicated APORT2X CHannel 25.

acmpInputAPORT2YCH26

Select Dedicated APORT2Y CHannel 26.

acmpInputAPORT2XCH27

Select Dedicated APORT2X CHannel 27.

acmpInputAPORT2YCH28

Select Dedicated APORT2Y CHannel 28.

acmpInputAPORT2XCH29

Select Dedicated APORT2X CHannel 29.

acmpInputAPORT2YCH30

Select Dedicated APORT2Y CHannel 30.

acmpInputAPORT2XCH31

Select Dedicated APORT2X CHannel 31.

acmpInputAPORT3XCH0

Select Dedicated APORT3X CHannel 0.

acmpInputAPORT3YCH1

Select Dedicated APORT3Y CHannel 1.

acmpInputAPORT3XCH2

Select Dedicated APORT3X CHannel 2.

acmpInputAPORT3YCH3

Select Dedicated APORT3Y CHannel 3.

acmpInputAPORT3XCH4

Select Dedicated APORT3X CHannel 4.

acmpInputAPORT3YCH5

Select Dedicated APORT3Y CHannel 5.

acmpInputAPORT3XCH6

Select Dedicated APORT3X CHannel 6.

acmpInputAPORT3YCH7

Select Dedicated APORT3Y CHannel 7.

acmpInputAPORT3XCH8

Select Dedicated APORT3X CHannel 8.

acmpInputAPORT3YCH9

Select Dedicated APORT3Y CHannel 9.

acmpInputAPORT3XCH10

Select Dedicated APORT3X CHannel 10.

acmpInputAPORT3YCH11

Select Dedicated APORT3Y CHannel 11.

acmpInputAPORT3XCH12

Select Dedicated APORT3X CHannel 12.

acmpInputAPORT3YCH13

Select Dedicated APORT3Y CHannel 13.

acmpInputAPORT3XCH14

Select Dedicated APORT3X CHannel 14.

acmpInputAPORT3YCH15

Select Dedicated APORT3Y CHannel 15.

acmpInputAPORT3XCH16

Select Dedicated APORT3X CHannel 16.

acmpInputAPORT3YCH17

Select Dedicated APORT3Y CHannel 17.

acmpInputAPORT3XCH18

Select Dedicated APORT3X CHannel 18.

acmpInputAPORT3YCH19

Select Dedicated APORT3Y CHannel 19.

acmpInputAPORT3XCH20

Select Dedicated APORT3X CHannel 20.

acmpInputAPORT3YCH21

Select Dedicated APORT3Y CHannel 21.

acmpInputAPORT3XCH22

Select Dedicated APORT3X CHannel 22.

acmpInputAPORT3YCH23

Select Dedicated APORT3Y CHannel 23.

acmpInputAPORT3XCH24

Select Dedicated APORT3X CHannel 24.

acmpInputAPORT3YCH25

Select Dedicated APORT3Y CHannel 25.

acmpInputAPORT3XCH26

Select Dedicated APORT3X CHannel 26.

acmpInputAPORT3YCH27

Select Dedicated APORT3Y CHannel 27.

acmpInputAPORT3XCH28

Select Dedicated APORT3X CHannel 28.

acmpInputAPORT3YCH29

Select Dedicated APORT3Y CHannel 29.

acmpInputAPORT3XCH30

Select Dedicated APORT3X CHannel 30.

acmpInputAPORT3YCH31

Select Dedicated APORT3Y CHannel 31.

acmpInputAPORT4YCH0

Select Dedicated APORT4Y CHannel 0.

acmpInputAPORT4XCH1

Select Dedicated APORT4X CHannel 1.

acmpInputAPORT4YCH2

Select Dedicated APORT4Y CHannel 2.

acmpInputAPORT4XCH3

Select Dedicated APORT4X CHannel 3.

acmpInputAPORT4YCH4

Select Dedicated APORT4Y CHannel 4.

acmpInputAPORT4XCH5

Select Dedicated APORT4X CHannel 5.

acmpInputAPORT4YCH6

Select Dedicated APORT4Y CHannel 6.

acmpInputAPORT4XCH7

Select Dedicated APORT4X CHannel 7.

acmpInputAPORT4YCH8

Select Dedicated APORT4Y CHannel 8.

acmpInputAPORT4XCH9

Select Dedicated APORT4X CHannel 9.

acmpInputAPORT4YCH10

Select Dedicated APORT4Y CHannel 10.

acmpInputAPORT4XCH11

Select Dedicated APORT4X CHannel 11.

acmpInputAPORT4YCH12

Select Dedicated APORT4Y CHannel 12.

acmpInputAPORT4XCH13

Select Dedicated APORT4X CHannel 13.

acmpInputAPORT4YCH16

Select Dedicated APORT4Y CHannel 14.

acmpInputAPORT4XCH17

Select Dedicated APORT4X CHannel 15.

acmpInputAPORT4YCH18

Select Dedicated APORT4Y CHannel 16.

acmpInputAPORT4XCH19

Select Dedicated APORT4X CHannel 17.

acmpInputAPORT4YCH20

Select Dedicated APORT4Y CHannel 18.

acmpInputAPORT4XCH21

Select Dedicated APORT4X CHannel 19.

acmpInputAPORT4YCH22

Select Dedicated APORT4Y CHannel 20.

acmpInputAPORT4XCH23

Select Dedicated APORT4X CHannel 21.

acmpInputAPORT4YCH24

Select Dedicated APORT4Y CHannel 22.

acmpInputAPORT4XCH25

Select Dedicated APORT4X CHannel 23.

acmpInputAPORT4YCH26

Select Dedicated APORT4Y CHannel 24.

acmpInputAPORT4XCH27

Select Dedicated APORT4X CHannel 25.

acmpInputAPORT4YCH28

Select Dedicated APORT4Y CHannel 26.

acmpInputAPORT4XCH29

Select Dedicated APORT4X CHannel 27.

acmpInputAPORT4YCH30

Select Dedicated APORT4Y CHannel 28.

acmpInputAPORT4YCH14

Select Dedicated APORT4X CHannel 29.

acmpInputAPORT4XCH15

Select Dedicated APORT4Y CHannel 30.

acmpInputAPORT4XCH31

Select Dedicated APORT4X CHannel 31.

acmpInputDACOUT0

Select DAC Channel 0 Output.

acmpInputDACOUT1

Select DAC Channel 1 Output.

acmpInputVLP

Select Low-Power Sampled Voltage.

acmpInputVBDIV

Select Divided VB Voltage.

acmpInputVADIV

Select Divided VA Voltage.

acmpInputVDD

ACMPVDD as selected via PWRSEL.

acmpInputVSS

Select VSS.

◆ ACMP_ExternalInput_Typedef

ACMP external input select.

This type is used to select which APORT is used by an external module, such as LESENSE, when it's taking control over the ACMP input.

Enumerator
acmpExternalInputAPORT0X

Select APORT0X as an external input.

acmpExternalInputAPORT0Y

Select APORT0Y as an external input.

acmpExternalInputAPORT1X

Select APORT1X as an external input.

acmpExternalInputAPORT1Y

Select APORT1Y as an external input.

acmpExternalInputAPORT1XY

Select APORT1XY as an external input.

acmpExternalInputAPORT2X

Select APORT2X as an external input.

acmpExternalInputAPORT2Y

Select APORT2Y as an external input.

acmpExternalInputAPORT2YX

Select APORT2YX as an external input.

acmpExternalInputAPORT3X

Select APORT3X as an external input.

acmpExternalInputAPORT3Y

Select APORT3Y as an external input.

acmpExternalInputAPORT3XY

Select APORT3XY as an external input.

acmpExternalInputAPORT4X

Select APORT4X as an external input.

acmpExternalInputAPORT4Y

Select APORT4Y as an external input.

acmpExternalInputAPORT4YX

Select APORT4YX as an external input.