ACMP_VAConfig_TypeDef Struct Reference
VA Configuration structure.
      
       #include <em_acmp.h>
      
     
| Data Fields | |
| ACMP_VAInput_TypeDef | input | 
| VA voltage input source. | |
| uint32_t | div0 | 
| A divider for VA voltage input source when ACMP output is 0. | |
| uint32_t | div1 | 
| A divider for VA voltage input source when ACMP output is 1. | |
VA Configuration structure.
This structure is used to configure the VA voltage input source and its dividers.
Field Documentation
◆ input
| ACMP_VAInput_TypeDef ACMP_VAConfig_TypeDef::input | 
VA voltage input source.
◆ div0
| uint32_t ACMP_VAConfig_TypeDef::div0 | 
A divider for VA voltage input source when ACMP output is 0.
This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.
VA divided = VA input * (div0 + 1) / 64
◆ div1
| uint32_t ACMP_VAConfig_TypeDef::div1 | 
A divider for VA voltage input source when ACMP output is 1.
This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.
VA divided = VA input * (div1 + 1) / 64