RTCC_CCChConf_TypeDef Struct Reference
RTCC capture/compare channel configuration structure.
#include <em_rtcc.h>
Data Fields | |
RTCC_CapComChMode_TypeDef | chMode |
Select mode of Capture/Compare channel. | |
RTCC_CompMatchOutAction_TypeDef | compMatchOutAction |
Compare mode channel match output action. | |
RTCC_PRSSel_TypeDef | prsSel |
Capture mode channel PRS input channel selection. | |
RTCC_InEdgeSel_TypeDef | inputEdgeSel |
Capture mode channel input edge selection. | |
RTCC_CompBase_TypeDef | compBase |
Comparison base of channel in compare mode. | |
uint8_t | compMask |
The COMPMASK (5 bit) most significant bits of compare value will not be subject to comparison. | |
RTCC_DayCompareMode_TypeDef | dayCompMode |
Day compare mode. | |
RTCC capture/compare channel configuration structure.
Field Documentation
◆ chMode
RTCC_CapComChMode_TypeDef RTCC_CCChConf_TypeDef::chMode |
Select mode of Capture/Compare channel.
◆ compMatchOutAction
RTCC_CompMatchOutAction_TypeDef RTCC_CCChConf_TypeDef::compMatchOutAction |
Compare mode channel match output action.
◆ prsSel
RTCC_PRSSel_TypeDef RTCC_CCChConf_TypeDef::prsSel |
Capture mode channel PRS input channel selection.
◆ inputEdgeSel
RTCC_InEdgeSel_TypeDef RTCC_CCChConf_TypeDef::inputEdgeSel |
Capture mode channel input edge selection.
◆ compBase
RTCC_CompBase_TypeDef RTCC_CCChConf_TypeDef::compBase |
Comparison base of channel in compare mode.
◆ compMask
uint8_t RTCC_CCChConf_TypeDef::compMask |
The COMPMASK (5 bit) most significant bits of compare value will not be subject to comparison.
◆ dayCompMode
RTCC_DayCompareMode_TypeDef RTCC_CCChConf_TypeDef::dayCompMode |
Day compare mode.