ACMP_CapsenseInit_TypeDef Struct Reference

Capsense initialization structure.

#include <em_acmp.h>

Data Fields

bool fullBias
Full-bias current.
uint32_t biasProg
Bias current.
ACMP_HysteresisLevel_TypeDef hysteresisLevel_0
Hysteresis level when ACMP output is 0.
ACMP_HysteresisLevel_TypeDef hysteresisLevel_1
Hysteresis level when ACMP output is 1.
ACMP_CapsenseResistor_TypeDef resistor
A resistor used in the capacitive sensing circuit.
uint32_t vddLevelHigh
This value configures the upper voltage threshold of the capsense oscillation rail.
uint32_t vddLevelLow
This value configures the lower voltage threshold of the capsense oscillation rail.
bool enable
If true, ACMP is enabled after configuration.

Capsense initialization structure.

Field Documentation

◆ fullBias

bool ACMP_CapsenseInit_TypeDef::fullBias

Full-bias current.

See the ACMP chapter about bias and response time in the reference manual for details.

◆ biasProg

uint32_t ACMP_CapsenseInit_TypeDef::biasProg

Bias current.

See the ACMP chapter about bias and response time in the reference manual for details.

◆ hysteresisLevel_0

ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel_0

Hysteresis level when ACMP output is 0.

◆ hysteresisLevel_1

ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel_1

Hysteresis level when ACMP output is 1.

◆ resistor

ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor

A resistor used in the capacitive sensing circuit.

For values see the device data sheet.

◆ vddLevelHigh

uint32_t ACMP_CapsenseInit_TypeDef::vddLevelHigh

This value configures the upper voltage threshold of the capsense oscillation rail.

The voltage threshold is calculated as follows: VDD * (vddLevelHigh + 1) / 64

◆ vddLevelLow

uint32_t ACMP_CapsenseInit_TypeDef::vddLevelLow

This value configures the lower voltage threshold of the capsense oscillation rail.

The voltage threshold is calculated as follows: VDD * (vddLevelLow + 1) / 64

◆ enable

bool ACMP_CapsenseInit_TypeDef::enable

If true, ACMP is enabled after configuration.