RTCCEMLIB
Detailed Description
Real Time Counter (RTCC) Peripheral API.
This module contains functions to control the RTCC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTCC ensures timekeeping in low energy modes. The RTCC also includes a BCD calendar mode for easy time and date keeping.
Data Structures | |
struct | RTCC_CCChConf_TypeDef |
struct | RTCC_Init_TypeDef |
Macros | |
#define | RTCC_CH_INIT_CAPTURE_DEFAULT |
#define | RTCC_CH_INIT_COMPARE_DEFAULT |
#define | RTCC_CH_VALID(ch) ( (ch) < 3) |
#define | RTCC_INIT_DEFAULT |
Enumerations | |
enum | RTCC_CapComChMode_TypeDef { rtccCapComChModeOff = _RTCC_CC_CTRL_MODE_OFF, rtccCapComChModeCapture = _RTCC_CC_CTRL_MODE_INPUTCAPTURE, rtccCapComChModeCompare = _RTCC_CC_CTRL_MODE_OUTPUTCOMPARE } |
enum | RTCC_CntMode_TypeDef { rtccCntModeNormal = _RTCC_CTRL_CNTMODE_NORMAL, rtccCntModeCalendar = _RTCC_CTRL_CNTMODE_CALENDAR } |
enum | RTCC_CntPresc_TypeDef { rtccCntPresc_1 = _RTCC_CTRL_CNTPRESC_DIV1, rtccCntPresc_2 = _RTCC_CTRL_CNTPRESC_DIV2, rtccCntPresc_4 = _RTCC_CTRL_CNTPRESC_DIV4, rtccCntPresc_8 = _RTCC_CTRL_CNTPRESC_DIV8, rtccCntPresc_16 = _RTCC_CTRL_CNTPRESC_DIV16, rtccCntPresc_32 = _RTCC_CTRL_CNTPRESC_DIV32, rtccCntPresc_64 = _RTCC_CTRL_CNTPRESC_DIV64, rtccCntPresc_128 = _RTCC_CTRL_CNTPRESC_DIV128, rtccCntPresc_256 = _RTCC_CTRL_CNTPRESC_DIV256, rtccCntPresc_512 = _RTCC_CTRL_CNTPRESC_DIV512, rtccCntPresc_1024 = _RTCC_CTRL_CNTPRESC_DIV1024, rtccCntPresc_2048 = _RTCC_CTRL_CNTPRESC_DIV2048, rtccCntPresc_4096 = _RTCC_CTRL_CNTPRESC_DIV4096, rtccCntPresc_8192 = _RTCC_CTRL_CNTPRESC_DIV8192, rtccCntPresc_16384 = _RTCC_CTRL_CNTPRESC_DIV16384, rtccCntPresc_32768 = _RTCC_CTRL_CNTPRESC_DIV32768 } |
enum | RTCC_CompBase_TypeDef { rtccCompBaseCnt = _RTCC_CC_CTRL_COMPBASE_CNT, rtccCompBasePreCnt = _RTCC_CC_CTRL_COMPBASE_PRECNT } |
enum | RTCC_CompMatchOutAction_TypeDef { rtccCompMatchOutActionPulse = _RTCC_CC_CTRL_CMOA_PULSE, rtccCompMatchOutActionToggle = _RTCC_CC_CTRL_CMOA_TOGGLE, rtccCompMatchOutActionClear = _RTCC_CC_CTRL_CMOA_CLEAR, rtccCompMatchOutActionSet = _RTCC_CC_CTRL_CMOA_SET } |
enum | RTCC_DayCompareMode_TypeDef { rtccDayCompareModeMonth = _RTCC_CC_CTRL_DAYCC_MONTH, rtccDayCompareModeWeek = _RTCC_CC_CTRL_DAYCC_WEEK } |
enum | RTCC_InEdgeSel_TypeDef { rtccInEdgeRising = _RTCC_CC_CTRL_ICEDGE_RISING, rtccInEdgeFalling = _RTCC_CC_CTRL_ICEDGE_FALLING, rtccInEdgeBoth = _RTCC_CC_CTRL_ICEDGE_BOTH, rtccInEdgeNone = _RTCC_CC_CTRL_ICEDGE_NONE } |
enum | RTCC_PrescMode_TypeDef { rtccCntTickPresc = _RTCC_CTRL_CNTTICK_PRESC, rtccCntTickCCV0Match = _RTCC_CTRL_CNTTICK_CCV0MATCH } |
enum | RTCC_PRSSel_TypeDef { rtccPRSCh0 = _RTCC_CC_CTRL_PRSSEL_PRSCH0, rtccPRSCh1 = _RTCC_CC_CTRL_PRSSEL_PRSCH1, rtccPRSCh2 = _RTCC_CC_CTRL_PRSSEL_PRSCH2, rtccPRSCh3 = _RTCC_CC_CTRL_PRSSEL_PRSCH3, rtccPRSCh4 = _RTCC_CC_CTRL_PRSSEL_PRSCH4, rtccPRSCh5 = _RTCC_CC_CTRL_PRSSEL_PRSCH5, rtccPRSCh6 = _RTCC_CC_CTRL_PRSSEL_PRSCH6, rtccPRSCh7 = _RTCC_CC_CTRL_PRSSEL_PRSCH7, rtccPRSCh8 = _RTCC_CC_CTRL_PRSSEL_PRSCH8, rtccPRSCh9 = _RTCC_CC_CTRL_PRSSEL_PRSCH9, rtccPRSCh10 = _RTCC_CC_CTRL_PRSSEL_PRSCH10, rtccPRSCh11 = _RTCC_CC_CTRL_PRSSEL_PRSCH11 } |
Functions | |
__STATIC_INLINE uint32_t | RTCC_ChannelCCVGet (int ch) |
Get RTCC capture/compare register value (CCV) for selected channel. | |
__STATIC_INLINE void | RTCC_ChannelCCVSet (int ch, uint32_t value) |
Set RTCC capture/compare register value (CCV) for selected channel. | |
__STATIC_INLINE uint32_t | RTCC_ChannelDateGet (int ch) |
Get the calendar DATE register content for selected channel. | |
__STATIC_INLINE void | RTCC_ChannelDateSet (int ch, uint32_t date) |
Set the calendar DATE register for selected channel. | |
void | RTCC_ChannelInit (int ch, RTCC_CCChConf_TypeDef const *confPtr) |
Configure the selected capture/compare channel of the RTCC. | |
__STATIC_INLINE uint32_t | RTCC_ChannelTimeGet (int ch) |
Get the calendar TIME register content for selected channel. | |
__STATIC_INLINE void | RTCC_ChannelTimeSet (int ch, uint32_t time) |
Set the calendar TIME register for selected channel. | |
__STATIC_INLINE uint32_t | RTCC_CombinedCounterGet (void) |
Get the combined CNT/PRECNT register content. | |
__STATIC_INLINE uint32_t | RTCC_CounterGet (void) |
Get RTCC counter value. | |
__STATIC_INLINE void | RTCC_CounterSet (uint32_t value) |
Set RTCC CNT counter. | |
__STATIC_INLINE uint32_t | RTCC_DateGet (void) |
Get DATE register value. | |
__STATIC_INLINE void | RTCC_DateSet (uint32_t date) |
Set RTCC DATE register. | |
__STATIC_INLINE void | RTCC_EM4WakeupEnable (bool enable) |
Enable/disable EM4 wakeup capability. | |
void | RTCC_Enable (bool enable) |
Enable/disable RTCC. | |
void | RTCC_Init (const RTCC_Init_TypeDef *init) |
Initialize RTCC. | |
__STATIC_INLINE void | RTCC_IntClear (uint32_t flags) |
Clear one or more pending RTCC interrupts. | |
__STATIC_INLINE void | RTCC_IntDisable (uint32_t flags) |
Disable one or more RTCC interrupts. | |
__STATIC_INLINE void | RTCC_IntEnable (uint32_t flags) |
Enable one or more RTCC interrupts. | |
__STATIC_INLINE uint32_t | RTCC_IntGet (void) |
Get pending RTCC interrupt flags. | |
__STATIC_INLINE uint32_t | RTCC_IntGetEnabled (void) |
Get enabled and pending RTCC interrupt flags. | |
__STATIC_INLINE void | RTCC_IntSet (uint32_t flags) |
Set one or more pending RTCC interrupts from SW. | |
__STATIC_INLINE void | RTCC_Lock (void) |
Lock RTCC registers. | |
__STATIC_INLINE uint32_t | RTCC_PreCounterGet (void) |
Get RTCC pre-counter value. | |
__STATIC_INLINE void | RTCC_PreCounterSet (uint32_t preCntVal) |
Set RTCC pre-counter value. | |
void | RTCC_Reset (void) |
Restore RTCC to its reset state. | |
__STATIC_INLINE void | RTCC_RetentionRamPowerDown (void) |
Power down the retention ram. | |
void | RTCC_StatusClear (void) |
Clear STATUS register. | |
__STATIC_INLINE uint32_t | RTCC_StatusGet (void) |
Get STATUS register value. | |
__STATIC_INLINE uint32_t | RTCC_TimeGet (void) |
Get TIME register value. | |
__STATIC_INLINE void | RTCC_TimeSet (uint32_t time) |
Set RTCC TIME register. | |
__STATIC_INLINE void | RTCC_Unlock (void) |
Unlock RTCC registers. | |
Macro Definition Documentation
#define RTCC_CH_INIT_CAPTURE_DEFAULT |
Default RTCC channel input capture init structure.
Definition at line 292
of file em_rtcc.h
.
#define RTCC_CH_INIT_COMPARE_DEFAULT |
Default RTCC channel output compare init structure.
Definition at line 280
of file em_rtcc.h
.
#define RTCC_CH_VALID | ( | ch | ) | ( (ch) < 3) |
Validation of valid RTCC channel for assert statements.
Definition at line 304
of file em_rtcc.h
.
Referenced by RTCC_ChannelCCVGet(), RTCC_ChannelCCVSet(), RTCC_ChannelDateGet(), RTCC_ChannelDateSet(), RTCC_ChannelInit(), RTCC_ChannelTimeGet(), and RTCC_ChannelTimeSet().
#define RTCC_INIT_DEFAULT |
Default RTCC init structure.
Definition at line 265
of file em_rtcc.h
.
Referenced by UDELAY_Calibrate().
Enumeration Type Documentation
enum RTCC_CntMode_TypeDef |
Counter prescaler selection.
Definition at line 86
of file em_rtcc.h
.
enum RTCC_PRSSel_TypeDef |
PRS input sources.
Definition at line 131
of file em_rtcc.h
.
Function Documentation
__STATIC_INLINE uint32_t RTCC_ChannelCCVGet | ( | int | ch | ) |
Get RTCC capture/compare register value (CCV) for selected channel.
- Parameters
-
[in] ch
Channel selector.
- Returns
- Capture/compare register value.
Definition at line 320
of file em_rtcc.h
.
References RTCC, and RTCC_CH_VALID.
__STATIC_INLINE void RTCC_ChannelCCVSet | ( | int | ch, |
uint32_t | value |
||
) |
Set RTCC capture/compare register value (CCV) for selected channel.
- Parameters
-
[in] ch
Channel selector. [in] value
CCV value.
Definition at line 336
of file em_rtcc.h
.
References RTCC, and RTCC_CH_VALID.
__STATIC_INLINE uint32_t RTCC_ChannelDateGet | ( | int | ch | ) |
Get the calendar DATE register content for selected channel.
- Parameters
-
[in] ch
Channel selector.
- Returns
- DATE register value.
Definition at line 352
of file em_rtcc.h
.
References RTCC, and RTCC_CH_VALID.
__STATIC_INLINE void RTCC_ChannelDateSet | ( | int | ch, |
uint32_t | date |
||
) |
Set the calendar DATE register for selected channel.
- Parameters
-
[in] ch
Channel selector. [in] date
DATE value.
Definition at line 368
of file em_rtcc.h
.
References RTCC, and RTCC_CH_VALID.
void RTCC_ChannelInit | ( | int | ch, |
RTCC_CCChConf_TypeDef const * | confPtr |
||
) |
Configure the selected capture/compare channel of the RTCC.
Use this function to configure a RTCC channel. Select capture/compare mode, match output action, overflow output action and PRS input configuration. Refer to the configuration structure RTCC_CCChConf_TypeDef for more details.
- Parameters
-
[in] ch
Channel selector. [in] confPtr
Pointer to configuration structure.
Configure the selected capture/compare channel.
Definition at line 81
of file em_rtcc.c
.
References _RTCC_CC_CTRL_CMOA_SHIFT, _RTCC_CC_CTRL_COMPBASE_SHIFT, _RTCC_CC_CTRL_COMPMASK_MASK, _RTCC_CC_CTRL_COMPMASK_SHIFT, _RTCC_CC_CTRL_DAYCC_SHIFT, _RTCC_CC_CTRL_ICEDGE_SHIFT, _RTCC_CC_CTRL_MODE_SHIFT, _RTCC_CC_CTRL_PRSSEL_SHIFT, RTCC_CCChConf_TypeDef::chMode, RTCC_CCChConf_TypeDef::compBase, RTCC_CCChConf_TypeDef::compMask, RTCC_CCChConf_TypeDef::compMatchOutAction, RTCC_CCChConf_TypeDef::dayCompMode, RTCC_CCChConf_TypeDef::inputEdgeSel, RTCC_CCChConf_TypeDef::prsSel, RTCC, and RTCC_CH_VALID.
Referenced by RTCDRV_Init().
__STATIC_INLINE uint32_t RTCC_ChannelTimeGet | ( | int | ch | ) |
Get the calendar TIME register content for selected channel.
- Parameters
-
[in] ch
Channel selector.
- Returns
- TIME register value.
Definition at line 386
of file em_rtcc.h
.
References RTCC, and RTCC_CH_VALID.
__STATIC_INLINE void RTCC_ChannelTimeSet | ( | int | ch, |
uint32_t | time |
||
) |
Set the calendar TIME register for selected channel.
- Parameters
-
[in] ch
Channel selector. [in] time
TIME value.
Definition at line 402
of file em_rtcc.h
.
References RTCC, and RTCC_CH_VALID.
__STATIC_INLINE uint32_t RTCC_CombinedCounterGet | ( | void |
| ) |
Get the combined CNT/PRECNT register content.
- Returns
- CNT/PRECNT register value.
Definition at line 415
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE uint32_t RTCC_CounterGet | ( | void |
| ) |
Get RTCC counter value.
- Returns
- Current RTCC counter value.
Definition at line 427
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_CounterSet | ( | uint32_t | value | ) |
Set RTCC CNT counter.
- Parameters
-
[in] value
CNT value.
Definition at line 439
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE uint32_t RTCC_DateGet | ( | void |
| ) |
Get DATE register value.
- Returns
- Current DATE register value.
Definition at line 451
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_DateSet | ( | uint32_t | date | ) |
Set RTCC DATE register.
- Parameters
-
[in] date
DATE value.
Definition at line 463
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_EM4WakeupEnable | ( | bool | enable | ) |
Enable/disable EM4 wakeup capability.
- Parameters
-
[in] enable
True to enable EM4 wakeup, false to disable.
Definition at line 475
of file em_rtcc.h
.
References RTCC, and RTCC_EM4WUEN_EM4WU.
void RTCC_Enable | ( | bool | enable | ) |
Enable/disable RTCC.
- Parameters
-
[in] enable
True to enable RTCC, false to disable.
Definition at line 105
of file em_rtcc.c
.
References _RTCC_CTRL_ENABLE_SHIFT, BUS_RegBitWrite(), and RTCC.
Referenced by RTCDRV_DeInit(), and UDELAY_Calibrate().
void RTCC_Init | ( | const RTCC_Init_TypeDef * | init | ) |
Initialize RTCC.
Note that the compare values must be set separately with RTCC_CompareSet(). That should probably be done prior to the use of this function if configuring the RTCC to start when initialization is completed.
- Parameters
-
[in] init
Pointer to RTCC initialization structure.
Definition at line 123
of file em_rtcc.c
.
References _RTCC_CTRL_CCV1TOP_SHIFT, _RTCC_CTRL_CNTMODE_SHIFT, _RTCC_CTRL_CNTPRESC_SHIFT, _RTCC_CTRL_CNTTICK_SHIFT, _RTCC_CTRL_DEBUGRUN_SHIFT, _RTCC_CTRL_ENABLE_SHIFT, _RTCC_CTRL_LYEARCORRDIS_SHIFT, _RTCC_CTRL_OSCFDETEN_SHIFT, _RTCC_CTRL_PRECCV0TOP_SHIFT, RTCC_Init_TypeDef::cntMode, RTCC_Init_TypeDef::cntWrapOnCCV1, RTCC_Init_TypeDef::debugRun, RTCC_Init_TypeDef::disLeapYearCorr, RTCC_Init_TypeDef::enable, RTCC_Init_TypeDef::enaOSCFailDetect, RTCC_Init_TypeDef::precntWrapOnCCV0, RTCC_Init_TypeDef::presc, RTCC_Init_TypeDef::prescMode, and RTCC.
Referenced by RTCDRV_Init(), and UDELAY_Calibrate().
__STATIC_INLINE void RTCC_IntClear | ( | uint32_t | flags | ) |
Clear one or more pending RTCC interrupts.
- Parameters
-
[in] flags
RTCC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.
Definition at line 496
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_IntDisable | ( | uint32_t | flags | ) |
Disable one or more RTCC interrupts.
- Parameters
-
[in] flags
RTCC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt.
Definition at line 509
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_IntEnable | ( | uint32_t | flags | ) |
Enable one or more RTCC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. Consider using RTCC_IntClear() prior to enabling if such a pending interrupt should be ignored.
- Parameters
-
[in] flags
RTCC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt.
Definition at line 527
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE uint32_t RTCC_IntGet | ( | void |
| ) |
Get pending RTCC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
Definition at line 543
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE uint32_t RTCC_IntGetEnabled | ( | void |
| ) |
Get enabled and pending RTCC interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Returns
- Pending and enabled RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
Definition at line 559
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_IntSet | ( | uint32_t | flags | ) |
Set one or more pending RTCC interrupts from SW.
- Parameters
-
[in] flags
RTCC interrupt sources to set to pending. Use a set of interrupt flags (RTCC_IFS_nnn).
Definition at line 577
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_Lock | ( | void |
| ) |
Lock RTCC registers.
- Note
- When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers can not be written to.
Definition at line 591
of file em_rtcc.h
.
References CMU, CMU_LOCK_LOCKKEY_LOCK, CMU_LOCK_LOCKKEY_LOCKED, CMU_LOCK_LOCKKEY_UNLOCK, RTCC, and RTCC_LOCK_LOCKKEY_LOCK.
__STATIC_INLINE uint32_t RTCC_PreCounterGet | ( | void |
| ) |
Get RTCC pre-counter value.
- Returns
- Current RTCC pre-counter value.
Definition at line 620
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_PreCounterSet | ( | uint32_t | preCntVal | ) |
Set RTCC pre-counter value.
- Parameters
-
[in] preCntVal
RTCC pre-counter value to be set.
Definition at line 632
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_RetentionRamPowerDown | ( | void |
| ) |
Power down the retention ram.
- Note
- Once retention ram is powered down, it cannot be powered up again.
Definition at line 646
of file em_rtcc.h
.
References RTCC, and RTCC_POWERDOWN_RAM.
__STATIC_INLINE uint32_t RTCC_StatusGet | ( | void |
| ) |
Get STATUS register value.
- Returns
- Current STATUS register value.
Definition at line 664
of file em_rtcc.h
.
References RTCC, and RTCC_SYNCBUSY_CMD.
__STATIC_INLINE uint32_t RTCC_TimeGet | ( | void |
| ) |
Get TIME register value.
- Returns
- Current TIME register value.
Definition at line 679
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_TimeSet | ( | uint32_t | time | ) |
Set RTCC TIME register.
- Parameters
-
[in] time
TIME value.
Definition at line 691
of file em_rtcc.h
.
References RTCC.
__STATIC_INLINE void RTCC_Unlock | ( | void |
| ) |
Unlock RTCC registers.
- Note
- When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers can not be written to.
Definition at line 705
of file em_rtcc.h
.
References CMU, CMU_LOCK_LOCKKEY_LOCK, CMU_LOCK_LOCKKEY_LOCKED, CMU_LOCK_LOCKKEY_UNLOCK, RTCC, and RTCC_LOCK_LOCKKEY_UNLOCK.
Referenced by RTCC_Reset().