IDAC_TypeDef Struct ReferenceDevices > IDAC
IDAC Register Declaration
Definition at line 49
of file efm32jg1b_idac.h
.
#include <
efm32jg1b_idac.h
>
Data Fields | |
__IM uint32_t | APORTCONFLICT |
__IM uint32_t | APORTREQ |
__IOM uint32_t | CTRL |
__IOM uint32_t | CURPROG |
__IOM uint32_t | DUTYCONFIG |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
uint32_t | RESERVED0 [1] |
uint32_t | RESERVED1 [2] |
uint32_t | RESERVED2 [1] |
uint32_t | RESERVED3 [1] |
__IM uint32_t | STATUS |
Field Documentation
__IM uint32_t IDAC_TypeDef::APORTCONFLICT |
APORT Request Status Register
Definition at line 64
of file efm32jg1b_idac.h
.
__IM uint32_t IDAC_TypeDef::APORTREQ |
APORT Request Status Register
Definition at line 63
of file efm32jg1b_idac.h
.
__IOM uint32_t IDAC_TypeDef::CTRL |
Control Register
Definition at line 50
of file efm32jg1b_idac.h
.
Referenced by IDAC_Enable(), IDAC_Init(), IDAC_MinimalOutputTransitionMode(), IDAC_OutEnable(), IDAC_RangeSet(), and IDAC_Reset().
__IOM uint32_t IDAC_TypeDef::CURPROG |
Current Programming Register
Definition at line 51
of file efm32jg1b_idac.h
.
Referenced by IDAC_RangeSet(), IDAC_Reset(), and IDAC_StepSet().
__IOM uint32_t IDAC_TypeDef::DUTYCONFIG |
Duty Cycle Configuration Register
Definition at line 53
of file efm32jg1b_idac.h
.
Referenced by IDAC_Reset().
__IOM uint32_t IDAC_TypeDef::IEN |
Interrupt Enable Register
Definition at line 61
of file efm32jg1b_idac.h
.
Referenced by IDAC_IntDisable(), IDAC_IntEnable(), and IDAC_IntGetEnabled().
__IM uint32_t IDAC_TypeDef::IF |
Interrupt Flag Register
Definition at line 58
of file efm32jg1b_idac.h
.
Referenced by IDAC_IntGet(), and IDAC_IntGetEnabled().
__IOM uint32_t IDAC_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 60
of file efm32jg1b_idac.h
.
Referenced by IDAC_IntClear().
__IOM uint32_t IDAC_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 59
of file efm32jg1b_idac.h
.
Referenced by IDAC_IntSet().
uint32_t IDAC_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line 52
of file efm32jg1b_idac.h
.
uint32_t IDAC_TypeDef::RESERVED1[2] |
Reserved for future use
Definition at line 55
of file efm32jg1b_idac.h
.
uint32_t IDAC_TypeDef::RESERVED2[1] |
Reserved for future use
Definition at line 57
of file efm32jg1b_idac.h
.
uint32_t IDAC_TypeDef::RESERVED3[1] |
Reserved for future use
Definition at line 62
of file efm32jg1b_idac.h
.
__IM uint32_t IDAC_TypeDef::STATUS |
Status Register
Definition at line 56
of file efm32jg1b_idac.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG1B/Include/
efm32jg1b_idac.h