RTCC_CC_TypeDef Struct ReferenceDevicesDevices > | RTCC

RTCC_CC RTCC CC Register


      

.

Definition at line 47 of file efm32jg1b_rtcc_cc.h .

#include < efm32jg1b_rtcc_cc.h >

Data Fields

__IOM uint32_t CCV
__IOM uint32_t CTRL
__IOM uint32_t DATE
__IOM uint32_t TIME

Field Documentation

__IOM uint32_t RTCC_CC_TypeDef::CCV

Capture/Compare Value Register

Definition at line 49 of file efm32jg1b_rtcc_cc.h .

__IOM uint32_t RTCC_CC_TypeDef::CTRL

CC Channel Control Register

Definition at line 48 of file efm32jg1b_rtcc_cc.h .

__IOM uint32_t RTCC_CC_TypeDef::DATE

Capture/Compare Date Register

Definition at line 51 of file efm32jg1b_rtcc_cc.h .

__IOM uint32_t RTCC_CC_TypeDef::TIME

Capture/Compare Time Register

Definition at line 50 of file efm32jg1b_rtcc_cc.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG1B/Include/ efm32jg1b_rtcc_cc.h