EMU_DCDCInit_TypeDef Struct ReferenceEMLIB > EMU
DCDC initialization structure
       Definition at line
       
        572
       
       of file
       
        em_emu.h
       
       .
      
      
       #include <
       
     
        em_emu.h
       
       >
      
Field Documentation
| EMU_DcdcAnaPeripheralPower_TypeDef EMU_DCDCInit_TypeDef::anaPeripheralPower | 
Select analog peripheral power in DCDC-to-DVDD mode
        Definition at line
        
         589
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| EMU_DcdcLnCompCtrl_TypeDef EMU_DCDCInit_TypeDef::dcdcLnCompCtrl | 
DCDC Low-noise mode compensator control.
        Definition at line
        
         596
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| EMU_DcdcMode_TypeDef EMU_DCDCInit_TypeDef::dcdcMode | 
DCDC regulator operating mode in EM0/1
        Definition at line
        
         575
        
        of file
        
         em_emu.h
        
        .
       
Referenced by BSP_initDcdc() , and EMU_DCDCInit() .
| uint16_t EMU_DCDCInit_TypeDef::em01LoadCurrent_mA | 
Estimated average load current in EM0/1 (mA). This estimate is also used for EM1 optimization, so if EM1 current is expected to be higher than EM0, then this parameter should hold the higher EM1 current.
        Definition at line
        
         577
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| uint16_t EMU_DCDCInit_TypeDef::em234LoadCurrent_uA | 
Estimated average load current in EM2 (uA). This estimate is also used for EM3 and 4 optimization, so if EM3 or 4 current is expected to be higher than EM2, then this parameter should hold the higher EM3 or 4 current.
        Definition at line
        
         581
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| uint16_t EMU_DCDCInit_TypeDef::maxCurrent_mA | 
Maximum average DCDC output current (mA). This can be set to the maximum for the power source, for example the maximum for a battery.
        Definition at line
        
         585
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
| uint16_t EMU_DCDCInit_TypeDef::mVout | 
| EMU_PowerConfig_TypeDef EMU_DCDCInit_TypeDef::powerConfig | 
Device external power configuration. emuPowerConfig_DcdcToDvdd is currently the only supported mode.
        Definition at line
        
         573
        
        of file
        
         em_emu.h
        
        .
       
| EMU_DcdcLnReverseCurrentControl_TypeDef EMU_DCDCInit_TypeDef::reverseCurrentControl | 
Low-noise reverse current control. NOTE: this parameter uses special encoding: >= 0 is forced CCM mode where the parameter is used as the reverse current threshold in mA. -1 is encoded as emuDcdcLnHighEfficiencyMode (EFM32 only)
        Definition at line
        
         591
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_DCDCInit() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_emu.h