LDMA_CH_TypeDef Struct ReferenceDevicesDevices > | LDMA
LDMA_CH LDMA CH Register
.
       Definition at line
       
        47
       
       of file
       
        efm32jg1b_ldma_ch.h
       
       .
      
      
       #include <
       
     
        efm32jg1b_ldma_ch.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | CFG | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DST | 
| __IOM uint32_t | LINK | 
| __IOM uint32_t | LOOP | 
| __IOM uint32_t | REQSEL | 
| uint32_t | RESERVED0 [5] | 
| __IOM uint32_t | SRC | 
Field Documentation
| __IOM uint32_t LDMA_CH_TypeDef::CFG | 
Channel Configuration Register
        Definition at line
        
         49
        
        of file
        
         efm32jg1b_ldma_ch.h
        
        .
       
| __IOM uint32_t LDMA_CH_TypeDef::CTRL | 
Channel Descriptor Control Word Register
        Definition at line
        
         51
        
        of file
        
         efm32jg1b_ldma_ch.h
        
        .
       
| __IOM uint32_t LDMA_CH_TypeDef::DST | 
Channel Descriptor Destination Data Address Register
        Definition at line
        
         53
        
        of file
        
         efm32jg1b_ldma_ch.h
        
        .
       
| __IOM uint32_t LDMA_CH_TypeDef::LINK | 
Channel Descriptor Link Structure Address Register
        Definition at line
        
         54
        
        of file
        
         efm32jg1b_ldma_ch.h
        
        .
       
| __IOM uint32_t LDMA_CH_TypeDef::LOOP | 
Channel Loop Counter Register
        Definition at line
        
         50
        
        of file
        
         efm32jg1b_ldma_ch.h
        
        .
       
| __IOM uint32_t LDMA_CH_TypeDef::REQSEL | 
Channel Peripheral Request Select Register
        Definition at line
        
         48
        
        of file
        
         efm32jg1b_ldma_ch.h
        
        .
       
| uint32_t LDMA_CH_TypeDef::RESERVED0[5] | 
Reserved future
        Definition at line
        
         55
        
        of file
        
         efm32jg1b_ldma_ch.h
        
        .
       
| __IOM uint32_t LDMA_CH_TypeDef::SRC | 
Channel Descriptor Source Data Address Register
        Definition at line
        
         52
        
        of file
        
         efm32jg1b_ldma_ch.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG1B/Include/
       efm32jg1b_ldma_ch.h