CMU_TypeDef Struct ReferenceDevices > CMU
CMU Register Declaration
       Definition at line
       
        49
       
       of file
       
        efm32jg1b_cmu.h
       
       .
      
      
       #include <
       
     
        efm32jg1b_cmu.h
       
       >
      
| Data Fields | |
| __IOM uint32_t | ADCCTRL | 
| __IOM uint32_t | AUXHFRCOCTRL | 
| __IOM uint32_t | CALCNT | 
| __IOM uint32_t | CALCTRL | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DBGCLKSEL | 
| __IOM uint32_t | FREEZE | 
| __IOM uint32_t | HFBUSCLKEN0 | 
| __IOM uint32_t | HFCLKSEL | 
| __IM uint32_t | HFCLKSTATUS | 
| __IOM uint32_t | HFCOREPRESC | 
| __IOM uint32_t | HFEXPPRESC | 
| __IOM uint32_t | HFPERCLKEN0 | 
| __IOM uint32_t | HFPERPRESC | 
| __IOM uint32_t | HFPRESC | 
| __IOM uint32_t | HFRCOCTRL | 
| __IOM uint32_t | HFXOCTRL | 
| __IOM uint32_t | HFXOCTRL1 | 
| __IOM uint32_t | HFXOSTARTUPCTRL | 
| __IOM uint32_t | HFXOSTEADYSTATECTRL | 
| __IOM uint32_t | HFXOTIMEOUTCTRL | 
| __IM uint32_t | HFXOTRIMSTATUS | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | LFACLKEN0 | 
| __IOM uint32_t | LFACLKSEL | 
| __IOM uint32_t | LFAPRESC0 | 
| __IOM uint32_t | LFBCLKEN0 | 
| __IOM uint32_t | LFBCLKSEL | 
| __IOM uint32_t | LFBPRESC0 | 
| __IOM uint32_t | LFECLKEN0 | 
| __IOM uint32_t | LFECLKSEL | 
| __IOM uint32_t | LFEPRESC0 | 
| __IOM uint32_t | LFRCOCTRL | 
| __IOM uint32_t | LFXOCTRL | 
| __IOM uint32_t | LOCK | 
| __IOM uint32_t | OSCENCMD | 
| __IOM uint32_t | PCNTCTRL | 
| uint32_t | RESERVED0 [3] | 
| uint32_t | RESERVED1 [1] | 
| uint32_t | RESERVED10 [7] | 
| uint32_t | RESERVED11 [1] | 
| uint32_t | RESERVED12 [1] | 
| uint32_t | RESERVED13 [3] | 
| uint32_t | RESERVED14 [1] | 
| uint32_t | RESERVED15 [1] | 
| uint32_t | RESERVED16 [2] | 
| uint32_t | RESERVED17 [1] | 
| uint32_t | RESERVED18 [1] | 
| uint32_t | RESERVED19 [3] | 
| uint32_t | RESERVED2 [1] | 
| uint32_t | RESERVED20 [2] | 
| uint32_t | RESERVED21 [2] | 
| uint32_t | RESERVED22 [4] | 
| uint32_t | RESERVED23 [2] | 
| uint32_t | RESERVED3 [4] | 
| uint32_t | RESERVED4 [2] | 
| uint32_t | RESERVED5 [2] | 
| uint32_t | RESERVED6 [2] | 
| uint32_t | RESERVED7 [1] | 
| uint32_t | RESERVED8 [1] | 
| uint32_t | RESERVED9 [3] | 
| __IOM uint32_t | ROUTELOC0 | 
| __IOM uint32_t | ROUTEPEN | 
| __IM uint32_t | STATUS | 
| __IM uint32_t | SYNCBUSY | 
| __IOM uint32_t | ULFRCOCTRL | 
Field Documentation
| __IOM uint32_t CMU_TypeDef::ADCCTRL | 
ADC Control Register
        Definition at line
        
         127
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::AUXHFRCOCTRL | 
AUXHFRCO Control Register
        Definition at line
        
         56
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::CALCNT | 
Calibration Counter Register
        Definition at line
        
         70
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::CALCTRL | 
Calibration Control Register
        Definition at line
        
         69
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::CMD | 
Command Register
        Definition at line
        
         73
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::CTRL | 
CMU Control Register
        Definition at line
        
         50
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::DBGCLKSEL | 
Debug Trace Clock Select
        Definition at line
        
         75
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::FREEZE | 
Freeze Register
        Definition at line
        
         122
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFBUSCLKEN0 | 
High Frequency Bus Clock Enable Register 0
        Definition at line
        
         91
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFCLKSEL | 
High Frequency Clock Select Command Register
        Definition at line
        
         76
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IM uint32_t CMU_TypeDef::HFCLKSTATUS | 
HFCLK Status Register
        Definition at line
        
         84
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFCOREPRESC | 
High Frequency Core Clock Prescaler Register
        Definition at line
        
         107
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFEXPPRESC | 
High Frequency Export Clock Prescaler Register
        Definition at line
        
         111
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFPERCLKEN0 | 
High Frequency Peripheral Clock Enable Register 0
        Definition at line
        
         94
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFPERPRESC | 
High Frequency Peripheral Clock Prescaler Register
        Definition at line
        
         108
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFPRESC | 
High Frequency Clock Prescaler Register
        Definition at line
        
         104
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFRCOCTRL | 
HFRCO Control Register
        Definition at line
        
         53
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFXOCTRL | 
HFXO Control Register
        Definition at line
        
         60
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFXOCTRL1 | 
HFXO Control 1
        Definition at line
        
         61
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFXOSTARTUPCTRL | 
HFXO Startup Control
        Definition at line
        
         62
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFXOSTEADYSTATECTRL | 
HFXO Steady State Control
        Definition at line
        
         63
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::HFXOTIMEOUTCTRL | 
HFXO Timeout Control
        Definition at line
        
         64
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IM uint32_t CMU_TypeDef::HFXOTRIMSTATUS | 
HFXO Trim Status
        Definition at line
        
         86
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         90
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IM uint32_t CMU_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         87
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         89
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         88
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFACLKEN0 | 
Low Frequency a Clock Enable Register 0 (Async Reg)
        Definition at line
        
         97
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFACLKSEL | 
Low Frequency A Clock Select Register
        Definition at line
        
         78
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFAPRESC0 | 
Low Frequency a Prescaler Register 0 (Async Reg)
        Definition at line
        
         114
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFBCLKEN0 | 
Low Frequency B Clock Enable Register 0 (Async Reg)
        Definition at line
        
         99
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFBCLKSEL | 
Low Frequency B Clock Select Register
        Definition at line
        
         79
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFBPRESC0 | 
Low Frequency B Prescaler Register 0 (Async Reg)
        Definition at line
        
         116
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFECLKEN0 | 
Low Frequency E Clock Enable Register 0 (Async Reg)
        Definition at line
        
         102
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFECLKSEL | 
Low Frequency E Clock Select Register
        Definition at line
        
         80
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFEPRESC0 | 
Low Frequency E Prescaler Register 0 (Async Reg)
        Definition at line
        
         118
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFRCOCTRL | 
LFRCO Control Register
        Definition at line
        
         59
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LFXOCTRL | 
LFXO Control Register
        Definition at line
        
         65
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         134
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::OSCENCMD | 
Oscillator Enable/Disable Command Register
        Definition at line
        
         72
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::PCNTCTRL | 
PCNT Control Register
        Definition at line
        
         124
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED0[3] | 
Reserved for future use
        Definition at line
        
         52
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED1[1] | 
Reserved for future use
        Definition at line
        
         55
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED10[7] | 
Reserved for future use
        Definition at line
        
         96
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED11[1] | 
Reserved for future use
        Definition at line
        
         98
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED12[1] | 
Reserved for future use
        Definition at line
        
         101
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED13[3] | 
Reserved for future use
        Definition at line
        
         103
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED14[1] | 
Reserved for future use
        Definition at line
        
         106
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED15[1] | 
Reserved for future use
        Definition at line
        
         110
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED16[2] | 
Reserved for future use
        Definition at line
        
         113
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED17[1] | 
Reserved for future use
        Definition at line
        
         115
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED18[1] | 
Reserved for future use
        Definition at line
        
         117
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED19[3] | 
Reserved for future use
        Definition at line
        
         120
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED2[1] | 
Reserved for future use
        Definition at line
        
         58
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED20[2] | 
Reserved for future use
        Definition at line
        
         123
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED21[2] | 
Reserved for future use
        Definition at line
        
         126
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED22[4] | 
Reserved for future use
        Definition at line
        
         129
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED23[2] | 
Reserved for future use
        Definition at line
        
         133
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED3[4] | 
Reserved for future use
        Definition at line
        
         68
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED4[2] | 
Reserved for future use
        Definition at line
        
         71
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED5[2] | 
Reserved for future use
        Definition at line
        
         74
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED6[2] | 
Reserved for future use
        Definition at line
        
         77
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED7[1] | 
Reserved for future use
        Definition at line
        
         82
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED8[1] | 
Reserved for future use
        Definition at line
        
         85
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| uint32_t CMU_TypeDef::RESERVED9[3] | 
Reserved for future use
        Definition at line
        
         93
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::ROUTELOC0 | 
I/O Routing Location Register
        Definition at line
        
         131
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::ROUTEPEN | 
I/O Routing Pin Enable Register
        Definition at line
        
         130
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IM uint32_t CMU_TypeDef::STATUS | 
Status Register
        Definition at line
        
         83
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IM uint32_t CMU_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         121
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
| __IOM uint32_t CMU_TypeDef::ULFRCOCTRL | 
ULFRCO Control Register
        Definition at line
        
         66
        
        of file
        
         efm32jg1b_cmu.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG1B/Include/
       efm32jg1b_cmu.h