tftdirect.c File Reference
EFM32GG_DK3750, TFT Initialization and setup for Direct Drive mode.
- Version
- 5.4.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        tftdirect.c
       
       .
      
       #include <stdbool.h>
      
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_gpio.h
       
       "
      
      
       #include "
       
        em_ebi.h
       
       "
      
      
       #include "
       
        bsp.h
       
       "
      
      
       #include "
       
        tftdirect.h
       
       "
      
      
       #include "
       
        glib/glib.h
       
       "
      
      
| Functions | |
| void | TFT_DirectGPIOConfig (void) | 
| GPIO configuration for TFT direct drive. | |
| bool | TFT_DirectInit (const EBI_TFTInit_TypeDef *tftInit) | 
| TFT initialize or reinitialize Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI) | |
| Variables | |
| static bool | runOnce = true | 
Variable Documentation
| 
 | static | 
Flag to indicate that we need to initialize once if starting up in
        Definition at line
        
         26
        
        of file
        
         tftdirect.c
        
        .
       
Referenced by TFT_DirectInit() .