FPUEH_TypeDef Struct ReferenceDevices > FPUEH

FPUEH Register Declaration

Definition at line 49 of file efr32mg1p_fpueh.h .

#include < efr32mg1p_fpueh.h >

Data Fields

__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS

Field Documentation

__IOM uint32_t FPUEH_TypeDef::IEN

Interrupt Enable Register

Definition at line 53 of file efr32mg1p_fpueh.h .

__IM uint32_t FPUEH_TypeDef::IF

Interrupt Flag Register

Definition at line 50 of file efr32mg1p_fpueh.h .

__IOM uint32_t FPUEH_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 52 of file efr32mg1p_fpueh.h .

__IOM uint32_t FPUEH_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 51 of file efr32mg1p_fpueh.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32MG1P/Include/ efr32mg1p_fpueh.h