MIC - Microphone Driver (ADC)BSP > Thunderboard Sense BSP
Detailed Description
Driver for the Knowles SPV1840LR5H-B MEMS Microphone.
         Functions | 
       |
| void | MIC_deInit (void) | 
| 
         Powers down the MEMS microphone stops the ADC and frees up the DMA channel.
          | 
       |
| float | MIC_getMean (void) | 
| 
         Calculates the average value of the samples in the buffer.
          | 
       |
| uint16_t * | MIC_getSampleBuffer (void) | 
| 
         Gets the sample buffer.
          | 
       |
| float | MIC_getSoundLevel (float *var) | 
| 
         Calculates the sound level.
          | 
       |
| uint32_t | MIC_init (uint32_t fs, uint16_t *buffer, size_t len) | 
| 
         Initializes MEMS microphone and sets up the DMA, ADC and clocking.
          | 
       |
| bool | MIC_isBusy (void) | 
| 
         Checks if the microphone is in use.
          | 
       |
| void | MIC_start (uint32_t nSamples) | 
| 
         Starts taking samples using DMA from the microphone.
          | 
       |
         Error Codes | 
       |
| #define | MIC_OK 0 | 
Macro Definition Documentation
| #define MIC_OK 0 | 
No errors
        Definition at line
        
         43
        
        of file
        
         mic.h
        
        .
       
Function Documentation
| void MIC_deInit | ( | void | 
           
           
           | 
          ) | 
Powers down the MEMS microphone stops the ADC and frees up the DMA channel.
- Returns
 - None
 
        Definition at line
        
         174
        
        of file
        
         mic.c
        
        .
       
References BOARD_micEnable() , DMADRV_FreeChannel() , and PRS_SourceAsyncSignalSet() .
| float MIC_getMean | ( | void | 
           
           
           | 
          ) | 
Calculates the average value of the samples in the buffer.
- Returns
 - The mean value of the samples in the buffer
 
        Definition at line
        
         247
        
        of file
        
         mic.c
        
        .
       
Referenced by MIC_getSoundLevel() .
| uint16_t * MIC_getSampleBuffer | ( | void | 
           
           
           | 
          ) | 
Gets the sample buffer.
- Returns
 - Returns a pointer to the sample buffer
 
        Definition at line
        
         235
        
        of file
        
         mic.c
        
        .
       
| float MIC_getSoundLevel | ( | float * | 
           
            var
           
           | 
          ) | 
Calculates the sound level.
- Parameters
 - 
         
[out] varThe variance of the samples  
- Returns
 - The sound level in dB
 
        Definition at line
        
         272
        
        of file
        
         mic.c
        
        .
       
References MIC_getMean() .
| uint32_t MIC_init | ( | uint32_t | 
           
            fs,
           
           | 
         
| uint16_t * | 
           
            buffer,
           
           | 
         ||
| size_t | 
           
            len
           
           | 
         ||
| ) | 
Initializes MEMS microphone and sets up the DMA, ADC and clocking.
- Parameters
 - 
         
[in] fsThe desired sample rate in Hz [in] bufferPointer to the sample buffer to store the ADC data [in] lenThe size of the sample buffer  
- Returns
 - Returns zero on OK, non-zero otherwise
 
        Definition at line
        
         78
        
        of file
        
         mic.c
        
        .
       
References ADC0 , ADC_Init() , ADC_INIT_DEFAULT , ADC_InitScan() , ADC_INITSCAN_DEFAULT , ADC_PrescaleCalc() , ADC_ScanInputClear() , ADC_ScanSingleEndedInputAdd() , ADC_TimebaseCalc() , adcInit() , adcRef2V5 , BOARD_micEnable() , CMU , CMU_ADCCTRL_ADC0CLKSEL_AUXHFRCO , CMU_ClockEnable() , CMU_ClockFreqGet() , CMU_ClockSelectSet() , CMU_CTRL_CLKOUTSEL1_LFXOQ , CMU_CTRL_CLKOUTSEL1_ULFRCOQ , cmuClock_ADC0 , cmuClock_AUX , cmuClock_LFA , cmuClock_PRS , cmuSelect_LFXO , LETIMER_Init_TypeDef::comp0Top , DMADRV_AllocateChannel() , DMADRV_Init() , ECODE_EMDRV_DMADRV_OK , ADC_Init_TypeDef::em2ClockConfig , LETIMER_Init_TypeDef::enable , LETIMER_CompareSet() , LETIMER_Init() , LETIMER_INIT_DEFAULT , LETIMER_RepeatSet() , letimerUFOAPulse , ADC_Init_TypeDef::prescale , PRS_SourceAsyncSignalSet() , ADC_InitScan_TypeDef::prsEnable , ADC_InitScan_TypeDef::prsSel , ADC_InitScan_TypeDef::reference , ADC_InitScan_TypeDef::scanDmaEm2Wu , ADC_Init_TypeDef::timebase , and LETIMER_Init_TypeDef::ufoa0 .
| bool MIC_isBusy | ( | void | 
           
           
           | 
          ) | 
Checks if the microphone is in use.
- Returns
 - Returns true if the DMA is busy taking microphone samples
 
        Definition at line
        
         311
        
        of file
        
         mic.c
        
        .
       
| void MIC_start | ( | uint32_t | 
           
            nSamples
           
           | 
          ) | 
Starts taking samples using DMA from the microphone.
- Parameters
 - 
         
[in] nSamplesThe number of the samples to take  
- Returns
 - None
 
        Definition at line
        
         200
        
        of file
        
         mic.c
        
        .
       
References ADC0 , DMADRV_PeripheralMemory() , dmadrvDataSize2 , and dmadrvPeripheralSignal_ADC0_SCAN .