PCNT_TypeDef Struct ReferenceDevices > PCNT
PCNT Register Declaration
       Definition at line
       
        49
       
       of file
       
        efm32jg1b_pcnt.h
       
       .
      
      
       #include <
       
     
        efm32jg1b_pcnt.h
       
       >
      
         Data Fields | 
       |
| __IM uint32_t | AUXCNT | 
| __IOM uint32_t | CMD | 
| __IM uint32_t | CNT | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | FREEZE | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | INPUT | 
| __IOM uint32_t | OVSCFG | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [4] | 
| uint32_t | RESERVED2 [7] | 
| __IOM uint32_t | ROUTELOC0 | 
| __IM uint32_t | STATUS | 
| __IM uint32_t | SYNCBUSY | 
| __IM uint32_t | TOP | 
| __IOM uint32_t | TOPB | 
Field Documentation
| __IM uint32_t PCNT_TypeDef::AUXCNT | 
Auxiliary Counter Value Register
        Definition at line
        
         68
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_AuxCounterGet() .
| __IOM uint32_t PCNT_TypeDef::CMD | 
Command Register
        Definition at line
        
         51
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_CounterTopSet() , PCNT_Init() , and PCNT_TopSet() .
| __IM uint32_t PCNT_TypeDef::CNT | 
Counter Value Register
        Definition at line
        
         53
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_CounterGet() .
| __IOM uint32_t PCNT_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_CounterReset() , PCNT_CounterTopSet() , PCNT_Enable() , PCNT_FilterConfiguration() , PCNT_Init() , PCNT_Reset() , and PCNT_TCCConfiguration() .
| __IOM uint32_t PCNT_TypeDef::FREEZE | 
Freeze Register
        Definition at line
        
         64
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_FreezeEnable() .
| __IOM uint32_t PCNT_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         59
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_IntDisable() , PCNT_IntEnable() , PCNT_IntGetEnabled() , and PCNT_Reset() .
| __IM uint32_t PCNT_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         56
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_IntGet() , and PCNT_IntGetEnabled() .
| __IOM uint32_t PCNT_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         58
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_IntClear() , and PCNT_Reset() .
| __IOM uint32_t PCNT_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         57
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_IntSet() .
| __IOM uint32_t PCNT_TypeDef::INPUT | 
PCNT Input Register
        Definition at line
        
         69
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_Init() , and PCNT_PRSInputEnable() .
| __IOM uint32_t PCNT_TypeDef::OVSCFG | 
Oversampling Config Register
        Definition at line
        
         70
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_FilterConfiguration() .
| uint32_t PCNT_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         60
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
| uint32_t PCNT_TypeDef::RESERVED1[4] | 
Reserved for future use
        Definition at line
        
         63
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
| uint32_t PCNT_TypeDef::RESERVED2[7] | 
Reserved for future use
        Definition at line
        
         67
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
| __IOM uint32_t PCNT_TypeDef::ROUTELOC0 | 
I/O Routing Location Register
        Definition at line
        
         61
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
| __IM uint32_t PCNT_TypeDef::STATUS | 
Status Register
        Definition at line
        
         52
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
| __IM uint32_t PCNT_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         65
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_FreezeEnable() .
| __IM uint32_t PCNT_TypeDef::TOP | 
Top Value Register
        Definition at line
        
         54
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_CounterSet() , and PCNT_TopGet() .
| __IOM uint32_t PCNT_TypeDef::TOPB | 
Top Value Buffer Register
        Definition at line
        
         55
        
        of file
        
         efm32jg1b_pcnt.h
        
        .
       
Referenced by PCNT_CounterTopSet() , PCNT_Init() , PCNT_TopBufferGet() , PCNT_TopBufferSet() , and PCNT_TopSet() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG1B/Include/
       
efm32jg1b_pcnt.h