RTCC_TypeDef Struct ReferenceDevices > RTCC
RTCC Register Declaration
       Definition at line
       
        49
       
       of file
       
        efm32jg1b_rtcc.h
       
       .
      
      
       #include <
       
     
        efm32jg1b_rtcc.h
       
       >
      
         Data Fields | 
       |
| RTCC_CC_TypeDef | CC [3] | 
| __IOM uint32_t | CMD | 
| __IOM uint32_t | CNT | 
| __IM uint32_t | COMBCNT | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DATE | 
| __IOM uint32_t | EM4WUEN | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | LOCK | 
| __IOM uint32_t | POWERDOWN | 
| __IOM uint32_t | PRECNT | 
| uint32_t | RESERVED0 [37] | 
| RTCC_RET_TypeDef | RET [32] | 
| __IM uint32_t | STATUS | 
| __IM uint32_t | SYNCBUSY | 
| __IOM uint32_t | TIME | 
Field Documentation
| RTCC_CC_TypeDef RTCC_TypeDef::CC[3] | 
Capture/Compare Channel
        Definition at line
        
         67
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::CMD | 
Command Register
        Definition at line
        
         61
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::CNT | 
Counter Value Register
        Definition at line
        
         52
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IM uint32_t RTCC_TypeDef::COMBCNT | 
Combined Pre-Counter and Counter Value Register
        Definition at line
        
         53
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::DATE | 
Date Register
        Definition at line
        
         55
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::EM4WUEN | 
Wake Up Enable
        Definition at line
        
         65
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         59
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IM uint32_t RTCC_TypeDef::IF | 
RTCC Interrupt Flags
        Definition at line
        
         56
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         58
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         57
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::LOCK | 
Configuration Lock Register
        Definition at line
        
         64
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::POWERDOWN | 
Retention RAM Power-down Register
        Definition at line
        
         63
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::PRECNT | 
Pre-Counter Value Register
        Definition at line
        
         51
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| uint32_t RTCC_TypeDef::RESERVED0[37] | 
Reserved registers
        Definition at line
        
         69
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| RTCC_RET_TypeDef RTCC_TypeDef::RET[32] | 
RetentionReg
        Definition at line
        
         70
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IM uint32_t RTCC_TypeDef::STATUS | 
Status Register
        Definition at line
        
         60
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IM uint32_t RTCC_TypeDef::SYNCBUSY | 
Synchronization Busy Register
        Definition at line
        
         62
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
| __IOM uint32_t RTCC_TypeDef::TIME | 
Time of Day Register
        Definition at line
        
         54
        
        of file
        
         efm32jg1b_rtcc.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG1B/Include/
       
efm32jg1b_rtcc.h